AM263Px MCU+ SDK  26.00.00

Detailed Description

This is a FirewallReq_t type which holds the information of Firewall configuration.

Data Fields

uint16_t regionCount
 
uint16_t crcArr
 
FirewallRegionReq_tFirewallRegionArr
 
uint16_t statusFirewallRegionArr
 

Field Documentation

◆ regionCount

uint16_t FirewallReq_t::regionCount

Region count

◆ crcArr

uint16_t FirewallReq_t::crcArr

crc of FirewallRegionArr

◆ FirewallRegionArr

FirewallRegionReq_t* FirewallReq_t::FirewallRegionArr

Array containing set firewall region request

◆ statusFirewallRegionArr

uint16_t FirewallReq_t::statusFirewallRegionArr

Status of all region requests