AM263Px MCU+ SDK  26.00.00
FLSOPSKD_Params Struct Reference

Data Fields

uint8_t eraseOpCode
 
uint8_t eraseExOpCode
 
uint16_t pageSizeInBytes
 
uint32_t eraseSizeInBytes
 
uint32_t pollTimeout
 

Field Documentation

◆ eraseOpCode

uint8_t FLSOPSKD_Params::eraseOpCode

Configure Erase OpCode

◆ eraseExOpCode

uint8_t FLSOPSKD_Params::eraseExOpCode

Configure Erase ExOpCode

◆ pageSizeInBytes

uint16_t FLSOPSKD_Params::pageSizeInBytes

Size of page in bytes during writing. Should be less than 512B

◆ eraseSizeInBytes

uint32_t FLSOPSKD_Params::eraseSizeInBytes

Number of bytes erase at time with above opcode

◆ pollTimeout

uint32_t FLSOPSKD_Params::pollTimeout

Amount of time to block waiting, in units of system ticks