AM263Px MCU+ SDK  26.00.00
Enet_DfltFlowInfo Struct Reference

Detailed Description

Rx Default Flow Info used for default flow registration/unregistration.

Data Fields

uint32_t coreKey
 
uint32_t chIdx
 
uint32_t startIdx
 
uint32_t flowIdx
 

Field Documentation

◆ coreKey

uint32_t Enet_DfltFlowInfo::coreKey

Core key

◆ chIdx

uint32_t Enet_DfltFlowInfo::chIdx

0-relative channel index

◆ startIdx

uint32_t Enet_DfltFlowInfo::startIdx

RX flow base or start index

◆ flowIdx

uint32_t Enet_DfltFlowInfo::flowIdx

Allocated flow's index (offset from startIdx)