AM263Px MCU+ SDK  26.00.00
EnetRm_IoctlPermissionTable Struct Reference

Detailed Description

Enet RM IOCTL permission table.

This structure has the information about IOCTL permissions for all IOCTL commands.

Data Fields

uint32_t defaultPermittedCoreMask
 
uint32_t numEntries
 
EnetRm_IoctlPermissionEntry entry [ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX]
 

Field Documentation

◆ defaultPermittedCoreMask

uint32_t EnetRm_IoctlPermissionTable::defaultPermittedCoreMask

Permitted core mask if IOCTL command not found in explicit permission entry table

◆ numEntries

uint32_t EnetRm_IoctlPermissionTable::numEntries

Number of explicit permission entry

◆ entry

Permission table entries. Must have numEntries valid entries