AM263Px MCU+ SDK  26.00.00
EnetRm_IoctlPermissionEntry Struct Reference

Detailed Description

Enet RM IOCTL permission entry.

This structure has the information about IOCTL permissions for each IOCTL command.

Data Fields

uint32_t cmd
 
uint32_t permittedCoreMask
 

Field Documentation

◆ cmd

uint32_t EnetRm_IoctlPermissionEntry::cmd

IOCTL command

◆ permittedCoreMask

uint32_t EnetRm_IoctlPermissionEntry::permittedCoreMask

Cores from which this IOCTL call is allowed. This is a bitmask of allowed coreIds