AM263Px MCU+ SDK  26.00.00

Detailed Description

DP83TG721 PHY configuration parameters.

Data Fields

bool isMDIMaster
 
bool enablePTPstatusFrames
 
uint32_t srcMacStatusFrameType
 
uint8_t clockSource
 
uint8_t enableMediaClock
 
uint8_t mediaClockMode
 
uint8_t enableCodecClock
 
uint32_t codecClkDiv
 
uint32_t mediaClkDiv
 

Field Documentation

◆ isMDIMaster

bool Dp83tg721_Cfg::isMDIMaster

◆ enablePTPstatusFrames

bool Dp83tg721_Cfg::enablePTPstatusFrames

◆ srcMacStatusFrameType

uint32_t Dp83tg721_Cfg::srcMacStatusFrameType

◆ clockSource

uint8_t Dp83tg721_Cfg::clockSource

◆ enableMediaClock

uint8_t Dp83tg721_Cfg::enableMediaClock

◆ mediaClockMode

uint8_t Dp83tg721_Cfg::mediaClockMode

◆ enableCodecClock

uint8_t Dp83tg721_Cfg::enableCodecClock

◆ codecClkDiv

uint32_t Dp83tg721_Cfg::codecClkDiv

◆ mediaClkDiv

uint32_t Dp83tg721_Cfg::mediaClkDiv