AM263Px MCU+ SDK  26.00.00
Diag_Mon_Sin_Cos_Weak_Amplitude Struct Reference

Detailed Description

Structure to hold the control/status data for Diagnostics mentioned under Monitor weak Sin or Cos signal below a threshold (LOS)

Values that can be passed to RDC_getDiagnosticsWeakAmplitudeData(), RDC_setDiagnosticsWeakAmplitudeData() as Diag_Mon_Sin_Cos_Weak_Amplitude parameter

Data Fields

uint16_t lowAmplitude_threshold
 
uint8_t lowAmplitude_glitchcount
 
bool lowAmplitude_error
 
int16_t lowAmplitude_sin_value
 
int16_t lowAmplitude_cos_value
 

Field Documentation

◆ lowAmplitude_threshold

uint16_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_threshold

◆ lowAmplitude_glitchcount

uint8_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_glitchcount

◆ lowAmplitude_error

bool Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_error

◆ lowAmplitude_sin_value

int16_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_sin_value

◆ lowAmplitude_cos_value

int16_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_cos_value