AM263Px MCU+ SDK  26.00.00
Diag_Mon_Sin_Cos_High_Amplitude Struct Reference

Detailed Description

Structure to hold the control/status data for Diagnostics mentioned under Monitor Sin or Cos saturation or very high amplitude (DOS)

Values that can be passed to RDC_getDiagnosticsHighAmplitudeData(), RDC_setDiagnosticsHighAmplitudeData() as Diag_Mon_Sin_Cos_High_Amplitude parameter

Data Fields

uint16_t highAmplitude_threshold
 
uint8_t highAmplitude_glitchcount
 
int16_t highAmplitude_sin_value
 
int16_t highAmplitude_cos_value
 
bool highAmplitude_sin_error
 
bool highAmplitude_cos_error
 

Field Documentation

◆ highAmplitude_threshold

uint16_t Diag_Mon_Sin_Cos_High_Amplitude::highAmplitude_threshold

◆ highAmplitude_glitchcount

uint8_t Diag_Mon_Sin_Cos_High_Amplitude::highAmplitude_glitchcount

◆ highAmplitude_sin_value

int16_t Diag_Mon_Sin_Cos_High_Amplitude::highAmplitude_sin_value

◆ highAmplitude_cos_value

int16_t Diag_Mon_Sin_Cos_High_Amplitude::highAmplitude_cos_value

◆ highAmplitude_sin_error

bool Diag_Mon_Sin_Cos_High_Amplitude::highAmplitude_sin_error

◆ highAmplitude_cos_error

bool Diag_Mon_Sin_Cos_High_Amplitude::highAmplitude_cos_error