AM263Px MCU+ SDK  26.00.00
Diag_Mon_Signal_Integrity_SinSq_CosSq Struct Reference

Detailed Description

Structure to hold the control/status data for Diagnostics mentioned under Monitor signal integrity by checking Sin2+Cos2=Constant (DOS)

Values that can be passed to RDC_getDiagnosticsSignalIntegritySquareSumData(), RDC_setDiagnosticsSignalIntegritySquareSumData() as Diag_Mon_Signal_Integrity_SinSq_CosSq parameter

Data Fields

uint16_t sinsqcossq_threshold_hi
 
uint16_t sinsqcossq_threshold_lo
 
uint8_t sinsqcossq_glitchcount
 
uint16_t sinsqcossq_cossq
 
uint16_t sinsqcossq_sinsq
 
bool sinsqcossq_hi
 
bool sinsqcossq_lo
 

Field Documentation

◆ sinsqcossq_threshold_hi

uint16_t Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_threshold_hi

◆ sinsqcossq_threshold_lo

uint16_t Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_threshold_lo

◆ sinsqcossq_glitchcount

uint8_t Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_glitchcount

◆ sinsqcossq_cossq

uint16_t Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_cossq

◆ sinsqcossq_sinsq

uint16_t Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_sinsq

◆ sinsqcossq_hi

bool Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_hi

◆ sinsqcossq_lo

bool Diag_Mon_Signal_Integrity_SinSq_CosSq::sinsqcossq_lo