AM263Px MCU+ SDK  26.00.00
DTHE_Attrs Struct Reference

Detailed Description

DTHE attributes.

Data Fields

uint32_t caBaseAddr
 
uint32_t aesBaseAddr
 
uint32_t shaBaseAddr
 
uint32_t sm3BaseAddr
 
uint32_t sm4BaseAddr
 
uint32_t isOpen
 
uint32_t faultStatus
 

Field Documentation

◆ caBaseAddr

uint32_t DTHE_Attrs::caBaseAddr

Crypto Accelerator Base Adders

◆ aesBaseAddr

uint32_t DTHE_Attrs::aesBaseAddr

Aes Base address

◆ shaBaseAddr

uint32_t DTHE_Attrs::shaBaseAddr

sha Base address

◆ sm3BaseAddr

uint32_t DTHE_Attrs::sm3BaseAddr

sm3 Base address if supported by the device

◆ sm4BaseAddr

uint32_t DTHE_Attrs::sm4BaseAddr

sm4 Base address if supported by the device

◆ isOpen

uint32_t DTHE_Attrs::isOpen

Flag to indicate whether the instance is opened already

◆ faultStatus

uint32_t DTHE_Attrs::faultStatus

Flag to ascertain whether the handle was opened successfully