AM263Px MCU+ SDK  26.00.00
CpswCpts_SetCompValInArgs Struct Reference

Detailed Description

Input args for CPSW_CPTS_IOCTL_SET_COMP command.

Data Fields

uint64_t tsCompVal
 
uint32_t tsCompLen
 
bool tsCompToggle
 

Field Documentation

◆ tsCompVal

uint64_t CpswCpts_SetCompValInArgs::tsCompVal

64-bit time stamp compare value

◆ tsCompLen

uint32_t CpswCpts_SetCompValInArgs::tsCompLen

Time stamp comparison length value

◆ tsCompToggle

bool CpswCpts_SetCompValInArgs::tsCompToggle

Time stamp compare toggle mode selection. true : Toggle mode false: Non-toggle mode