AM263Px MCU+ SDK  26.00.00
CANFD_MCANBitTimingParams Struct Reference

Data Fields

uint32_t nomBrp
 
uint32_t nomPropSeg
 
uint32_t nomPseg1
 
uint32_t nomPseg2
 
uint32_t nomSjw
 
uint32_t dataBrp
 
uint32_t dataPropSeg
 
uint32_t dataPseg1
 
uint32_t dataPseg2
 
uint32_t dataSjw
 

Field Documentation

◆ nomBrp

uint32_t CANFD_MCANBitTimingParams::nomBrp

Nominal Baud Rate Pre-scaler

◆ nomPropSeg

uint32_t CANFD_MCANBitTimingParams::nomPropSeg

NominalProp Segment value

◆ nomPseg1

uint32_t CANFD_MCANBitTimingParams::nomPseg1

NominalPhase Segment1 value

◆ nomPseg2

uint32_t CANFD_MCANBitTimingParams::nomPseg2

NominalPhase Segment2 value

◆ nomSjw

uint32_t CANFD_MCANBitTimingParams::nomSjw

Nominal (Re)Synchronization Jump Width

◆ dataBrp

uint32_t CANFD_MCANBitTimingParams::dataBrp

Nominal Baud Rate Pre-scaler

◆ dataPropSeg

uint32_t CANFD_MCANBitTimingParams::dataPropSeg

NominalProp Segment value

◆ dataPseg1

uint32_t CANFD_MCANBitTimingParams::dataPseg1

NominalPhase Segment1 value

◆ dataPseg2

uint32_t CANFD_MCANBitTimingParams::dataPseg2

NominalPhase Segment2 value

◆ dataSjw

uint32_t CANFD_MCANBitTimingParams::dataSjw

Nominal (Re)Synchronization Jump Width