AM263Px MCU+ SDK  26.00.00

Introduction

MMCSD LLD Driver API/interface file.

Go to the source code of this file.

Return status

#define MMCSD_STS_SUCCESS   ((int32_t) 0)
 Return status when the API execution was successful. More...
 
#define MMCSD_STS_ERR   ((int32_t)-1)
 Return status when the API execution was not successful due to a generic Error. More...
 
#define MMCSD_STS_ERR_TIMEOUT   ((int32_t)-2)
 Return status when the API execution was not successful due to a time out. More...
 
#define MMCSD_STS_ERR_INVALID_PARAM   ((int32_t)-3)
 Return status when the API execution failed due invalid parameters. More...
 
#define MMCSD_STS_ERR_BUSY   ((int32_t)-4)
 Return status when the API execution failed due to driver busy. More...
 
#define MMCSD_STS_ERR_CARD_NOT_FOUND   ((int32_t)-5)
 Return status when the API execution failed due to missing card. More...
 
#define MMCSD_STS_ERR_CARD_UNUSEABLE   ((int32_t)-6)
 Return status when the API execution failed due to unuseable card. More...
 
#define MMCSD_STS_ERR_CARD_UNLOCK_FAIL   ((int32_t)-7)
 Return status when the API execution failed due to card Unlock Failure. More...
 
typedef EDMA_Handle MMCSD_DmaHandle
 
typedef struct MMCSD_EdmaChConfig_s * MMCSD_DmaChConfig
 

Data Structures

struct  MMCSD_EmmcDeviceData
 eMMC device properties More...
 
struct  MMCSD_SdDeviceData
 SD device properties. More...
 
struct  MMCSDLLD_Transaction
 MMCSD LLD Transaction. More...
 
struct  MMCSDLLD_InitObject
 MMCSD Driver Initialization Object. More...
 
struct  MMCSDLLD_Object
 MMCSD Driver Object. More...
 

Macros

Timeout values

#define MMCSD_NO_WAIT   ((uint32_t)0)
 Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More...
 
#define MMCSD_WAIT_FOREVER   ((uint32_t)-1)
 Value to use when needing a timeout of infinity or wait forever until resource is available. More...
 
MMCSD Driver states

#define MMCSD_STATE_RESET   ((uint8_t) 0U)
 MMCSD driver is in Reset State prior to driver init and post driver deinit. More...
 
#define MMCSD_STATE_IDLE   ((uint8_t) 1U)
 MMCSD driver accepts runtime APIs only Ready State, otherwise return error. More...
 
#define MMCSD_STATE_BUSY   ((uint8_t) 2U)
 MMCSD driver is busy performing operation with peripherals, return error when APIs are invoked. More...
 
#define MMCSD_STATE_ERROR   ((uint8_t) 3U)
 MMCSD driver ran into error, returns error for all APIs other than deinit in this state. More...
 
MMCSD Transfer states

#define MMCSD_XFER_IDLE_STATE   ((uint8_t) 0U)
 XFER is in IDLE state. More...
 
#define MMCSD_XFER_CMD_STATE   ((uint8_t) 1U)
 XFER is in CMD state. More...
 
#define MMCSD_XFER_WRITE_STATE   ((uint8_t) 2U)
 XFER is in Write state. More...
 
#define MMCSD_XFER_READ_STATE   ((uint8_t) 3U)
 XFER is in Read state. More...
 
MACROS used to select one of the possible Card Types.

#define MMCSD_CARD_TYPE_SD   ((uint32_t) 0U)
 Card type SD. More...
 
#define MMCSD_CARD_TYPE_EMMC   ((uint32_t) 2U)
 Card type MMC. More...
 
#define MMCSD_CARD_TYPE_NO_DEVICE   ((uint32_t) 3U)
 No Card Installed. More...
 
MACROS for the possible values of Bus Width configuration.

#define MMCSD_BUS_WIDTH_1BIT   ((uint32_t) 1U)
 Card bus width configuration for 1-bit mode. More...
 
#define MMCSD_BUS_WIDTH_4BIT   ((uint32_t) 4U)
 Card bus width configuration for 4-bit mode. More...
 
#define MMCSD_BUS_WIDTH_8BIT   ((uint32_t) 8U)
 Card bus width configuration for 8-bit mode. More...
 
ECSD Bus Width Macros

Macros for Extended CSD (ECSD) bus width configuration in eMMC devices. These macros are used to set or interpret the bus width field in the ECSD register.

#define MMCSD_ECSD_BUS_WIDTH_INDEX   (183U)
 ECSD register index for bus width configuration. More...
 
#define MMCSD_ECSD_BUS_WIDTH_1BIT   (0U)
 ECSD value for 1-bit bus width. More...
 
#define MMCSD_ECSD_BUS_WIDTH_4BIT   (1U)
 ECSD value for 4-bit bus width. More...
 
#define MMCSD_ECSD_BUS_WIDTH_8BIT   (2U)
 ECSD value for 8-bit bus width. More...
 
#define MMCSD_ECSD_BUS_WIDTH_4BIT_DDR   (5U)
 ECSD value for 4-bit DDR bus width. More...
 
#define MMCSD_ECSD_BUS_WIDTH_8BIT_DDR   (6U)
 ECSD value for 8-bit DDR bus width. More...
 
#define MMCSD_ECSD_BUS_WIDTH_BUSWIDTH_MASK   (0x0FU)
 Mask for extracting bus width bits from ECSD value. More...
 
#define MMCSD_ECSD_BUS_WIDTH_BUSWIDTH_SHIFT   (0U)
 Bit shift for bus width bits in ECSD value. More...
 
#define MMCSD_ECSD_BUS_WIDTH_ES_ENABLE   (0x80U)
 Enable Enhanced Strobe in ECSD bus width field. More...
 
#define MMCSD_ECSD_BUS_WIDTH_ES_MASK   (0x80U)
 Mask for Enhanced Strobe bit in ECSD bus width field. More...
 
#define MMCSD_ECSD_BUS_WIDTH_ES_SHIFT   (7U)
 Bit shift for Enhanced Strobe bit in ECSD bus width field. More...
 
MACROS used to select one of the possible Speed Modes for SD Device.

#define MMCSD_SD_MODE_DS   ((uint32_t) 10U)
 Default Speed. More...
 
#define MMCSD_SD_MODE_HS   ((uint32_t) 11U)
 High Speed. More...
 

Typedefs

typedef void(* MMCSD_lld_transferCompleteCallback) (void *args, int32_t xferStatus)
 The definition of a transfer completion callback function used by the MMCSD driver when used in Callback Mode. More...
 
typedef struct MMCSDLLD_InitObjectMMCSDLLD_InitHandle
 
typedef struct MMCSDLLD_ObjectMMCSDLLD_Handle
 

Functions

int32_t MMCSD_lld_init (MMCSDLLD_Handle handle)
 This API Initializes the MMCSD instance. More...
 
int32_t MMCSD_lld_InitDma (MMCSDLLD_Handle handle)
 This API Initializes the MMCSD instance for DMA transfers. More...
 
int32_t MMCSD_lld_deInit (MMCSDLLD_Handle handle)
 This API De-Initializes the MMCSD instance. More...
 
int32_t MMCSD_lld_deInitDma (MMCSDLLD_Handle handle)
 This API De-Initializes the MMCSD instance with DMA transfers. More...
 
int32_t MMCSD_lld_write_SD_Poll (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block writes to the SD media in Polling Mode. More...
 
int32_t MMCSD_lld_read_SD_Poll (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block reads from the SD media in Polling Mode. More...
 
int32_t MMCSD_lld_write_SD_Intr (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block writes to the SD media in Interrupt Mode. More...
 
int32_t MMCSD_lld_read_SD_Intr (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block reads from the SD media in Interrupt Mode. More...
 
int32_t MMCSD_lld_write_SD_Dma (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block writes to the SD media in DMA Mode. More...
 
int32_t MMCSD_lld_read_SD_Dma (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block reads from the SD media in DMA Mode. More...
 
int32_t MMCSD_lld_write_MMC_Poll (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Writes data to the MMC card using polling method. More...
 
int32_t MMCSD_lld_read_MMC_Poll (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Reads data from the MMC card using polling method. More...
 
int32_t MMCSD_lld_write_MMC_Intr (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Writes data to the MMC card using interrupt method. More...
 
int32_t MMCSD_lld_read_MMC_Intr (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Reads data from the MMC card using interrupt method. More...
 
int32_t MMCSD_lld_write_MMC_Dma (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block writes to the MMC media in DMA Mode. More...
 
int32_t MMCSD_lld_read_MMC_Dma (MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block reads from the MMC media in DMA Mode. More...
 
uint32_t MMCSD_lld_getBlockSize (MMCSDLLD_Handle handle)
 This function returns the block size of the MMC/SD media connected to the MMCSD controller. More...
 
void MMCSD_lld_completeCurrTransfer (MMCSDLLD_Handle handle, int32_t xferStatus)
 Completes the current MMC/SD data transfer operation. More...
 
void MMCSD_lld_Isr (void *args)
 This is the MMCSD Controller ISR and can be used as IRQ handler. More...