AM263Px MCU+ SDK  26.00.00
icss_emac.h File Reference

Go to the source code of this file.

Data Structures

struct  ICSS_EMAC_FwStaticMmap
 ICSS EMAC Static Firmware Memory Map offsets. These are offsets for PRU0 and PRU1 DRAM memory. More...
 
struct  ICSS_EMAC_FwDynamicMmap
 ICSS EMAC Dynamic Firmware Memory Map offsets. More...
 
struct  ICSS_EMAC_FwVlanFilterParams
 ICSS EMAC VLAN Filtering Parameters. More...
 
struct  ICSS_EMAC_FwMulticastFilterParams
 ICSS EMAC Multicast Filtering Parameters. More...
 
struct  ICSS_EMAC_Attrs
 
struct  ICSS_EMAC_InternalObject
 Opaque ICSS EMAC driver object. More...
 
struct  ICSS_EMAC_Config
 Base EMAC handle containing pointers to all modules required for driver to work. More...
 
struct  ICSS_EMAC_CallBackConfig
 Generic callback configuration for protocol specific callbacks.
ICSS_EMAC_CallBack is the function prototype used. While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in this structure. More...
 
struct  ICSS_EMAC_CallBackObject
 Different callbacks which can be registered.
While calling the function set in ICSS_EMAC_CallBack, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (as mentioned in the member descriptions), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig. More...
 
struct  ICSS_EMAC_Params
 ICSS_EMAC Parameters. More...
 
struct  ICSS_EMAC_RxArgument
 Rx packet processing information block that needs to passed into call to ICSS_EMAC_RxPktGet. More...
 
struct  ICSS_EMAC_TxArgument
 Tx packet processing information block that needs to passed into call to ICSS_EMAC_txPacket. More...
 
struct  ICSS_EMAC_IoctlCmd
 IOCTL command members for configuring switch/EMAC. More...
 
struct  ICSS_EMAC_PruStatistics
 Statistics structure for capturing statistics on PRU. More...
 

Macros

#define ICSS_EMAC_MAX_PORTS_PER_INSTANCE   (2)
 Maximum number of Ports in a single ICSS
More...
 
#define ICSS_EMAC_NUMQUEUES   ((uint32_t)17U)
 Total Queues available. More...
 
#define ICSS_EMAC_MAXMTU   (1518U)
 Maximum Valid size (incl header + VLAN TAG..., no CRC) More...
 
#define ICSS_EMAC_MINMTU   (14U)
 Minimum Valid size ( DA + SA + Ethertype) More...
 
#define ICSS_EMAC_PORT_0   (0)
 Used to specify host side port. More...
 
#define ICSS_EMAC_PORT_1   (1U)
 Used to specify physical port 1 MII 0 (tx) More...
 
#define ICSS_EMAC_PORT_2   (2U)
 Used to specify physical port 2 MII 1 (tx) More...
 
#define ICSS_EMAC_IOCTL_PORT_CTRL_DISABLE   (0u)
 ICSS_EMAC_IOCTL_PORT_CTRL options. More...
 
#define ICSS_EMAC_IOCTL_PORT_CTRL_ENABLE   (1u)
 Generic IOCTL Disable macro. More...
 
#define ICSS_EMAC_LEARNING_PORT_STATE_LEARNING   (0U)
 Macros for different port states in learning module. More...
 
#define ICSS_EMAC_LEARNING_PORT_STATE_NOT_LEARNING   (1U)
 
#define ICSS_EMAC_LEARNING_PORT_STATE_LOCKED   (2U)
 
#define ICSS_EMAC_OBJECT_SIZE_IN_BYTES   (42000)
 
ICSS EMAC Modes

#define ICSS_EMAC_MODE_MAC1   (1U)
 Single EMAC Mode. Port 1 Enabled. More...
 
#define ICSS_EMAC_MODE_MAC2   (2U)
 Single EMAC Mode. Port 2 Enabled. More...
 
#define ICSS_EMAC_MODE_SWITCH   (3U)
 Switch Mode. More...
 
#define ICSS_EMAC_MODE_DUALMAC   (4U)
 Dual MAC Mode. Both Ports Enabled. More...
 
ICSS EMAC PHY to MAC Interface Modes

#define ICSS_EMAC_MII_MODE   (0U)
 Media-independent Interface. More...
 
#define ICSS_EMAC_RGMII_MODE   (1U)
 Reduced Gigabit Media-independent Interface
More...
 
ICSS EMAC Learning Modes

#define ICSS_EMAC_LEARNING_DISABLE   (0U)
 Driver-based Learning Mode Disabled
More...
 
#define ICSS_EMAC_LEARNING_ENABLE   (1U)
 Driver-based Learning Mode Enabled
More...
 
ICSS EMAC Interrupt Pacing Configuration

#define ICSS_EMAC_ENABLE_PACING   (0)
 Interrupt pacing enabled. More...
 
#define ICSS_EMAC_DISABLE_PACING   (1)
 Interrupt pacing disabled. More...
 
ICSS EMAC Interrupt Pacing Modes

#define ICSS_EMAC_INTR_PACING_MODE1   (0)
 Frame Count based Interrupt pacing. More...
 
ICSS EMAC Queues

#define ICSS_EMAC_QUEUE1   ((uint32_t)0U)
 Priority Queue 1. More...
 
#define ICSS_EMAC_QUEUE2   ((uint32_t)1U)
 Priority Queue 2. More...
 
#define ICSS_EMAC_QUEUE3   ((uint32_t)2U)
 Priority Queue 3. More...
 
#define ICSS_EMAC_QUEUE4   ((uint32_t)3U)
 Priority Queue 4. More...
 
#define ICSS_EMAC_QUEUE5   ((uint32_t)4U)
 Priority Queue 5. More...
 
#define ICSS_EMAC_QUEUE6   ((uint32_t)5U)
 Priority Queue 6. More...
 
#define ICSS_EMAC_QUEUE7   ((uint32_t)6U)
 Priority Queue 7. More...
 
#define ICSS_EMAC_QUEUE8   ((uint32_t)7U)
 Priority Queue 8. More...
 
#define ICSS_EMAC_QUEUE9   ((uint32_t)8U)
 Priority Queue 9. More...
 
#define ICSS_EMAC_QUEUE10   ((uint32_t)9U)
 Priority Queue 10. More...
 
#define ICSS_EMAC_QUEUE11   ((uint32_t)10U)
 Priority Queue 11. More...
 
#define ICSS_EMAC_QUEUE12   ((uint32_t)11U)
 Priority Queue 12. More...
 
#define ICSS_EMAC_QUEUE13   ((uint32_t)12U)
 Priority Queue 13. More...
 
#define ICSS_EMAC_QUEUE14   ((uint32_t)13U)
 Priority Queue 14. More...
 
#define ICSS_EMAC_QUEUE15   ((uint32_t)14U)
 Priority Queue 15. More...
 
#define ICSS_EMAC_QUEUE16   ((uint32_t)15U)
 Priority Queue 16. More...
 
#define ICSS_EMAC_COLQUEUE   ((uint32_t)16U)
 Collision Queue. More...
 
ICSS EMAC Error Codes

#define ICSS_EMAC_SWITCH_ERROR_BASE   ((uint32_t)0x21Fu)
 Switch Error Base. More...
 
#define ICSS_EMAC_SWITCH_ERROR_CODE   (ICSS_EMAC_SWITCH_ERROR_BASE)
 Switch Error Code. More...
 
#define ICSS_EMAC_SWITCH_ERROR_INFO   (ICSS_EMAC_SWITCH_ERROR_CODE)
 Switch Error/Informational. More...
 
#define ICSS_EMAC_SWITCH_ERROR_WARNING   (ICSS_EMAC_SWITCH_ERROR_CODE | 0x1000u)
 Switch Error/Warning. More...
 
#define ICSS_EMAC_SWITCH_ERROR_MINOR   (ICSS_EMAC_SWITCH_ERROR_CODE | 0x2000u)
 Switch Error Minor. More...
 
#define ICSS_EMAC_SWITCH_ERROR_MAJOR   (ICSS_EMAC_SWITCH_ERROR_CODE | 0x3000u)
 Switch Error Major. More...
 
#define ICSS_EMAC_SWITCH_ERROR_CRITICAL   (ICSS_EMAC_SWITCH_ERROR_CODE | 0x4000u)
 Switch Error Critical. More...
 
#define ICSS_EMAC_SWITCH_SUCCESS   (0u)
 Success code. More...
 
#define ICSS_EMAC_PORT1_TX_ERROR_MASK   (0xFFFFu)
 
#define ICSS_EMAC_PORT2_TX_ERROR_MASK   (0xFFFF0000u)
 
#define ICSS_EMAC_ERR_DEV_NOT_INSTANTIATED   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 1u)
 Device is not instantiated yet. More...
 
#define ICSS_EMAC_ERR_SWITCH_INVALID_PARAM   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 2u)
 Function or calling parameter is invalid. More...
 
#define ICSS_EMAC_ERR_CH_INVALID   (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 3u)
 Channel number invalid. More...
 
#define ICSS_EMAC_ERR_CH_ALREADY_INIT   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 4u)
 Channel already initialized and setup. More...
 
#define ICSS_EMAC_ERR_TX_CH_ALREADY_CLOSED   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 5u)
 Tx Channel already closed. Channel close failed. More...
 
#define ICSS_EMAC_ERR_TX_CH_NOT_OPEN   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 6u)
 Tx Channel not open. More...
 
#define ICSS_EMAC_ERR_TX_NO_LINK   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 7u)
 Tx Link not up. More...
 
#define ICSS_EMAC_ERR_TX_OUT_OF_BD   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 8u)
 Tx ran out of Buffer descriptors to use. More...
 
#define ICSS_EMAC_ERR_RX_CH_INVALID   (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 9u)
 Rx Channel invalid number. More...
 
#define ICSS_EMAC_ERR_RX_CH_ALREADY_INIT   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 10u)
 Rx Channel already setup. More...
 
#define ICSS_EMAC_ERR_RX_CH_ALREADY_CLOSED   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 11u)
 Rx Channel already closed. Channel close failed. More...
 
#define ICSS_EMAC_ERR_RX_CH_NOT_OPEN   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 12u)
 Rx Channel not open yet. More...
 
#define ICSS_EMAC_ERR_DEV_ALREADY_CREATED   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 13u)
 EMAC device already created. More...
 
#define ICSS_EMAC_ERR_DEV_NOT_OPEN   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 14u)
 Device is not open or not ready. More...
 
#define ICSS_EMAC_ERR_DEV_ALREADY_CLOSED   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 15u)
 Device close failed. Device already closed. More...
 
#define ICSS_EMAC_ERR_DEV_ALREADY_OPEN   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 16u)
 Device open failed. Device already open. More...
 
#define ICSS_EMAC_ERR_RX_BUFFER_ALLOC_FAIL   (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 17u)
 Rx Buffer Descriptor allocation failed. More...
 
#define ICSS_EMAC_SWITCH_INTERNAL_FAILURE   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 18u)
 EMAC Internal failure. More...
 
#define ICSS_EMAC_SWITCH_VLAN_UNAWARE_MODE   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 19u)
 VLAN support not enabled in EMAC. More...
 
#define ICSS_EMAC_SWITCH_ALE_TABLE_FULL   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 20u)
 ALE Table full. More...
 
#define ICSS_EMAC_SWITCH_ADDR_NOTFOUND   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 21u)
 Multicast/Unicast/OUI Address not found in ALE. More...
 
#define ICSS_EMAC_SWITCH_INVALID_VLANID   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 22u)
 Invalid VLAN Id. More...
 
#define ICSS_EMAC_SWITCH_INVALID_PORT   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 23u)
 Invalid Port Specified. More...
 
#define ICSS_EMAC_SWITCH_BD_ALLOC_FAIL   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 24u)
 Buffer Descriptor Allocation failure. OOM. More...
 
#define ICSS_EMAC_ERR_BADPACKET   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 25u)
 Supplied packet was invalid. More...
 
#define ICSS_EMAC_ERR_COLLISION_FAIL   (ICSS_EMAC_SWITCH_ERROR_MAJOR + 26u)
 Collision queue was full. More...
 
#define ICSS_EMAC_ERR_MACFATAL   (ICSS_EMAC_SWITCH_ERROR_CRITICAL + 26u)
 Fatal Error - ICSS_EMAC_close required. More...
 
ICSS-EMAC Storm Prevention IOCTL Command Options

#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE   (0u)
 IOCTL Storm Control Enable command. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE   (1u)
 IOCTL Storm Control Disable command. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS   (2u)
 IOCTL Storm Control set credit command. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_INIT   (3u)
 IOCTL Storm Control initialize command. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_RESET   (4u)
 IOCTL Storm Control reset command. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE_BC   (5u)
 IOCTL Storm Control Enable command for BC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE_BC   (6u)
 IOCTL Storm Control Disable command for BC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_BC   (7u)
 IOCTL Storm Control set credit command for BC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_INIT_BC   (8u)
 IOCTL Storm Control initialize command for BC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_RESET_BC   (9u)
 IOCTL Storm Control reset command for BC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE_MC   (10u)
 IOCTL Storm Control Enable command for MC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE_MC   (11u)
 IOCTL Storm Control Disable command for MC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_MC   (12u)
 IOCTL Storm Control set credit command for MC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_INIT_MC   (13u)
 IOCTL Storm Control initialize command for MC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_RESET_MC   (14u)
 IOCTL Storm Control reset command for MC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE_UC   (15u)
 IOCTL Storm Control Enable command for UC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE_UC   (16u)
 IOCTL Storm Control Disable command for UC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_UC   (17u)
 IOCTL Storm Control set credit command for UC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_INIT_UC   (18u)
 IOCTL Storm Control initialize command for UC traffic. More...
 
#define ICSS_EMAC_STORM_PREV_CTRL_RESET_UC   (19u)
 IOCTL Storm Control reset command for UC traffic. More...
 
ICSS-EMAC Learning Control IOCTL Command Options

#define ICSS_EMAC_LEARN_CTRL_UPDATE_TABLE   (0u)
 IOCTL Learning Table update command. More...
 
#define ICSS_EMAC_LEARN_CTRL_CLR_TABLE   (1u)
 IOCTL Learning Table clear table command. More...
 
#define ICSS_EMAC_LEARN_CTRL_AGEING   (2u)
 IOCTL Learning Table age out entry command. More...
 
#define ICSS_EMAC_LEARN_CTRL_FIND_MAC   (3u)
 IOCTL Learning Table find port from MAC ID command. More...
 
#define ICSS_EMAC_LEARN_CTRL_REMOVE_MAC   (4u)
 IOCTL Learning Table remove a MAC ID from table command. More...
 
#define ICSS_EMAC_LEARN_CTRL_INC_COUNTER   (5u)
 IOCTL Learning Table increment counters (for ageing) command. More...
 
#define ICSS_EMAC_LEARN_CTRL_INIT_TABLE   (6u)
 IOCTL Learning Table initialize command. More...
 
#define ICSS_EMAC_LEARN_CTRL_SET_PORTSTATE   (7u)
 IOCTL Learning Table set port state command. More...
 
ICSS-EMAC Statistics IOCTL Command Options

#define ICSS_EMAC_IOCTL_STAT_CTRL_GET   (0u)
 IOCTL Statistics get from PRU command. More...
 
#define ICSS_EMAC_IOCTL_STAT_CTRL_CLEAR   (1u)
 IOCTL Statistics clear all counters command. More...
 
ICSS-EMAC IOCTL Command for selecting a module

#define ICSS_EMAC_IOCTL_PORT_CTRL   (0u)
 IOCTL select port control APIs command. More...
 
#define ICSS_EMAC_IOCTL_LEARNING_CTRL   (1u)
 IOCTL select learning Table APIs command. More...
 
#define ICSS_EMAC_IOCTL_STORM_PREV_CTRL   (2u)
 IOCTL select Storm Prevention APIs command. More...
 
#define ICSS_EMAC_IOCTL_STATS_CTRL   (3u)
 IOCTL select Statistics APIs command. More...
 
#define ICSS_EMAC_IOCTL_PROMISCUOUS_CTRL   (4u)
 IOCTL select Promiscuous Mode APIs command. More...
 
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL   (5u)
 IOCTL select Multicast filtering APIs command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL   (6u)
 IOCTL select Vlan filtering APIs command. More...
 
#define ICSS_EMAC_IOCTL_PORT_FLUSH_CTRL   (7u)
 IOCTL select Port flush APIs command. More...
 
#define ICSS_EMAC_IOCTL_SPECIAL_UNICAST_MAC_CTRL   (8u)
 IOCTL select Special Unicast MAC address APIs command. More...
 
#define ICSS_EMAC_IOCTL_PORT_FWD_CTRL   (9u)
 IOCTL select Port Forwarding APIs command. More...
 
ICSS-EMAC Multicast Filtering IOCTL Command Options

#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ENABLE   (0u)
 IOCTL Multicast filter Control Enable command. More...
 
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_DISABLE   (1u)
 IOCTL Multicast filter Control Disable command. More...
 
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_OVERRIDE_HASHMASK   (2u)
 IOCTL Multicast filter Control override hashmask command. More...
 
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ADD_MACID   (3u)
 IOCTL Multicast filter Control allow MC MAC ID command. More...
 
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_REMOVE_MACID   (4u)
 IOCTL Multicast filter Control do not allow MC MAC ID command. More...
 
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_GET_DROPPED   (5u)
 IOCTL Multicast filter Control do not allow MC MAC ID command. More...
 
ICSS-EMAC VLAN Filtering IOCTL Command Options

#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ENABLE_CMD   (0u)
 IOCTL Vlan filter Control Enable command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_DISABLE_CMD   (1u)
 IOCTL Vlan filter Control Disable command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_ALL_CMD   (2u)
 IOCTL Vlan filter allow Untagged frames Host Receive command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_NAL_CMD   (3u)
 IOCTL Vlan filter do not allow Untagged frames Host Receive command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_ALL_CMD   (4u)
 IOCTL Vlan filter allow Priority Tag frames Host Receive command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_NAL_CMD   (5u)
 IOCTL Vlan filter do not allow Priority Tag frames Host Receive command. More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ADD_VID_CMD   (6u)
 IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, ADD VLAN ID to allow packet to host
More...
 
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_REMOVE_VID_CMD   (7u)
 IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, Remove VLAN ID to do not allow packet to host
More...
 
ICSS-EMAC Special Unicast MAC IOCTL Command Options

#define ICSS_EMAC_IOCTL_SPECIAL_UNICAST_MAC_CTRL_DISABLE_CMD   (0u)
 IOCTL Special Unicast MAC Disable command. More...
 
#define ICSS_EMAC_IOCTL_SPECIAL_UNICAST_MAC_CTRL_ENABLE_CMD   (1u)
 IOCTL Special Unicast MAC Enable command. More...
 
ICSS-EMAC Port Forwarding IOCTL Command Options

#define ICSS_EMAC_IOCTL_PORT_FWD_CTRL_ENABLE_CMD   (0u)
 IOCTL Port Forwarding Enable command. More...
 
#define ICSS_EMAC_IOCTL_PORT_FWD_CTRL_DISABLE_CMD   (1u)
 IOCTL Port Forwarding Disable command. More...
 

Typedefs

typedef struct ICSS_EMAC_Config_s * ICSS_EMAC_Handle
 Alias for ICSS EMAC Handle containing base addresses and modules. More...
 
typedef int32_t(* ICSS_EMAC_CallBack) (void *arg0, void *arg1, void *arg2)
 Definition for a generic callback function used in ICSS-EMAC.
While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig. More...
 

Functions

void ICSS_EMAC_init (void)
 This function initializes the ICSS_EMAC module. More...
 
void ICSS_EMAC_deinit (void)
 This function de-initializes the ICSS_EMAC module. More...
 
void ICSS_EMAC_Params_init (ICSS_EMAC_Params *params)
 Initialize the parmeters data structure with defaults. More...
 
ICSS_EMAC_Handle ICSS_EMAC_open (uint32_t idx, const ICSS_EMAC_Params *params)
 API to initialize and configure ICSS in MAC/Switch Mode. More...
 
void ICSS_EMAC_close (ICSS_EMAC_Handle icssEmacHandle)
 API to stop MAC/Switch Mode. More...
 
int32_t ICSS_EMAC_ioctl (ICSS_EMAC_Handle icssEmacHandle, uint32_t ioctlCommand, uint8_t portNo, void *ioctlParams)
 IOCTL Function for ICSS EMAC. More...
 
int32_t ICSS_EMAC_rxPktGet (ICSS_EMAC_RxArgument *rxArg, void *userArg)
 Retrieves a frame from a host queue and copies it in the allocated stack buffer. More...
 
int32_t ICSS_EMAC_rxPktInfo (ICSS_EMAC_Handle icssEmacHandle, int32_t *portNumber, int32_t *queueNumber)
 API to retrieve the information about the received frame which is then used to dequeue the frame from the host queues. More...
 
int32_t ICSS_EMAC_txPacket (const ICSS_EMAC_TxArgument *txArg, void *userArg)
 API to queue a frame which has to be transmitted on the specified port queue. More...