AM263Px MCU+ SDK  26.00.00
VTM Functions

Introduction

Functions

int32_t SDL_VTM_initTs (const SDL_VTM_configTs *pConfig)
 VTM Temperature sensor initialization. More...
 
int32_t SDL_VTM_getTemp (SDL_VTM_InstTs instance, uint32_t *pTempVal)
 Read VTM Temperature sensor values in degree celcius. More...
 
int32_t SDL_VTM_setAlertTemp (SDL_VTM_InstTs instance, int32_t alert_th_hot, int32_t alert_th_cold)
 Set thresholds for temperature alerts. More...
 
int32_t SDL_VTM_setTShutTemp (SDL_VTM_InstTs instance, int32_t tshut_th_hot, int32_t tshut_th_cold)
 Set thresholds for temperature Shutdown. More...
 
int32_t SDL_VTM_setClearInterrupts (SDL_VTM_InstTs instance, uint8_t hotintr, uint8_t coldintr, uint8_t lowthresholdintr)
 API to set/Clear masks for generating interrupts. More...
 
int32_t SDL_VTM_getSensorStatus (SDL_VTM_Stat_val *pStat_val)
 Read VTM Temperature sensor status. More...
 
void SDL_VTM_enableTs (uint32_t sensorSelect, uint8_t delay)
 Enable Required Temperature sensors. More...
 
void SDL_VTM_enableTc (void)
 Enable Temperature Controller. More...
 
void SDL_VTM_disableTc (void)
 Disable Temperature Controller. More...
 
int32_t SDL_VTM_getStaticRegistersTs (SDL_VTM_staticRegsTs *pStaticRegs)
 VTM Temperature sensor readback Static configuration registers. More...
 
int32_t SDL_VTM_enableESMWarmReset (SDL_VTM_InstTs instance)
 Enable Warm Reset Generation. More...
 

Function Documentation

◆ SDL_VTM_initTs()

int32_t SDL_VTM_initTs ( const SDL_VTM_configTs pConfig)

VTM Temperature sensor initialization.

This function executes a VTM Temperature sensor initialization of the specified type for a specific VTM TS instance. VTM is a feature that is used to set control register, thermal shutdown range, Threshold values and interrupts

Parameters
pConfig[IN] Pointer to VTM TS configuration (optional)
Returns
The SDL error code for the API. If pConfig is NULL: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_getTemp()

int32_t SDL_VTM_getTemp ( SDL_VTM_InstTs  instance,
uint32_t *  pTempVal 
)

Read VTM Temperature sensor values in degree celcius.

Parameters
instance[IN] VTM Temperature sensor instance
pTempVal[OUT] Pointer to Temperature sensor values
Returns
The SDL error code for the API. If pTempVal is NULL: SDL_EBADARGS If instance is invalid: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_setAlertTemp()

int32_t SDL_VTM_setAlertTemp ( SDL_VTM_InstTs  instance,
int32_t  alert_th_hot,
int32_t  alert_th_cold 
)

Set thresholds for temperature alerts.

Parameters
instance[IN] VTM Temperature sensor instance
alert_th_hot[IN] Alert hot temperature in milli degree celcius
alert_th_cold[IN] Alert cold temperature in milli degree celcius
Returns
The SDL error code for the API. If instance is invalid: SDL_EBADARGS If temperatures are invalid: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_setTShutTemp()

int32_t SDL_VTM_setTShutTemp ( SDL_VTM_InstTs  instance,
int32_t  tshut_th_hot,
int32_t  tshut_th_cold 
)

Set thresholds for temperature Shutdown.

Parameters
instance[IN] VTM Temperature sensor instance
tshut_th_hot[IN] Shutdown hot temperature in milli degree celcius
tshut_th_cold[IN] Shutdown cold temperature in milli degree celcius
Returns
The SDL error code for the API. If instance is invalid: SDL_EBADARGS If temperatures are invalid: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_setClearInterrupts()

int32_t SDL_VTM_setClearInterrupts ( SDL_VTM_InstTs  instance,
uint8_t  hotintr,
uint8_t  coldintr,
uint8_t  lowthresholdintr 
)

API to set/Clear masks for generating interrupts.

Parameters
instance[IN] VTM Temperature sensor instance
hotintr[IN] Enable/disable hot interrupt.
coldintr[IN] Enable/disable cold interrupt.
lowthresholdintr[IN] Enable/disable low treshold interrupt.
Returns
The SDL error code for the API. If instance is invalid: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_getSensorStatus()

int32_t SDL_VTM_getSensorStatus ( SDL_VTM_Stat_val pStat_val)

Read VTM Temperature sensor status.

Parameters
pStat_val[OUT] Pointer to Temperature sensor status
Returns
The SDL error code for the API. If pStat_val are NULL: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_enableTs()

void SDL_VTM_enableTs ( uint32_t  sensorSelect,
uint8_t  delay 
)

Enable Required Temperature sensors.

Parameters
sensorSelect[IN] Enable configured sensors
delay[IN] delay between each read of temperature sensor. 0 is not valid value.

◆ SDL_VTM_enableTc()

void SDL_VTM_enableTc ( void  )

Enable Temperature Controller.

◆ SDL_VTM_disableTc()

void SDL_VTM_disableTc ( void  )

Disable Temperature Controller.

◆ SDL_VTM_getStaticRegistersTs()

int32_t SDL_VTM_getStaticRegistersTs ( SDL_VTM_staticRegsTs pStaticRegs)

VTM Temperature sensor readback Static configuration registers.

Parameters
pStaticRegs[OUT] Pointer to VTM TS static register
Returns
The SDL error code for the API. If pStaticRegs is NULL: SDL_EBADARGS If instance is invalid: SDL_EBADARGS Success: SDL_PASS

◆ SDL_VTM_enableESMWarmReset()

int32_t SDL_VTM_enableESMWarmReset ( SDL_VTM_InstTs  instance)

Enable Warm Reset Generation.

Parameters
instance[IN] VTM Temperature sensor instance
Returns
The SDL error code for the API. If instance is invalid: SDL_EBADARGS Success: SDL_PASS