AM263Px MCU+ SDK  26.00.00

Introduction

Functions

int32_t SDL_STC_getStatus (SDL_STC_Inst instance)
 This API is used to get status for STC result. More...
 
int32_t SDL_STC_selfTest (SDL_STC_Inst instance, SDL_STC_TestType testType, SDL_STC_Config *pConfig)
 This API is used to run the STC module. More...
 
static int32_t SDL_STC_configure (SDL_STC_Inst instance, SDL_STC_Config *pConfig, SDL_STC_TestType testType)
 This API is used to configure STC module. More...
 
static int32_t SDL_STC_runTest (SDL_STC_Inst instance)
 This API is used to enable the STC module. More...
 
static void SDL_STC_delay (int32_t count)
 This API is used to provide delay for processor core. More...
 
static void SDL_Delay (void)
 This API is used to execute asm nop operation. More...
 
void SDL_STC_dspInit (void)
 This API is used to initialize all the required configuration in RCM & CTRL Module for performing DSP STC. More...
 
static void SDL_STC_resetCauseClearR5F0 (void)
 This API is used to clear the reset cause bits for processor core. More...
 
static void SDL_STC_resetCauseClearR5F1 (void)
 

Function Documentation

◆ SDL_STC_getStatus()

int32_t SDL_STC_getStatus ( SDL_STC_Inst  instance)

This API is used to get status for STC result.

Parameters
instanceHolds the instance for STC module.

NOTE: This API informes only first that we should run STC test or not.if it will return that STC has been Done, then programe will be terminated simply from here.

◆ SDL_STC_selfTest()

int32_t SDL_STC_selfTest ( SDL_STC_Inst  instance,
SDL_STC_TestType  testType,
SDL_STC_Config pConfig 
)

This API is used to run the STC module.

Parameters
instanceHolds the instance for STC module.
testTypetestType that in wwhich mode test need to be run.
pConfigConfiguration that need to be run.

NOTE: This API informes only first that we should run STC test or not.if it will return that STC has been Done, then programe will be terminated simply from here. There nothing will be returned as core will be reset after run this API. testType that in wwhich mode test need to be run.

◆ SDL_STC_configure()

static int32_t SDL_STC_configure ( SDL_STC_Inst  instance,
SDL_STC_Config pConfig,
SDL_STC_TestType  testType 
)
static

This API is used to configure STC module.

Parameters
instanceHolds the instance for STC module.
pConfigpointer to the STC config structure
testTypeEnum value for specifying testType

NOTE: There are two types of testType

  1. SDL_STC_TEST-> FOR THIS TEST STATUS SHOULD BE PASS.
  2. SDL_STC_NEG_TEST-> FOR THIS TEST STATUS SHOULD BE FAIL.

◆ SDL_STC_runTest()

static int32_t SDL_STC_runTest ( SDL_STC_Inst  instance)
static

This API is used to enable the STC module.

Parameters
instanceHolds the instance for STC module.

◆ SDL_STC_delay()

static void SDL_STC_delay ( int32_t  count)
static

This API is used to provide delay for processor core.

◆ SDL_Delay()

static void SDL_Delay ( void  )
static

This API is used to execute asm nop operation.

◆ SDL_STC_dspInit()

void SDL_STC_dspInit ( void  )

This API is used to initialize all the required configuration in RCM & CTRL Module for performing DSP STC.

◆ SDL_STC_resetCauseClearR5F0()

static void SDL_STC_resetCauseClearR5F0 ( void  )
static

This API is used to clear the reset cause bits for processor core.

◆ SDL_STC_resetCauseClearR5F1()

static void SDL_STC_resetCauseClearR5F1 ( void  )
static