AM263Px MCU+ SDK  26.00.00

Introduction

Functions

int32_t SDL_RTI_chkWindowSize (uint32_t dwwdWindowSize)
 This API will check the Window Size for DWWD. More...
 
int32_t SDL_RTI_chkReaction (uint32_t dwwdReaction)
 This API will check the reaction to perform when error is detected from DWWD. More...
 
int32_t SDL_RTI_getWindowSize (uint32_t baseAddr, uint32_t *pWinSize)
 This API will return current configured Window Size. More...
 
int32_t SDL_RTI_setPreload (uint32_t baseAddr, uint32_t dwwdPreloadVal)
 Set DWWD preload value. From this value down counter starts down counting. More...
 
int32_t SDL_RTI_getPreload (uint32_t baseAddr, uint32_t *pPreloadVal)
 This API will return current configured Preload value. More...
 

Function Documentation

◆ SDL_RTI_chkWindowSize()

int32_t SDL_RTI_chkWindowSize ( uint32_t  dwwdWindowSize)

This API will check the Window Size for DWWD.

Parameters
dwwdWindowSizevariable which holds window size which should be verified
Returns
status Success of the window configuration
  • Success: SDL_PASS
  • Fail : SDL_EFAIL

◆ SDL_RTI_chkReaction()

int32_t SDL_RTI_chkReaction ( uint32_t  dwwdReaction)

This API will check the reaction to perform when error is detected from DWWD.

Parameters
dwwdReactionVariable which holds the reaction to be verified.
Returns
status Success of the window configuration
  • Success: SDL_PASS
  • Fail : SDL_EFAIL

◆ SDL_RTI_getWindowSize()

int32_t SDL_RTI_getWindowSize ( uint32_t  baseAddr,
uint32_t *  pWinSize 
)

This API will return current configured Window Size.

Parameters
baseAddrBase Address of the RTI instance.
pWinSizepointer to Configured Window Size. Refer macro RTI_WindowSize_t
Returns
status Success of the window configuration
  • Success: SDL_PASS
  • Fail : SDL_EFAIL

◆ SDL_RTI_setPreload()

int32_t SDL_RTI_setPreload ( uint32_t  baseAddr,
uint32_t  dwwdPreloadVal 
)

Set DWWD preload value. From this value down counter starts down counting.

Parameters
baseAddrBase Address of the RTI instance.
dwwdPreloadValDown counter preload value. Refer DWWD Down Counter Overview.
Returns
status Success of the window configuration
  • Success: SDL_PASS
  • Fail : SDL_EFAIL

◆ SDL_RTI_getPreload()

int32_t SDL_RTI_getPreload ( uint32_t  baseAddr,
uint32_t *  pPreloadVal 
)

This API will return current configured Preload value.

Parameters
baseAddrBase Address of the RTI instance.
pPreloadValpointer to current preload value
Returns
status Success of the window configuration
  • Success: SDL_PASS
  • Fail : SDL_EFAIL