AM263Px MCU+ SDK  26.00.00
APIs for timer setup and control

Introduction

This module define's generic APIs to configure and control a timer Depending on the SOC there can be different timer implementation's

For more details and example usage, see Timer

Timer is used by Clock to generate system ticks.

Currently below timer implementations are supported

Data Structures

struct  TimerP_Params
 Parameters for TimerP_setup. More...
 

Functions

void TimerP_Params_init (TimerP_Params *params)
 Set default value for TimerP_Params. More...
 
void TimerP_setup (uint32_t baseAddr, TimerP_Params *params)
 Setup timer but does not start it. More...
 
void TimerP_start (uint32_t baseAddr)
 Start timer. More...
 
void TimerP_stop (uint32_t baseAddr)
 Stop timer. More...
 
uint32_t TimerP_getCount (uint32_t baseAddr)
 Get timer current count. More...
 
uint32_t TimerP_getReloadCount (uint32_t baseAddr)
 Get timer reload count. More...
 
void TimerP_clearOverflowInt (uint32_t baseAddr)
 Clear timer overflow interrupt. More...
 
uint32_t TimerP_isOverflowed (uint32_t baseAddr)
 Check if timer is overflowed. More...
 

Macros

#define TIME_IN_MICRO_SECONDS   (1000000U)
 
#define MAX_TIMER_COUNT_VALUE   (0xFFFFFFFFU)
 
#define TIME_IN_MILLI_SECONDS   (1000U)
 
#define TIME_IN_NANO_SECONDS   (1000000000U)
 
#define TIMERP_SHIFT_BY_EIGHT   (8U)
 
#define MAX_NUMBER_OF_CYCLES   (0xFFFFFFFFU)
 
#define MAX_NUMBER_OF_COUNT   (0xFFFFFFFFU)
 

Macro Definition Documentation

◆ TIME_IN_MICRO_SECONDS

#define TIME_IN_MICRO_SECONDS   (1000000U)

Macro defines the time in micro seconds

◆ MAX_TIMER_COUNT_VALUE

#define MAX_TIMER_COUNT_VALUE   (0xFFFFFFFFU)

Macro defines the maximum timer count value

◆ TIME_IN_MILLI_SECONDS

#define TIME_IN_MILLI_SECONDS   (1000U)

Macro defines the time in milli seconds

◆ TIME_IN_NANO_SECONDS

#define TIME_IN_NANO_SECONDS   (1000000000U)

Macro defines the time in nano seconds

◆ TIMERP_SHIFT_BY_EIGHT

#define TIMERP_SHIFT_BY_EIGHT   (8U)

Macro defines the shift by eight

◆ MAX_NUMBER_OF_CYCLES

#define MAX_NUMBER_OF_CYCLES   (0xFFFFFFFFU)

Macro defines the maximum number of cycles

◆ MAX_NUMBER_OF_COUNT

#define MAX_NUMBER_OF_COUNT   (0xFFFFFFFFU)

Macro defines the maximum number of count

Function Documentation

◆ TimerP_Params_init()

void TimerP_Params_init ( TimerP_Params params)

Set default value for TimerP_Params.

Parameters
params[out] timer parameters initalized to default

◆ TimerP_setup()

void TimerP_setup ( uint32_t  baseAddr,
TimerP_Params params 
)

Setup timer but does not start it.

Parameters
baseAddr[in] HW timer base addresss
params[in] timer parameters

◆ TimerP_start()

void TimerP_start ( uint32_t  baseAddr)

Start timer.

Parameters
baseAddr[in] HW timer base addresss

◆ TimerP_stop()

void TimerP_stop ( uint32_t  baseAddr)

Stop timer.

Parameters
baseAddr[in] HW timer base addresss

◆ TimerP_getCount()

uint32_t TimerP_getCount ( uint32_t  baseAddr)

Get timer current count.

Parameters
baseAddr[in] HW timer base addresss
Returns
current timer count value

◆ TimerP_getReloadCount()

uint32_t TimerP_getReloadCount ( uint32_t  baseAddr)

Get timer reload count.

Parameters
baseAddr[in] HW timer base addresss
Returns
reload count value

◆ TimerP_clearOverflowInt()

void TimerP_clearOverflowInt ( uint32_t  baseAddr)

Clear timer overflow interrupt.

Parameters
baseAddr[in] HW timer base addresss

◆ TimerP_isOverflowed()

uint32_t TimerP_isOverflowed ( uint32_t  baseAddr)

Check if timer is overflowed.

Note
make sure to clear overflow status TimerP_clearOverflowInt
Parameters
baseAddr[in] HW timer base addresss