AM263Px MCU+ SDK  26.00.00

Introduction

Sub Modules

 CPDMA Configuration
 
 CPDMA Packet Definitions
 

Functions

void EnetCpdma_initRxChParams (EnetCpdma_OpenRxChPrms *pRxChPrms)
 Initialize RX channel open parameters. More...
 
EnetDma_RxChHandle EnetCpdma_openRxCh (EnetDma_Handle hDma, const EnetCpdma_OpenRxChPrms *pRxChPrms)
 Enet DMA open RX channel. More...
 
int32_t EnetCpdma_closeRxCh (EnetDma_RxChHandle hRxCh, EnetDma_PktQ *fq, EnetDma_PktQ *cq)
 Enet DMA close RX channel. More...
 
void EnetCpdma_initTxChParams (EnetCpdma_OpenTxChPrms *pTxChPrms)
 Initialize TX channel open parameters. More...
 
EnetDma_TxChHandle EnetCpdma_openTxCh (EnetDma_Handle hDma, const EnetCpdma_OpenTxChPrms *pTxChPrms)
 Enet DMA open TX channel. More...
 
int32_t EnetCpdma_closeTxCh (EnetDma_TxChHandle hTxCh, EnetDma_PktQ *fq, EnetDma_PktQ *cq)
 Enet DMA close TX channel. More...
 
EnetDma_Handle EnetCpdma_open (Enet_Type enetType, uint32_t instId, const EnetDma_Cfg *dmaCfg, uint32_t appCoreId)
 Set default data path parameters. More...
 
EnetDma_Handle EnetCpdma_restoreCtxt (Enet_Type enetType, uint32_t instId, uint32_t appCoreId)
 Open DMA with default data path parameters. More...
 
int32_t EnetCpdma_close (EnetDma_Handle hEnetDma)
 Close Enet DMA (data path). More...
 
int32_t EnetCpdma_saveCtxt (EnetDma_Handle hEnetDma)
 Saves and closes Enet DMA (data path). More...
 
int32_t EnetCpdma_rxThreshIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Rx Threshold interrupt service routine. More...
 
int32_t EnetCpdma_rxIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Rx interrupt service routine. More...
 
int32_t EnetCpdma_txIsr (EnetDma_Handle hEnetDma)
 ENET CPDMA Tx interrupt service routine. More...
 
int32_t EnetCpdma_miscIsrGetStatus (EnetDma_Handle hEnetDma, uint32_t *pStatusMask)
 ENET CPDMA Miscellaneous interrupt service routine. More...
 
int32_t EnetCpdma_ackMiscIsr (EnetDma_Handle hEnetDma)
 
void EnetCpdma_initParams (EnetDma_Cfg *pDmaConfig)
 Initialize CPDMA config params. More...
 

Typedefs

typedef EnetQ EnetDma_PktQ
 Packet queue. More...
 

Macros

#define ENET_CPDMA_CPSW_MAX_SG_LIST   (4U)
 
#define ENET_CPDMA_CSUM_START_BYTE_SHIFT   (16U)
 
#define ENET_CPDMA_CSUM_START_BYTE_MASK   (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_START_BYTE_SHIFT)
 
#define ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT   (24U)
 
#define ENET_CPDMA_CSUM_RESULT_BYTE_MASK   (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT)
 
#define ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT   (0U)
 
#define ENET_CPDMA_CSUM_BYTE_COUNT_MASK   (((uint32_t) 0x3FFU) << ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT)
 
#define ENET_CPDMA_GET_CSUM_RESULT_BYTE(chkSumInfo)    ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_RESULT_BYTE)
 
#define ENET_CPDMA_GET_CSUM_START_BYTE(chkSumInfo)    ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_START_BYTE)
 
#define ENET_CPDMA_GET_CSUM_BYTE_COUNT(chkSumInfo)    ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_BYTE_COUNT)
 

Enet CPDMA instance configuration

Configuration macros for Enet CPDMA module.

#define ENET_CPDMA_CPSW_MAX_TX_CH   (8U)
 Maximum number of CPSW TX DMA channels. More...
 
#define ENET_CPDMA_CPSW_MAX_RX_CH   (8U)
 Maximum number of CPSW RX DMA channels. More...
 

Enet DMA driver opaque handles

Enet DMA configuration structure.

Opaque handle typedefs for Enet DMA driver objects.

typedef void(* EnetDma_PktNotifyCb) (void *cbArg)
 Function pointer type for packet notify call back. More...
 

Macro Definition Documentation

◆ ENET_CPDMA_CPSW_MAX_TX_CH

#define ENET_CPDMA_CPSW_MAX_TX_CH   (8U)

Maximum number of CPSW TX DMA channels.

◆ ENET_CPDMA_CPSW_MAX_RX_CH

#define ENET_CPDMA_CPSW_MAX_RX_CH   (8U)

Maximum number of CPSW RX DMA channels.

◆ ENET_CPDMA_CPSW_MAX_SG_LIST

#define ENET_CPDMA_CPSW_MAX_SG_LIST   (4U)

Maximum number of scatter gather segements supported in a packet

◆ ENET_CPDMA_CSUM_START_BYTE_SHIFT

#define ENET_CPDMA_CSUM_START_BYTE_SHIFT   (16U)

Utilities to read the ChksumInfo fields

◆ ENET_CPDMA_CSUM_START_BYTE_MASK

#define ENET_CPDMA_CSUM_START_BYTE_MASK   (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_START_BYTE_SHIFT)

◆ ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT

#define ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT   (24U)

◆ ENET_CPDMA_CSUM_RESULT_BYTE_MASK

#define ENET_CPDMA_CSUM_RESULT_BYTE_MASK   (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT)

◆ ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT

#define ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT   (0U)

◆ ENET_CPDMA_CSUM_BYTE_COUNT_MASK

#define ENET_CPDMA_CSUM_BYTE_COUNT_MASK   (((uint32_t) 0x3FFU) << ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT)

◆ ENET_CPDMA_GET_CSUM_RESULT_BYTE

#define ENET_CPDMA_GET_CSUM_RESULT_BYTE (   chkSumInfo)     ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_RESULT_BYTE)

◆ ENET_CPDMA_GET_CSUM_START_BYTE

#define ENET_CPDMA_GET_CSUM_START_BYTE (   chkSumInfo)     ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_START_BYTE)

◆ ENET_CPDMA_GET_CSUM_BYTE_COUNT

#define ENET_CPDMA_GET_CSUM_BYTE_COUNT (   chkSumInfo)     ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_BYTE_COUNT)

Typedef Documentation

◆ EnetDma_PktNotifyCb

typedef void(* EnetDma_PktNotifyCb) (void *cbArg)

Function pointer type for packet notify call back.

This is called by driver when packet is received on the RX channel or transmission completed from TX channel.

◆ EnetDma_PktQ

Packet queue.

A queue of packets, which are used for managing the packets given to the DMA driver by an application. It can also be used by the translation or application layer to manage free packets pools.

Function Documentation

◆ EnetCpdma_initRxChParams()

void EnetCpdma_initRxChParams ( EnetCpdma_OpenRxChPrms pRxChPrms)

Initialize RX channel open parameters.

Initializes RX channel parameters with default values. Refer to SOC DMA specific RX channel config structure for specific config details.

Parameters
pRxChPrmsRX channel configuration parameters.

◆ EnetCpdma_openRxCh()

EnetDma_RxChHandle EnetCpdma_openRxCh ( EnetDma_Handle  hDma,
const EnetCpdma_OpenRxChPrms pRxChPrms 
)

Enet DMA open RX channel.

Opens the Enet DMA RX channel based on the channel parameters. This function configures the DMA channel. This also configures event if notifyCb is not null. Refer to SOC DMA specific RX channel config structure for specific config details.

Enet DMA is peripheral-aware as peripherals in a given SoC may need different handling, i.e. DMA descriptor's extra fields having different meaning for two peripherals using same DMA engine. This peripheral-awareness is given to the RX channel/flow via EnetDma_Handle passed at open time.

Parameters
hDmaEnet DMA handle
pRxChPrmsRX channel configuration parameters. This parameter can't be NULL.
Returns
RX channel opaque handle if opened. Otherwise, NULL.

◆ EnetCpdma_closeRxCh()

int32_t EnetCpdma_closeRxCh ( EnetDma_RxChHandle  hRxCh,
EnetDma_PktQ fq,
EnetDma_PktQ cq 
)

Enet DMA close RX channel.

Closes the Enet DMA RX channel and frees all associated resources. During close operation, we flush FQ taking all DMA descriptors with packet submitted in advance for reception and return to app. Also we retrieve all packets from the CQ (packets received between last EnetDma_retrieveRxPktQ() function call) and return those to app. App doesn't need to call function EnetDma_retrieveRxPktQ() explicitly to retrieve these packets.

Parameters
hRxCh[IN] Enet DMA channel handle. This parameter can't be NULL.
fq[OUT] Pointer to EnetDma_PktQ structure where packets from FQ (submitted for reception) are retrieved and returned to application. This parameter can't be NULL.
cq[OUT] Pointer to EnetDma_PktQ structure where packets from CQ (received packets) are retrieved and returned to application. This parameter can't be NULL.
Returns
Enet_ErrorCodes

◆ EnetCpdma_initTxChParams()

void EnetCpdma_initTxChParams ( EnetCpdma_OpenTxChPrms pTxChPrms)

Initialize TX channel open parameters.

Initializes TX channel open parameters with default values. Refer to SOC DMA specific RX channel config structure for specific config details.

Parameters
pTxChPrmsTX channel configuration parameters.

◆ EnetCpdma_openTxCh()

EnetDma_TxChHandle EnetCpdma_openTxCh ( EnetDma_Handle  hDma,
const EnetCpdma_OpenTxChPrms pTxChPrms 
)

Enet DMA open TX channel.

Opens the DMA TX DMA channel based on the channel parameters. This function open TX channel using chNum provided in EnetDma_OpenTxChPrms() and configures TX channel. This also configures event if notifyCb is not null. Refer to SOC DMA specific RX channel config structure for specific config details.

Enet DMA is peripheral-aware as peripherals in a given SoC may need different handling, i.e. DMA descriptor's extra fields having different meaning for two peripherals using same DMA engine. This peripheral-awareness is given to the TX channel via EnetDma_Handle passed at open time.

Parameters
hDmaEnet DMA handle
pTxChPrmsTX channel configuration parameters. This parameter can't be NULL.
Returns
TX channel opaque handle if opened. Otherwise, NULL.

◆ EnetCpdma_closeTxCh()

int32_t EnetCpdma_closeTxCh ( EnetDma_TxChHandle  hTxCh,
EnetDma_PktQ fq,
EnetDma_PktQ cq 
)

Enet DMA close TX channel.

Closes the Enet DMA TX channel and frees all associated resources. During close operation, we flush FQ taking all DMA descriptors with packet submitted but not yet transmitted and return to app. Also we retrieve all packets from the CQ (transmission completed packets) and return those to app. App doesn't need to call EnetDma_retrieveTxPktQ() explicitly to retrieve these packets.

Parameters
hTxCh[IN] Enet DMA TX Channel handle. This parameter can't be NULL.
fq[OUT] Pointer to EnetDma_PktQ structure where packets from FQ (TX ready - submitted for transmission) are retrieved and returned to application. This parameter can't be NULL.
cq[OUT] Pointer to EnetDma_PktQ structure where packets from CQ (TX free - transmitted packets) are retrieved and returned to application. This parameter can't be NULL.
Returns
Enet_ErrorCodes

◆ EnetCpdma_open()

EnetDma_Handle EnetCpdma_open ( Enet_Type  enetType,
uint32_t  instId,
const EnetDma_Cfg dmaCfg,
uint32_t  appCoreId 
)

Set default data path parameters.

Parameters
enetType[IN] Enet Peripheral type
instId[IN] Enet Peripheral instance id
dmaCfg[IN] DMA module (data path) configuration pointer.
appCoreId[IN] Application core Id
Return values
EnetDMA handle if opened. Otherwise, NULL.

◆ EnetCpdma_restoreCtxt()

EnetDma_Handle EnetCpdma_restoreCtxt ( Enet_Type  enetType,
uint32_t  instId,
uint32_t  appCoreId 
)

Open DMA with default data path parameters.

Parameters
enetType[IN] Enet Peripheral type
instId[IN] Enet Peripheral instance id
appCoreId[IN] Application core Id
Return values
EnetDMA handle if opened. Otherwise, NULL.

◆ EnetCpdma_close()

int32_t EnetCpdma_close ( EnetDma_Handle  hEnetDma)

Close Enet DMA (data path).

Parameters
hEnetDma[IN] DMA handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_saveCtxt()

int32_t EnetCpdma_saveCtxt ( EnetDma_Handle  hEnetDma)

Saves and closes Enet DMA (data path).

Parameters
hEnetDma[IN] DMA handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_rxThreshIsr()

int32_t EnetCpdma_rxThreshIsr ( EnetDma_Handle  hEnetDma)

ENET CPDMA Rx Threshold interrupt service routine.

Processes Rx Threshold interrupt. This function retrieves the received packets from the linked CPPI descriptors and passes them to the receive queue when the number of received descriptors exceed the threshold

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_rxIsr()

int32_t EnetCpdma_rxIsr ( EnetDma_Handle  hEnetDma)

ENET CPDMA Rx interrupt service routine.

Processes Rx interrupt. This function retrieves the received packets from the linked CPPI descriptors and passes them to the receive queue when one or more packets has been received

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_txIsr()

int32_t EnetCpdma_txIsr ( EnetDma_Handle  hEnetDma)

ENET CPDMA Tx interrupt service routine.

Processes Tx interrupt. This function retrieves the completed Tx packets from the linked CPPI descriptors and passes them to the free queue when one or more packets have been transmitted.

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
Returns
Enet_ErrorCodes

◆ EnetCpdma_miscIsrGetStatus()

int32_t EnetCpdma_miscIsrGetStatus ( EnetDma_Handle  hEnetDma,
uint32_t *  pStatusMask 
)

ENET CPDMA Miscellaneous interrupt service routine.

Processes Miscellaneous interrupt. This function extracts the intrrupt status bit masks from MMR and pass it to the caller to process all masked interrupts.

Requirement:

Parameters
hEnetDma[IN] Enet DMA Handle
pStatusMask[IN] pointer to the interrupt status bit mask
Returns
Enet_ErrorCodes

◆ EnetCpdma_ackMiscIsr()

int32_t EnetCpdma_ackMiscIsr ( EnetDma_Handle  hEnetDma)

EnetCpdma_ackMiscIsr
CPSW CPDMA Miscellaneous ISR ACK.

Parameters
[in]hEnetDma
Return values
ENET_SOK

◆ EnetCpdma_initParams()

void EnetCpdma_initParams ( EnetDma_Cfg pDmaConfig)

Initialize CPDMA config params.

Initialize CPDMA config params to default values

Requirement:

Parameters
pDmaConfig[IN] pointer to the config structure