AM263Px MCU+ SDK  26.00.00

Introduction

TI DP83TG721 Ethernet PHY.

Data Structures

struct  Dp83tg721_Cfg
 DP83TG721 PHY configuration parameters. More...
 

Functions

void Dp83tg721_initCfg (Dp83tg721_Cfg *cfg)
 Initialize DP83TC811 PHY specific config params. More...
 

Macros

#define DP83TG721_LED_NUM   (2U)
 Number of LEDs available in the PHY. More...
 

Macro Definition Documentation

◆ DP83TG721_LED_NUM

#define DP83TG721_LED_NUM   (2U)

Number of LEDs available in the PHY.

Function Documentation

◆ Dp83tg721_initCfg()

void Dp83tg721_initCfg ( Dp83tg721_Cfg cfg)

Initialize DP83TC811 PHY specific config params.

Initializes the DP83TC811 PHY specific configuration parameters.

Parameters
cfgDP83TC811 PHY config structure pointer