AM263Px MCU+ SDK  26.00.00

Introduction

This module contains APIs to program and use the MCSPI LLD module. The APIs can be used by other drivers to get access to MCSPI and also by application to initiate data transfer operation.

Sub Modules

 APIs for MCSPI DMA mode
 

Files

file  mcspi_lld.h
 MCSPI LLD Driver API/interface file.
 

Data Structures

struct  MCSPI_Transaction
 Data structure used with MCSPI_transfer() More...
 
struct  MCSPI_ExtendedParams
 Data structure used with MCSPI_lld_read(), MCSPI_lld_readIntr(), MCSPI_lld_readDma(), MCSPI_lld_write(), MCSPI_lld_writeIntr, MCSPI_lld_writeDma, MCSPI_lld_readWrite(), MCSPI_lld_readWriteIntr(), MCSPI_lld_readWriteDma(). MCSPI ExtendedParams to be used in case, one's don't want to use default parameters, else pass NULL. More...
 
struct  MCSPI_ChConfig
 MCSPI configuration parameters for the channel. More...
 
struct  MCSPI_ChObject
 MCSPI channel object. More...
 
struct  MCSPILLD_InitObject
 MCSPI driver initialization object. More...
 
struct  MCSPILLD_Object
 MCSPI driver object. More...
 

Functions

void MCSPI_reset (uint32_t baseAddr)
 
void MCSPI_clearAllIrqStatus (uint32_t baseAddr)
 
void MCSPI_stop (MCSPILLD_Handle hMcspi, MCSPI_ChObject *chObj, uint32_t chNum)
 
void MCSPI_setChDataSize (uint32_t baseAddr, MCSPI_ChObject *chObj, uint32_t dataSize, uint32_t csDisable)
 
static void MCSPI_intrStatusClear (const MCSPI_ChObject *chObj, uint32_t baseAddr, uint32_t intFlags)
 
int32_t MCSPI_lld_init (MCSPILLD_Handle hMcspi)
 This API Initializes the McSPI instance. More...
 
int32_t MCSPI_lld_initDma (MCSPILLD_Handle hMcspi)
 This API Initializes the McSPI instance in DMA Mode. More...
 
int32_t MCSPI_lld_deInit (MCSPILLD_Handle hMcspi)
 This API De-Initializes the McSPI instance. More...
 
int32_t MCSPI_lld_deInitDma (MCSPILLD_Handle hMcspi)
 This API De-Initializes the McSPI instance in DMA mode. More...
 
int32_t MCSPI_lld_write (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API writes data to the McSPI instance in Polling mode. More...
 
int32_t MCSPI_lld_writeIntr (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API writes data to the McSPI instance in Interrupt mode. More...
 
int32_t MCSPI_lld_writeDma (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API writes data to the McSPI instance in DMA mode. More...
 
int32_t MCSPI_lld_read (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API reads data from the McSPI instance in Polling mode. More...
 
int32_t MCSPI_lld_readIntr (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API reads data from the McSPI instance in Interrupt mode. More...
 
int32_t MCSPI_lld_readDma (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API reads data from the McSPI instance in DMA mode. More...
 
int32_t MCSPI_lld_readWrite (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API reads writes data from the McSPI instance in polling mode. More...
 
int32_t MCSPI_lld_readWriteIntr (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API reads writes data from the McSPI instance in Interrupt mode. More...
 
int32_t MCSPI_lld_readWriteDma (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams)
 This API reads writes data from the McSPI instance in DMA mode. More...
 
int32_t MCSPI_lld_readWriteCancel (MCSPILLD_Handle hMcspi)
 This API cancels current McSPI transfer. More...
 
int32_t MCSPI_lld_readWriteDmaCancel (MCSPILLD_Handle hMcspi)
 This API cancels current McSPI transfer in DMA mode. More...
 
int32_t MCSPI_lld_transfer (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction)
 This API transfers data from the McSPI instance in Polling mode. More...
 
int32_t MCSPI_lld_transferIntr (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction)
 This API reads data from the McSPI instance in Interrupt mode. More...
 
int32_t MCSPI_lld_transferDma (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction)
 This API reads data from the McSPI instance in DMA mode. More...
 
void MCSPI_lld_controllerIsr (void *args)
 This is the McSPI Controller ISR and can be used as IRQ handler in Controller mode. More...
 
void MCSPI_lld_peripheralIsr (void *args)
 This is the McSPI Peripheral ISR and can be used as IRQ handler in Peripheral mode. More...
 
int32_t MCSPI_lld_getState (MCSPILLD_Handle hMcspi)
 This API returns the driver state. More...
 
int32_t MCSPI_lld_transferCancel (MCSPILLD_Handle hMcspi)
 This API cancels current McSPI transfer. More...
 
int32_t MCSPI_lld_transferDmaCancel (MCSPILLD_Handle hMcspi)
 This API cancels current McSPI transfer in DMA mode. More...
 
static void MCSPI_lld_ChConfig_init (MCSPI_ChConfig *chConfig)
 Function to initialize the MCSPI_ChConfig struct to its defaults. More...
 
static void MCSPI_lld_Transaction_init (MCSPI_Transaction *trans)
 Function to initialize the MCSPI_Transaction struct to its defaults. More...
 
uint32_t MCSPI_lld_getBaseAddr (MCSPILLD_Handle handle)
 Function to get base address of MCSPI instance of a particular handle. More...
 
int32_t MCSPI_lld_reConfigFifo (MCSPILLD_Handle handle, uint32_t chNum, uint32_t numWordsRxTx)
 Function to re-configure Effective FIFO Words. More...
 
void MCSPI_initiateLastChunkTransfer (MCSPILLD_Handle hMcspi, MCSPI_ChObject *chObj, const MCSPI_Transaction *transaction)
 This API will initiate the last chuncks when FIFO is enabled. The byte thats are non-multiple of FIFO trigger level. More...
 
static uint8_t MCSPI_getBufWidthShift (uint32_t dataSize)
 This API will return the buffer width in bytes based on dataSize. More...
 
static uint32_t MCSPI_readChStatusReg (uint32_t baseAddr, uint32_t chNum)
 This API will return the status of the McSPI channel currently in use. More...
 
static uint32_t MCSPI_readChCtrlReg (uint32_t baseAddr, uint32_t chNum)
 This API returns Channel control register value. More...
 
static void MCSPI_writeChCtrlReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal)
 This API sets Channel control register value. More...
 
static uint32_t MCSPI_readChConf (uint32_t baseAddr, uint32_t chNum)
 This API returns Channel Config register value. More...
 
static void MCSPI_writeChConfReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal)
 This API sets Channel Config register value. More...
 
static void MCSPI_writeTxDataReg (uint32_t baseAddr, uint32_t txData, uint32_t chNum)
 This API will put the data on to the McSPI Channel transmit register. More...
 
static void MCSPI_enableTxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag)
 This API will enable/disable the Tx FIFOs of McSPI peripheral. More...
 
static void MCSPI_enableRxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag)
 This API will enable/disable the Rx FIFOs of McSPI peripheral. More...
 
static uint32_t MCSPI_readRxDataReg (uint32_t baseAddr, uint32_t chNum)
 This API will return the data present in the MCSPI_RX register. More...
 
static void MCSPI_setDataWidth (uint32_t baseAddr, uint32_t chNum, uint32_t dataWidth)
 This API will set the data width in the channel config register. More...
 

Typedefs

typedef uint32_t(* MCSPI_clockGet) (void)
 
typedef void(* MCSPI_transferCallbackFxn) (void *args, uint32_t transferStatus)
 The definition of a transfer completion callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More...
 
typedef void(* MCSPI_errorCallbackFxn) (void *args, uint32_t transferStatus)
 The definition of a error callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More...
 
typedef struct MCSPILLD_InitObjectMCSPILLD_InitHandle
 
typedef struct MCSPILLD_ObjectMCSPILLD_Handle
 

Macros

#define MCSPI_MAX_NUM_CHANNELS   (4U)
 Max number of channels/Chip Select (CS) supported. More...
 
#define MCSPI_ERROR_TX_UNDERFLOW   (0x00000001U)
 McSPI error macro's. More...
 
#define MCSPI_ERROR_RX_OVERFLOW   (0x00000002U)
 
#define MCSPI_MAX_CLK_DIVIDER_SUPPORTED   (4096U)
 
#define MCSPI_FIFO_LENGTH   (64U)
 Total length of FIFO for both TX/RX. More...
 
#define MCSPI_RX_FIFO_ENABLE
 McSPI peripheral Rx FIFO is enabled. More...
 
#define MCSPI_RX_FIFO_DISABLE
 McSPI peripheral Rx FIFO is disabled. More...
 
#define MCSPI_TX_FIFO_ENABLE
 McSPI peripheral Tx FIFO is enabled. More...
 
#define MCSPI_TX_FIFO_DISABLE
 McSPI peripheral Tx FIFO is disabled. More...
 
#define MCSPI_REG_OFFSET   (0x14U)
 McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set. More...
 
#define MCSPI_CHCONF(x)
 Base address of McSPI_CHCONF(x) More...
 
#define MCSPI_CHSTAT(x)
 Base address of McSPI_CHSTAT(x) More...
 
#define MCSPI_CHCTRL(x)
 Base address of McSPI_CHCTRL(x) More...
 
#define MCSPI_CHTX(x)
 Base address of McSPI_CHTX(x) More...
 
#define MCSPI_CHRX(x)
 Base address of McSPI_CHRX(x) More...
 
#define MCSPI_CLKD_MASK   (0x0FU)
 
#define MCSPI_IRQSTATUS_CLEAR_ALL
 Bit mask to clear all status bits. More...
 

Return status

#define MCSPI_STATUS_SUCCESS   ((int32_t)0)
 Return status when the API execution was successful. More...
 
#define MCSPI_STATUS_FAILURE   ((int32_t)-1)
 Return status when the API execution was not successful due to a failure. More...
 
#define MCSPI_TIMEOUT   ((int32_t)-2)
 Return status when the API execution was not successful due to a time out. More...
 
#define MCSPI_INVALID_PARAM   ((int32_t)-3)
 Return status when the API execution failed due invalid parameters. More...
 
#define MCSPI_STATUS_BUSY   ((int32_t)-4)
 Return status when the API execution failed due to driver busy. More...
 
#define MCSPI_INVALID_STATE   ((int32_t)-5)
 Return status when the API execution failed due to invalid state. More...
 

Timeout values

#define MCSPI_NO_WAIT   ((uint32_t)0)
 Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More...
 
#define MCSPI_WAIT_FOREVER   ((uint32_t)-1)
 Value to use when needing a timeout of infinity or wait forver until resource is available. More...
 

MCSPI Driver states

#define MCSPI_STATE_RESET   ((uint32_t)0U)
 MCSPI driver is in Reset State prior to driver init and post driver deinit. More...
 
#define MCSPI_STATE_READY   ((uint32_t)1U)
 MCSPI driver accepts runtime APIs only Ready State, otherwise return error. More...
 
#define MCSPI_STATE_BUSY   ((uint32_t)2U)
 MCSPI driver is busy performing operation with peripherals, return error when APIs are invoked. More...
 
#define MCSPI_STATE_ERROR   ((uint32_t)3U)
 MCSPI driver ran into error, returns error for all APIs other than deinit in this state. More...
 

Channel Id

Values used to determine the channel number used for McSPI communication. This determines which Chip Select (CS) line to use

#define MCSPI_CHANNEL_0   (0U)
 
#define MCSPI_CHANNEL_1   (1U)
 
#define MCSPI_CHANNEL_2   (2U)
 
#define MCSPI_CHANNEL_3   (3U)
 

Operating Mode

Values used to determine the McSPI driver operation.

#define MCSPI_OPER_MODE_POLLED   (0U)
 
#define MCSPI_OPER_MODE_INTERRUPT   (1U)
 
#define MCSPI_OPER_MODE_DMA   (2U)
 

Transfer Status Code

Status codes that are set by the MCSPI driver

#define MCSPI_TRANSFER_COMPLETED   ((int32_t)0U)
 
#define MCSPI_TRANSFER_STARTED   ((int32_t)1U)
 
#define MCSPI_TRANSFER_CANCELLED   ((int32_t)2U)
 
#define MCSPI_TRANSFER_FAILED   ((int32_t)3U)
 
#define MCSPI_TRANSFER_CSN_DEASSERT   ((int32_t)4U)
 
#define MCSPI_TRANSFER_TIMEOUT   ((int32_t)5U)
 

Modes of Operation

Definitions for various MCSPI modes of operation

The MCSPI driver operates in both controller and SPI peripheral modes. Logically, the implementation is identical, however the difference between these two modes is driven by hardware. The default mode is MCSPI_MS_MODE_CONTROLLER, but can be set to peripheral mode by setting MCSPI_OpenParams.msMode to MCSPI_MS_MODE_PERIPHERAL in the parameters passed to MCSPI_open().

#define MCSPI_MS_MODE_CONTROLLER   (CSL_MCSPI_MODULCTRL_MS_MASTER)
 The module generates the clock and CS. More...
 
#define MCSPI_MS_MODE_PERIPHERAL   (CSL_MCSPI_MODULCTRL_MS_SLAVE)
 The module receives the clock and CS. More...
 

Frame Format

Definitions for various SPI data frame formats

POL0 = SPICLK is held low during the INACTIVE state POL1 = SPICLK is held high during the INACTIVE state

PHA0 = Data are latched on odd-numbered edges of SPICLK PHA1 = Data are latched on even-numbered edges of SPICLK

#define MCSPI_FF_POL0_PHA0   (0U)
 
#define MCSPI_FF_POL0_PHA1   (1U)
 
#define MCSPI_FF_POL1_PHA0   (2U)
 
#define MCSPI_FF_POL1_PHA1   (3U)
 

Chip-select Polarity

Type for SPI Chip Select Polarity and Clock Idle Level

#define MCSPI_CS_POL_HIGH   (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH)
 SPIEN (CS) is held high during the ACTIVE state. More...
 
#define MCSPI_CS_POL_LOW   (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW)
 SPIEN (CS) is held low during the ACTIVE state. More...
 

Transmit-Receive Modes

#define MCSPI_TR_MODE_TX_RX   (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI)
 
#define MCSPI_TR_MODE_RX_ONLY   (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY)
 
#define MCSPI_TR_MODE_TX_ONLY   (CSL_MCSPI_CH0CONF_TRM_TRANSONLY)
 

Input Select

#define MCSPI_IS_D0   (CSL_MCSPI_CH0CONF_IS_LINE0)
 Data line 0 (SPIDAT[0]) selected for reception. More...
 
#define MCSPI_IS_D1   (CSL_MCSPI_CH0CONF_IS_LINE1)
 Data line 1 (SPIDAT[1]) selected for reception. More...
 

Transmission Enable for Data Line

#define MCSPI_DPE_ENABLE   (CSL_MCSPI_CH0CONF_DPE0_ENABLED)
 Data line selected for transmission. More...
 
#define MCSPI_DPE_DISABLE   (CSL_MCSPI_CH0CONF_DPE0_DISABLED)
 No transmission on Data Line. More...
 

Peripheral Chip-select Signal Select

#define MCSPI_SLV_CS_SELECT_0   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0)
 
#define MCSPI_SLV_CS_SELECT_1   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1)
 
#define MCSPI_SLV_CS_SELECT_2   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2)
 
#define MCSPI_SLV_CS_SELECT_3   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3)
 

Start-bit Polarity

#define MCSPI_SB_POL_HIGH   (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL)
 SStart-bit polarity is held to 1 during MCSPI transfer. More...
 
#define MCSPI_SB_POL_LOW   (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL)
 Start-bit polarity is held to 0 during MCSPI transfer. More...
 

Chip-select Idle Time

Values used to configure the chip select time control (TCS)

#define MCSPI_TCS0_0_CLK   (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY)
 0.5 clock cycles delay More...
 
#define MCSPI_TCS0_1_CLK   (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY)
 1.5 clock cycles delay More...
 
#define MCSPI_TCS0_2_CLK   (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY)
 2.5 clock cycles delay More...
 
#define MCSPI_TCS0_3_CLK   (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY)
 3.5 clock cycles delay More...
 

Channel Mode

#define MCSPI_CH_MODE_SINGLE   (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE)
 Only one channel will be used in controller mode. This should be used when CS is used in forced enable mode. More...
 
#define MCSPI_CH_MODE_MULTI   (CSL_MCSPI_MODULCTRL_SINGLE_MULTI)
 More than one channel will be used in controller mode. More...
 

Pin Mode

#define MCSPI_PINMODE_3PIN   (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE)
 SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning. More...
 
#define MCSPI_PINMODE_4PIN   (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE)
 

Init Delay

Values used to enable initial delay for first transfer

#define MCSPI_INITDLY_0   (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY)
 No delay. More...
 
#define MCSPI_INITDLY_4   (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY)
 4 SPI bus clock delays More...
 
#define MCSPI_INITDLY_8   (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY)
 8 SPI bus clock delays More...
 
#define MCSPI_INITDLY_16   (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY)
 16 SPI bus clock delays More...
 
#define MCSPI_INITDLY_32   (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY)
 32 SPI bus clock delays More...
 

Macro Definition Documentation

◆ MCSPI_STATUS_SUCCESS

#define MCSPI_STATUS_SUCCESS   ((int32_t)0)

Return status when the API execution was successful.

◆ MCSPI_STATUS_FAILURE

#define MCSPI_STATUS_FAILURE   ((int32_t)-1)

Return status when the API execution was not successful due to a failure.

◆ MCSPI_TIMEOUT

#define MCSPI_TIMEOUT   ((int32_t)-2)

Return status when the API execution was not successful due to a time out.

◆ MCSPI_INVALID_PARAM

#define MCSPI_INVALID_PARAM   ((int32_t)-3)

Return status when the API execution failed due invalid parameters.

◆ MCSPI_STATUS_BUSY

#define MCSPI_STATUS_BUSY   ((int32_t)-4)

Return status when the API execution failed due to driver busy.

◆ MCSPI_INVALID_STATE

#define MCSPI_INVALID_STATE   ((int32_t)-5)

Return status when the API execution failed due to invalid state.

◆ MCSPI_NO_WAIT

#define MCSPI_NO_WAIT   ((uint32_t)0)

Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available.

◆ MCSPI_WAIT_FOREVER

#define MCSPI_WAIT_FOREVER   ((uint32_t)-1)

Value to use when needing a timeout of infinity or wait forver until resource is available.

◆ MCSPI_STATE_RESET

#define MCSPI_STATE_RESET   ((uint32_t)0U)

MCSPI driver is in Reset State prior to driver init and post driver deinit.

◆ MCSPI_STATE_READY

#define MCSPI_STATE_READY   ((uint32_t)1U)

MCSPI driver accepts runtime APIs only Ready State, otherwise return error.

◆ MCSPI_STATE_BUSY

#define MCSPI_STATE_BUSY   ((uint32_t)2U)

MCSPI driver is busy performing operation with peripherals, return error when APIs are invoked.

◆ MCSPI_STATE_ERROR

#define MCSPI_STATE_ERROR   ((uint32_t)3U)

MCSPI driver ran into error, returns error for all APIs other than deinit in this state.

◆ MCSPI_CHANNEL_0

#define MCSPI_CHANNEL_0   (0U)

◆ MCSPI_CHANNEL_1

#define MCSPI_CHANNEL_1   (1U)

◆ MCSPI_CHANNEL_2

#define MCSPI_CHANNEL_2   (2U)

◆ MCSPI_CHANNEL_3

#define MCSPI_CHANNEL_3   (3U)

◆ MCSPI_OPER_MODE_POLLED

#define MCSPI_OPER_MODE_POLLED   (0U)

◆ MCSPI_OPER_MODE_INTERRUPT

#define MCSPI_OPER_MODE_INTERRUPT   (1U)

◆ MCSPI_OPER_MODE_DMA

#define MCSPI_OPER_MODE_DMA   (2U)

◆ MCSPI_MAX_NUM_CHANNELS

#define MCSPI_MAX_NUM_CHANNELS   (4U)

Max number of channels/Chip Select (CS) supported.

◆ MCSPI_TRANSFER_COMPLETED

#define MCSPI_TRANSFER_COMPLETED   ((int32_t)0U)

◆ MCSPI_TRANSFER_STARTED

#define MCSPI_TRANSFER_STARTED   ((int32_t)1U)

◆ MCSPI_TRANSFER_CANCELLED

#define MCSPI_TRANSFER_CANCELLED   ((int32_t)2U)

◆ MCSPI_TRANSFER_FAILED

#define MCSPI_TRANSFER_FAILED   ((int32_t)3U)

◆ MCSPI_TRANSFER_CSN_DEASSERT

#define MCSPI_TRANSFER_CSN_DEASSERT   ((int32_t)4U)

◆ MCSPI_TRANSFER_TIMEOUT

#define MCSPI_TRANSFER_TIMEOUT   ((int32_t)5U)

◆ MCSPI_MS_MODE_CONTROLLER

#define MCSPI_MS_MODE_CONTROLLER   (CSL_MCSPI_MODULCTRL_MS_MASTER)

The module generates the clock and CS.

◆ MCSPI_MS_MODE_PERIPHERAL

#define MCSPI_MS_MODE_PERIPHERAL   (CSL_MCSPI_MODULCTRL_MS_SLAVE)

The module receives the clock and CS.

◆ MCSPI_FF_POL0_PHA0

#define MCSPI_FF_POL0_PHA0   (0U)

◆ MCSPI_FF_POL0_PHA1

#define MCSPI_FF_POL0_PHA1   (1U)

◆ MCSPI_FF_POL1_PHA0

#define MCSPI_FF_POL1_PHA0   (2U)

◆ MCSPI_FF_POL1_PHA1

#define MCSPI_FF_POL1_PHA1   (3U)

◆ MCSPI_CS_POL_HIGH

#define MCSPI_CS_POL_HIGH   (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH)

SPIEN (CS) is held high during the ACTIVE state.

◆ MCSPI_CS_POL_LOW

#define MCSPI_CS_POL_LOW   (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW)

SPIEN (CS) is held low during the ACTIVE state.

◆ MCSPI_TR_MODE_TX_RX

#define MCSPI_TR_MODE_TX_RX   (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI)

◆ MCSPI_TR_MODE_RX_ONLY

#define MCSPI_TR_MODE_RX_ONLY   (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY)

◆ MCSPI_TR_MODE_TX_ONLY

#define MCSPI_TR_MODE_TX_ONLY   (CSL_MCSPI_CH0CONF_TRM_TRANSONLY)

◆ MCSPI_IS_D0

#define MCSPI_IS_D0   (CSL_MCSPI_CH0CONF_IS_LINE0)

Data line 0 (SPIDAT[0]) selected for reception.

◆ MCSPI_IS_D1

#define MCSPI_IS_D1   (CSL_MCSPI_CH0CONF_IS_LINE1)

Data line 1 (SPIDAT[1]) selected for reception.

◆ MCSPI_DPE_ENABLE

#define MCSPI_DPE_ENABLE   (CSL_MCSPI_CH0CONF_DPE0_ENABLED)

Data line selected for transmission.

◆ MCSPI_DPE_DISABLE

#define MCSPI_DPE_DISABLE   (CSL_MCSPI_CH0CONF_DPE0_DISABLED)

No transmission on Data Line.

◆ MCSPI_SLV_CS_SELECT_0

#define MCSPI_SLV_CS_SELECT_0   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0)

◆ MCSPI_SLV_CS_SELECT_1

#define MCSPI_SLV_CS_SELECT_1   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1)

◆ MCSPI_SLV_CS_SELECT_2

#define MCSPI_SLV_CS_SELECT_2   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2)

◆ MCSPI_SLV_CS_SELECT_3

#define MCSPI_SLV_CS_SELECT_3   (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3)

◆ MCSPI_SB_POL_HIGH

#define MCSPI_SB_POL_HIGH   (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL)

SStart-bit polarity is held to 1 during MCSPI transfer.

◆ MCSPI_SB_POL_LOW

#define MCSPI_SB_POL_LOW   (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL)

Start-bit polarity is held to 0 during MCSPI transfer.

◆ MCSPI_TCS0_0_CLK

#define MCSPI_TCS0_0_CLK   (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY)

0.5 clock cycles delay

◆ MCSPI_TCS0_1_CLK

#define MCSPI_TCS0_1_CLK   (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY)

1.5 clock cycles delay

◆ MCSPI_TCS0_2_CLK

#define MCSPI_TCS0_2_CLK   (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY)

2.5 clock cycles delay

◆ MCSPI_TCS0_3_CLK

#define MCSPI_TCS0_3_CLK   (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY)

3.5 clock cycles delay

◆ MCSPI_CH_MODE_SINGLE

#define MCSPI_CH_MODE_SINGLE   (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE)

Only one channel will be used in controller mode. This should be used when CS is used in forced enable mode.

◆ MCSPI_CH_MODE_MULTI

#define MCSPI_CH_MODE_MULTI   (CSL_MCSPI_MODULCTRL_SINGLE_MULTI)

More than one channel will be used in controller mode.

◆ MCSPI_PINMODE_3PIN

#define MCSPI_PINMODE_3PIN   (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE)

SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning.

◆ MCSPI_PINMODE_4PIN

#define MCSPI_PINMODE_4PIN   (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE)

◆ MCSPI_INITDLY_0

#define MCSPI_INITDLY_0   (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY)

No delay.

◆ MCSPI_INITDLY_4

#define MCSPI_INITDLY_4   (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY)

4 SPI bus clock delays

◆ MCSPI_INITDLY_8

#define MCSPI_INITDLY_8   (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY)

8 SPI bus clock delays

◆ MCSPI_INITDLY_16

#define MCSPI_INITDLY_16   (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY)

16 SPI bus clock delays

◆ MCSPI_INITDLY_32

#define MCSPI_INITDLY_32   (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY)

32 SPI bus clock delays

◆ MCSPI_ERROR_TX_UNDERFLOW

#define MCSPI_ERROR_TX_UNDERFLOW   (0x00000001U)

McSPI error macro's.

◆ MCSPI_ERROR_RX_OVERFLOW

#define MCSPI_ERROR_RX_OVERFLOW   (0x00000002U)

◆ MCSPI_MAX_CLK_DIVIDER_SUPPORTED

#define MCSPI_MAX_CLK_DIVIDER_SUPPORTED   (4096U)

Maximuum Clock Divider supported

◆ MCSPI_FIFO_LENGTH

#define MCSPI_FIFO_LENGTH   (64U)

Total length of FIFO for both TX/RX.

◆ MCSPI_RX_FIFO_ENABLE

#define MCSPI_RX_FIFO_ENABLE
Value:
((uint32_t) CSL_MCSPI_CH0CONF_FFER_FFENABLED \
<< \
CSL_MCSPI_CH0CONF_FFER_SHIFT)

McSPI peripheral Rx FIFO is enabled.

◆ MCSPI_RX_FIFO_DISABLE

#define MCSPI_RX_FIFO_DISABLE
Value:
((uint32_t) CSL_MCSPI_CH0CONF_FFER_FFDISABLED \
<< CSL_MCSPI_CH0CONF_FFER_SHIFT)

McSPI peripheral Rx FIFO is disabled.

◆ MCSPI_TX_FIFO_ENABLE

#define MCSPI_TX_FIFO_ENABLE
Value:
((uint32_t) CSL_MCSPI_CH0CONF_FFEW_FFENABLED \
<< CSL_MCSPI_CH0CONF_FFEW_SHIFT)

McSPI peripheral Tx FIFO is enabled.

◆ MCSPI_TX_FIFO_DISABLE

#define MCSPI_TX_FIFO_DISABLE
Value:
((uint32_t) CSL_MCSPI_CH0CONF_FFEW_FFDISABLED \
<< CSL_MCSPI_CH0CONF_FFEW_SHIFT)

McSPI peripheral Tx FIFO is disabled.

◆ MCSPI_REG_OFFSET

#define MCSPI_REG_OFFSET   (0x14U)

McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set.

◆ MCSPI_CHCONF

#define MCSPI_CHCONF (   x)
Value:
((uint32_t) CSL_MCSPI_CH0CONF + \
(uint32_t) ((uint32_t) MCSPI_REG_OFFSET * \
(uint32_t) (x)))

Base address of McSPI_CHCONF(x)

◆ MCSPI_CHSTAT

#define MCSPI_CHSTAT (   x)
Value:
((uint32_t) CSL_MCSPI_CH0STAT + \
(uint32_t) ((uint32_t) MCSPI_REG_OFFSET * \
(uint32_t) (x)))

Base address of McSPI_CHSTAT(x)

◆ MCSPI_CHCTRL

#define MCSPI_CHCTRL (   x)
Value:
((uint32_t) CSL_MCSPI_CH0CTRL + \
(uint32_t) ((uint32_t) MCSPI_REG_OFFSET * \
(uint32_t) (x)))

Base address of McSPI_CHCTRL(x)

◆ MCSPI_CHTX

#define MCSPI_CHTX (   x)
Value:
((uint32_t) CSL_MCSPI_TX0 + \
(uint32_t) ((uint32_t) MCSPI_REG_OFFSET * \
(uint32_t) (x)))

Base address of McSPI_CHTX(x)

◆ MCSPI_CHRX

#define MCSPI_CHRX (   x)
Value:
((uint32_t) CSL_MCSPI_RX0 + \
(uint32_t) ((uint32_t) MCSPI_REG_OFFSET * \
(uint32_t) (x)))

Base address of McSPI_CHRX(x)

◆ MCSPI_CLKD_MASK

#define MCSPI_CLKD_MASK   (0x0FU)

◆ MCSPI_IRQSTATUS_CLEAR_ALL

#define MCSPI_IRQSTATUS_CLEAR_ALL
Value:
(CSL_MCSPI_IRQSTATUS_EOW_MASK | \
CSL_MCSPI_IRQSTATUS_WKS_MASK | \
CSL_MCSPI_IRQSTATUS_RX3_FULL_MASK | \
CSL_MCSPI_IRQSTATUS_TX3_UNDERFLOW_MASK | \
CSL_MCSPI_IRQSTATUS_TX3_EMPTY_MASK | \
CSL_MCSPI_IRQSTATUS_RX2_FULL_MASK | \
CSL_MCSPI_IRQSTATUS_TX2_UNDERFLOW_MASK | \
CSL_MCSPI_IRQSTATUS_TX2_EMPTY_MASK | \
CSL_MCSPI_IRQSTATUS_RX1_FULL_MASK | \
CSL_MCSPI_IRQSTATUS_TX1_UNDERFLOW_MASK | \
CSL_MCSPI_IRQSTATUS_TX1_EMPTY_MASK | \
CSL_MCSPI_IRQSTATUS_RX0_OVERFLOW_MASK | \
CSL_MCSPI_IRQSTATUS_RX0_FULL_MASK | \
CSL_MCSPI_IRQSTATUS_TX0_UNDERFLOW_MASK | \
CSL_MCSPI_IRQSTATUS_TX0_EMPTY_MASK)

Bit mask to clear all status bits.

Typedef Documentation

◆ MCSPI_clockGet

typedef uint32_t(* MCSPI_clockGet) (void)

◆ MCSPI_transferCallbackFxn

typedef void(* MCSPI_transferCallbackFxn) (void *args, uint32_t transferStatus)

The definition of a transfer completion callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK.

Parameters
args*void pointer
transferStatustransfer Status

◆ MCSPI_errorCallbackFxn

typedef void(* MCSPI_errorCallbackFxn) (void *args, uint32_t transferStatus)

The definition of a error callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK.

Parameters
args*void pointer
transferStatustransfer Status

◆ MCSPILLD_InitHandle

◆ MCSPILLD_Handle

typedef struct MCSPILLD_Object * MCSPILLD_Handle

Function Documentation

◆ MCSPI_reset()

void MCSPI_reset ( uint32_t  baseAddr)

◆ MCSPI_clearAllIrqStatus()

void MCSPI_clearAllIrqStatus ( uint32_t  baseAddr)

◆ MCSPI_stop()

void MCSPI_stop ( MCSPILLD_Handle  hMcspi,
MCSPI_ChObject chObj,
uint32_t  chNum 
)

◆ MCSPI_setChDataSize()

void MCSPI_setChDataSize ( uint32_t  baseAddr,
MCSPI_ChObject chObj,
uint32_t  dataSize,
uint32_t  csDisable 
)

◆ MCSPI_intrStatusClear()

static void MCSPI_intrStatusClear ( const MCSPI_ChObject chObj,
uint32_t  baseAddr,
uint32_t  intFlags 
)
inlinestatic

◆ MCSPI_lld_init()

int32_t MCSPI_lld_init ( MCSPILLD_Handle  hMcspi)

This API Initializes the McSPI instance.

Parameters
hMcspiHandle to the McSPI instance used
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_initDma()

int32_t MCSPI_lld_initDma ( MCSPILLD_Handle  hMcspi)

This API Initializes the McSPI instance in DMA Mode.

Parameters
hMcspiHandle to the McSPI instance used
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_deInit()

int32_t MCSPI_lld_deInit ( MCSPILLD_Handle  hMcspi)

This API De-Initializes the McSPI instance.

Parameters
hMcspiHandle to the McSPI instance used
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_deInitDma()

int32_t MCSPI_lld_deInitDma ( MCSPILLD_Handle  hMcspi)

This API De-Initializes the McSPI instance in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_write()

int32_t MCSPI_lld_write ( MCSPILLD_Handle  hMcspi,
void *  txBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API writes data to the McSPI instance in Polling mode.

Parameters
hMcspiHandle to the McSPI instance used
txBufPointer to write data buffer
countNumber of frames for this transaction
timeoutWrite timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_writeIntr()

int32_t MCSPI_lld_writeIntr ( MCSPILLD_Handle  hMcspi,
void *  txBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API writes data to the McSPI instance in Interrupt mode.

Parameters
hMcspiHandle to the McSPI instance used
txBufPointer to write data buffer
countNumber of frames for this transaction
timeoutwrite timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_writeDma()

int32_t MCSPI_lld_writeDma ( MCSPILLD_Handle  hMcspi,
void *  txBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API writes data to the McSPI instance in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
txBufPointer to write data buffer
countNumber of frames for this transaction
timeoutwrite timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_read()

int32_t MCSPI_lld_read ( MCSPILLD_Handle  hMcspi,
void *  rxBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API reads data from the McSPI instance in Polling mode.

Parameters
hMcspiHandle to the McSPI instance used
rxBufPointer to Read data buffer
countNumber of frames for this transaction
timeoutRead timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_readIntr()

int32_t MCSPI_lld_readIntr ( MCSPILLD_Handle  hMcspi,
void *  rxBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API reads data from the McSPI instance in Interrupt mode.

Parameters
hMcspiHandle to the McSPI instance used
rxBufPointer to Read data buffer
countNumber of frames for this transaction
timeoutRead timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_readDma()

int32_t MCSPI_lld_readDma ( MCSPILLD_Handle  hMcspi,
void *  rxBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API reads data from the McSPI instance in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
rxBufPointer to Read data buffer
countNumber of frames for this transaction
timeoutRead timeout value
extendedParamsPointer to structure that contains the transfer data. extendedParams
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_readWrite()

int32_t MCSPI_lld_readWrite ( MCSPILLD_Handle  hMcspi,
void *  txBuf,
void *  rxBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API reads writes data from the McSPI instance in polling mode.

Parameters
hMcspiHandle to the McSPI instance used
txBufPointer to write data buffer
rxBufPointer to Read data buffer
countNumber of frames for this transaction
timeoutRead write timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_readWriteIntr()

int32_t MCSPI_lld_readWriteIntr ( MCSPILLD_Handle  hMcspi,
void *  txBuf,
void *  rxBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API reads writes data from the McSPI instance in Interrupt mode.

Parameters
hMcspiHandle to the McSPI instance used
txBufPointer to write data buffer
rxBufPointer to Read data buffer
countNumber of frames for this transaction
timeoutRead write timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_readWriteDma()

int32_t MCSPI_lld_readWriteDma ( MCSPILLD_Handle  hMcspi,
void *  txBuf,
void *  rxBuf,
uint32_t  count,
uint32_t  timeout,
const MCSPI_ExtendedParams extendedParams 
)

This API reads writes data from the McSPI instance in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
txBufPointer to write data buffer
rxBufPointer to Read data buffer
countNumber of frames for this transaction
timeoutRead write timeout value
extendedParamsPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_readWriteCancel()

int32_t MCSPI_lld_readWriteCancel ( MCSPILLD_Handle  hMcspi)

This API cancels current McSPI transfer.

Parameters
hMcspiHandle to the McSPI instance used
Returns
Mcspi Status Status of current mcspi transaction

◆ MCSPI_lld_readWriteDmaCancel()

int32_t MCSPI_lld_readWriteDmaCancel ( MCSPILLD_Handle  hMcspi)

This API cancels current McSPI transfer in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
Returns
Mcspi Status Status of current mcspi transaction

◆ MCSPI_lld_transfer()

int32_t MCSPI_lld_transfer ( MCSPILLD_Handle  hMcspi,
MCSPI_Transaction transaction 
)

This API transfers data from the McSPI instance in Polling mode.

Parameters
hMcspiHandle to the McSPI instance used
transactionPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_transferIntr()

int32_t MCSPI_lld_transferIntr ( MCSPILLD_Handle  hMcspi,
MCSPI_Transaction transaction 
)

This API reads data from the McSPI instance in Interrupt mode.

Parameters
hMcspiHandle to the McSPI instance used
transactionPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_transferDma()

int32_t MCSPI_lld_transferDma ( MCSPILLD_Handle  hMcspi,
MCSPI_Transaction transaction 
)

This API reads data from the McSPI instance in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
transactionPointer to structure that contains the transfer data.
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_controllerIsr()

void MCSPI_lld_controllerIsr ( void *  args)

This is the McSPI Controller ISR and can be used as IRQ handler in Controller mode.

Parameters
argsArgument to the ISR.

◆ MCSPI_lld_peripheralIsr()

void MCSPI_lld_peripheralIsr ( void *  args)

This is the McSPI Peripheral ISR and can be used as IRQ handler in Peripheral mode.

Parameters
argsArgument to the ISR.

◆ MCSPI_lld_getState()

int32_t MCSPI_lld_getState ( MCSPILLD_Handle  hMcspi)

This API returns the driver state.

Parameters
hMcspiHandle to the McSPI instance used

◆ MCSPI_lld_transferCancel()

int32_t MCSPI_lld_transferCancel ( MCSPILLD_Handle  hMcspi)

This API cancels current McSPI transfer.

Parameters
hMcspiHandle to the McSPI instance used
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_transferDmaCancel()

int32_t MCSPI_lld_transferDmaCancel ( MCSPILLD_Handle  hMcspi)

This API cancels current McSPI transfer in DMA mode.

Parameters
hMcspiHandle to the McSPI instance used
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure

◆ MCSPI_lld_ChConfig_init()

static void MCSPI_lld_ChConfig_init ( MCSPI_ChConfig chConfig)
inlinestatic

Function to initialize the MCSPI_ChConfig struct to its defaults.

Parameters
chConfigPointer to MCSPI_ChConfig structure for initialization

◆ MCSPI_lld_Transaction_init()

static void MCSPI_lld_Transaction_init ( MCSPI_Transaction trans)
inlinestatic

Function to initialize the MCSPI_Transaction struct to its defaults.

Parameters
transPointer to MCSPI_Transaction structure for initialization

◆ MCSPI_lld_getBaseAddr()

uint32_t MCSPI_lld_getBaseAddr ( MCSPILLD_Handle  handle)

Function to get base address of MCSPI instance of a particular handle.

Parameters
handleMCSPILLD_Handle returned from MCSPI_open()
See also
MCSPI_open

◆ MCSPI_lld_reConfigFifo()

int32_t MCSPI_lld_reConfigFifo ( MCSPILLD_Handle  handle,
uint32_t  chNum,
uint32_t  numWordsRxTx 
)

Function to re-configure Effective FIFO Words.

Parameters
handleMCSPILLD_Handle returned from MCSPI_open()
chNumChannel used for communication.
numWordsRxTxNumber of words to transfer
Returns
MCSPI_STATUS_SUCCESS if successful; else error on failure
See also
MCSPI_open

◆ MCSPI_initiateLastChunkTransfer()

void MCSPI_initiateLastChunkTransfer ( MCSPILLD_Handle  hMcspi,
MCSPI_ChObject chObj,
const MCSPI_Transaction transaction 
)

This API will initiate the last chuncks when FIFO is enabled. The byte thats are non-multiple of FIFO trigger level.

Parameters
hMcspiMCSPILLD_Handle returned from MCSPI_open()
chObjPointer to the McSPI Channel Object.
transactionPointer to structure that contains the transfer data.

◆ MCSPI_getBufWidthShift()

static uint8_t MCSPI_getBufWidthShift ( uint32_t  dataSize)
inlinestatic

This API will return the buffer width in bytes based on dataSize.

Parameters
dataSizeMCSPI data frame size in bits - valid values: 4 bits to 32 bits
Returns
bufWidthShift Width of buffer in bytes - used for accessing the TX/RX buffer. When dataWidth <= 8, (1 byte - 0 shift) When dataWidth > 8 && <= 16, (2 bytes - 1 shift) When dataWidth > 16 && <= 32, (4 bytes - 2 shift)
See also
MCSPI_open

◆ MCSPI_readChStatusReg()

static uint32_t MCSPI_readChStatusReg ( uint32_t  baseAddr,
uint32_t  chNum 
)
inlinestatic

This API will return the status of the McSPI channel currently in use.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel used for communication.
    'chNum' can take the following values.\n
    MCSPI_CHANNEL_n - Channel n is used for communication.\n
Returns
This API will return the status of the McSPI channel status register. User can use the following macros to check the status
MCSPI_CH_STAT_RXS_FULL - Receiver register is full
MCSPI_CH_STAT_TXS_EMPTY - Transmitter register is full
MCSPI_CH_STAT_EOT - End of transfer status
MCSPI_CH_TXFFE - FIFO transmit buffer empty status
MCSPI_CH_TXFFF - FIFO transmit buffer full status
MCSPI_CH_RXFFE - FIFO receive buffer empty status
MCSPI_CH_RXFFF - FIFO receive buffer full status
See also
MCSPI_open

◆ MCSPI_readChCtrlReg()

static uint32_t MCSPI_readChCtrlReg ( uint32_t  baseAddr,
uint32_t  chNum 
)
inlinestatic

This API returns Channel control register value.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
Returns
Channel control register value.
See also
MCSPI_open

◆ MCSPI_writeChCtrlReg()

static void MCSPI_writeChCtrlReg ( uint32_t  baseAddr,
uint32_t  chNum,
uint32_t  regVal 
)
inlinestatic

This API sets Channel control register value.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
regValregister value to set in channel control register.
See also
MCSPI_open

◆ MCSPI_readChConf()

static uint32_t MCSPI_readChConf ( uint32_t  baseAddr,
uint32_t  chNum 
)
inlinestatic

This API returns Channel Config register value.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
Returns
Channel Config register value.
See also
MCSPI_open

◆ MCSPI_writeChConfReg()

static void MCSPI_writeChConfReg ( uint32_t  baseAddr,
uint32_t  chNum,
uint32_t  regVal 
)
inlinestatic

This API sets Channel Config register value.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
regValregister value to set in channel Config register.
See also
MCSPI_open

◆ MCSPI_writeTxDataReg()

static void MCSPI_writeTxDataReg ( uint32_t  baseAddr,
uint32_t  txData,
uint32_t  chNum 
)
inlinestatic

This API will put the data on to the McSPI Channel transmit register.

Parameters
baseAddrMemory Address of the McSPI instance used.
txData32 bit data sent by the user which is put on to the MCSPI_TX register.
chNumChannel number of the McSPI instance used.
    'chNum' can take the following values.\n
    MCSPI_CHANNEL_n - Channel n is used for communication.\n

    For chNum n can range from 0-3.\n
See also
MCSPI_open

◆ MCSPI_enableTxFIFO()

static void MCSPI_enableTxFIFO ( uint32_t  baseAddr,
uint32_t  chNum,
uint32_t  enableFlag 
)
inlinestatic

This API will enable/disable the Tx FIFOs of McSPI peripheral.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
enableFlagFlag to enable/diable FIFO transmit mode.
    'enableFlag' can take the following values.\n
    MCSPI_TX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n
    MCSPI_TX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n

    'chNum' can take the following values.\n
    MCSPI_CHANNEL_n - Channel n is used for communication.\n

    For chNum n can range from 0-3.\n
Note
: Enabling FIFO is restricted to only 1 channel.
See also
MCSPI_open

◆ MCSPI_enableRxFIFO()

static void MCSPI_enableRxFIFO ( uint32_t  baseAddr,
uint32_t  chNum,
uint32_t  enableFlag 
)
inlinestatic

This API will enable/disable the Rx FIFOs of McSPI peripheral.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
enableFlagFlag to enable/diable FIFO receive mode.
    'enableFlag' can take the following values.\n
    MCSPI_RX_FIFO_ENABLE - Enables the receiver FIFO of McSPI.\n
    MCSPI_RX_FIFO_DISABLE - Disables the receiver FIFO of McSPI.\n

    'chNum' can take the following values.\n
    MCSPI_CHANNEL_n - Channel n is used for communication.\n

    For chNum n can range from 0-3.\n
Note
: Enabling FIFO is restricted to only 1 channel.
See also
MCSPI_open

◆ MCSPI_readRxDataReg()

static uint32_t MCSPI_readRxDataReg ( uint32_t  baseAddr,
uint32_t  chNum 
)
inlinestatic

This API will return the data present in the MCSPI_RX register.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
    'chNum' can take the following values.\n
    MCSPI_CHANNEL_n - Channel n is used for communication.\n

    For chNum n can range from 0-3.\n
See also
MCSPI_open
Returns
This API will return the data received in the MCSPI_RX register.

◆ MCSPI_setDataWidth()

static void MCSPI_setDataWidth ( uint32_t  baseAddr,
uint32_t  chNum,
uint32_t  dataWidth 
)
inlinestatic

This API will set the data width in the channel config register.

Parameters
baseAddrMemory Address of the McSPI instance used.
chNumChannel number of the McSPI instance used.
dataWidthMCSPI data frame width in bits.
    'chNum' can take the following values.\n
    MCSPI_CHANNEL_n - Channel n is used for communication.\n

    For chNum n can range from 0-3.\n
    For dataWidth valid values: 4 bits to 32 bits
See also
MCSPI_open
MCSPI_REG_OFFSET
#define MCSPI_REG_OFFSET
McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx regist...
Definition: mcspi_lld.h:418