AM263Px MCU+ SDK  26.00.00

Introduction

This module contains APIs to program and use the I2C LLD module. The APIs can be used by other drivers to get access to I2C and also by application to initiate transaction operations.

The I2C LLD header file should be included in an application as follows:

Files

file  i2c_lld.h
 I2C LLD Driver API/interface file.
 

Data Structures

struct  I2CLLD_Transaction
 I2C Transaction. More...
 
struct  I2CLLD_Message
 I2C Message. More...
 
struct  I2C_ExtendedParams
 Data structure used with I2C_lld_write(), I2C_lld_writeIntr(), I2C_lld_read(), I2C_lld_readIntr() More...
 
struct  I2C_Memory_ExtendedParams
 Data structure used with I2C_lld_mem_write(), I2C_lld_mem_writeIntr(), I2C_lld_mem_read(), I2C_lld_mem_readIntr() More...
 
struct  I2CLLD_targetTransaction
 I2C Target Transaction. More...
 
struct  I2CLLD_Object
 I2C Driver Object. More...
 

Functions

int32_t I2C_lld_init (I2CLLD_Handle handle)
 API to Initializes the I2C instance. More...
 
int32_t I2C_lld_deInit (I2CLLD_Handle handle)
 API to De-Initializes the I2C instance. More...
 
int32_t I2C_lld_Transaction_init (I2CLLD_Transaction *transaction)
 API to set default values of I2CLLD_Transaction in transaction. More...
 
int32_t I2C_lld_Message_init (I2CLLD_Message *msg)
 API to set default values of I2CLLD_Message in msg. More...
 
int32_t I2C_lld_write (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
 API to initiate an I2C write operation in polled mode as I2C Controller. More...
 
int32_t I2C_lld_target_write (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
 API to initiate an I2C write operation in polled mode as I2C Target. More...
 
int32_t I2C_lld_writeIntr (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
 API to initiate an I2C write operation in interrupt mode as I2C Controller. More...
 
int32_t I2C_lld_target_writeIntr (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
 API to Initiate an I2C write operation in interrupt mode as I2C Target. More...
 
int32_t I2C_lld_read (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
 API to initiate an I2C read operation in polled mode as I2C Controller. More...
 
int32_t I2C_lld_target_read (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
 API to initiate an I2C read Operation in polled mode as I2C Target. More...
 
int32_t I2C_lld_readIntr (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
 API to initiate an I2C read operation in interrupt mode as I2C Controller. More...
 
int32_t I2C_lld_target_readIntr (I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
 API to initiate an I2C read operation in interrupt mode as I2C Target. More...
 
int32_t I2C_lld_mem_write (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
 API to initiate a Memory write Operation in polling Mode. More...
 
int32_t I2C_lld_mem_writeIntr (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
 API to initiate a Memory write operation in interrupt Mode. More...
 
int32_t I2C_lld_mem_read (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
 API to initiate a Memory read operation in Polled mode. More...
 
int32_t I2C_lld_mem_readIntr (I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
 API to initiate a Memory read operation in interrupt mode. More...
 
int32_t I2C_lld_transferPoll (I2CLLD_Handle handle, I2CLLD_Message *msg)
 API to initiate a transfer from I2C in polled mode. More...
 
int32_t I2C_lld_transferIntr (I2CLLD_Handle handle, I2CLLD_Message *msg)
 API to initiate a transfer from I2C in interrupt mode. More...
 
int32_t I2C_lld_targetTransferIntr (I2CLLD_Handle handle, I2CLLD_targetTransaction *txn)
 API to initiate a transfer from I2C in interrupt mode as target. More...
 
int32_t I2C_lld_probe (I2CLLD_Handle handle, uint32_t targetAddr)
 API to probe I2C. More...
 
int32_t I2C_lld_setBusFrequency (I2CLLD_Handle handle, uint32_t busFrequency)
 API to set the bus frequency. More...
 
void I2C_lld_controllerIsr (void *args)
 I2C Controller ISR, can be used as IRQ handler in Controller mode. More...
 
void I2C_lld_targetIsr (void *args)
 I2C Target ISR, can be used as IRQ handler in Target mode. More...
 
void I2CControllerControl (uint32_t baseAddr, uint32_t ctrlMask, uint32_t ctrlCmds)
 
void I2CSetDataCount (uint32_t baseAddr, uint32_t count)
 
void I2CControllerStart (uint32_t baseAddr)
 
void I2CControllerIntEnableEx (uint32_t baseAddr, uint32_t intFlag)
 
void I2CControllerTargetAddrSet (uint32_t baseAddr, uint32_t targetAddr)
 
void I2CControllerIntClearEx (uint32_t baseAddr, uint32_t intFlag)
 
void I2CModeControl (uint32_t baseAddr, uint32_t ctrlMask, uint32_t ctrlCmds)
 
void I2CTargetEnable (uint32_t baseAddr)
 

Typedefs

typedef uint32_t(* I2C_Clock_getTicks) (void)
 The definition of a get System Tick function used by the I2C driver to keep track of time. More...
 
typedef uint32_t(* I2C_Clock_usecToTicks) (uint64_t usecs)
 The definition of a micro seconds to ticks function used by the I2C driver to get ticks from microseconds. More...
 
typedef void(* I2C_Clock_uSleep) (uint32_t usec)
 The definition of a sleep function used by the I2C driver for delay. More...
 
typedef void(* I2C_lld_transferCompleteCallback) (void *args, const I2CLLD_Message *msg, int32_t transferStatus)
 The definition of a transfer completion callback function used by the I2C driver when used in Controller Callback Mode. More...
 
typedef void(* I2C_lld_targetTransferCompleteCallback) (void *args, const I2CLLD_targetTransaction *targetTxn, int32_t transferStatus)
 The definition of a transfer completion callback function used by the I2C driver when used in Target Mode. More...
 
typedef struct I2CLLD_ObjectI2CLLD_Handle
 

Return status

#define I2C_STS_SUCCESS   ((int32_t) 0)
 Return status when the API execution was successful. More...
 
#define I2C_STS_ERR   ((int32_t)-1)
 Return status when the API execution was not successful due to a generic Error. More...
 
#define I2C_STS_ERR_TIMEOUT   ((int32_t)-2)
 Return status when the API execution was not successful due to a time out. More...
 
#define I2C_STS_ERR_INVALID_PARAM   ((int32_t)-3)
 Return status when the API execution failed due invalid parameters. More...
 
#define I2C_STS_ERR_BUS_BUSY   ((int32_t)-4)
 Return status when the API execution failed due to driver busy. More...
 
#define I2C_STS_ERR_NO_ACK   ((int32_t)-5)
 Return status when the API execution failed due to no Acknowledgement from target. More...
 
#define I2C_STS_ERR_ARBITRATION_LOST   ((int32_t)-6)
 Return status when the API execution failed due to loss in arbitration during transmission. More...
 

Timeout values

#define I2C_NO_WAIT   ((uint32_t)0)
 Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More...
 
#define I2C_WAIT_FOREVER   ((uint32_t)-1)
 Value to use when needing a timeout of infinity or wait forver until resource is available. More...
 

I2C Driver states

#define I2C_STATE_RESET   ((uint8_t) 0U)
 I2C driver is in Reset State prior to driver init and post driver deinit. More...
 
#define I2C_STATE_IDLE   ((uint8_t) 1U)
 I2C driver accepts runtime APIs only Ready State, otherwise return error. More...
 
#define I2C_STATE_BUSY   ((uint8_t) 2U)
 I2C driver is busy performing operation with peripherals, return error when APIs are invoked. More...
 
#define I2C_STATE_ERROR   ((uint8_t) 3U)
 I2C driver ran into error, returns error for all APIs other than deinit in this state. More...
 

MACROS used to select one of the standardized bus bit rates for

I2C communication. Deafults to I2C_400KHZ

#define I2C_100KHZ   ((uint8_t) 0U)
 I2C bus frequency : 100KHz. More...
 
#define I2C_400KHZ   ((uint8_t) 1U)
 I2C bus frequency : 400KHz. More...
 

MACROS for the possible values of Memory Write/Read API parameter.

#define I2C_MEM_ADDR_SIZE_8_BITS   ((uint8_t) 1U)
 I2C Target Internal Memory address 8 bits. More...
 
#define I2C_MEM_ADDR_SIZE_16_BITS   ((uint8_t) 2U)
 I2C Target Internal Memory address 16 bits. More...
 

MACROS used to define the state of the I2C Driver State Machine

#define I2C_WRITE_STATE   ((uint8_t) 10U)
 I2C is in Write state. More...
 
#define I2C_READ_STATE   ((uint8_t) 11U)
 I2C is in Write state. More...
 
#define I2C_TARGET_XFER_STATE   ((uint8_t) 12U)
 I2C is trasferring in target mode. More...
 
#define I2C_TARGET_RESTART_STATE   ((uint8_t) 13U)
 I2C is restarting trasfer in target mode. More...
 

MACROS for I2CControllerControl mask and command values (ICMDR register)

#define I2C_CFG_MASK_TX   (CSL_I2C_ICMDR_TRX_MASK)
 
#define I2C_CFG_MASK_RX   (CSL_I2C_ICMDR_TRX_MASK)
 
#define I2C_CFG_MASK_STOP   (CSL_I2C_ICMDR_STP_MASK)
 
#define I2C_CFG_MASK_START   (CSL_I2C_ICMDR_STT_MASK)
 
#define I2C_CFG_MASK_RUN_FREE   (CSL_I2C_ICMDR_FREE_MASK)
 
#define I2C_CFG_MASK_REPEAT_MODE   (CSL_I2C_ICMDR_RM_MASK)
 
#define I2C_CFG_MASK_LOOP_BACK   (CSL_I2C_ICMDR_DLB_MASK)
 
#define I2C_CFG_MASK_XA   (CSL_I2C_ICMDR_XA_MASK)
 
#define I2C_CFG_CMD_TX   (CSL_I2C_ICMDR_TRX_MASK)
 
#define I2C_CFG_CMD_RX   (0U)
 
#define I2C_CFG_CMD_STOP   (CSL_I2C_ICMDR_STP_MASK)
 
#define I2C_CFG_CMD_START   (CSL_I2C_ICMDR_STT_MASK)
 
#define I2C_CFG_CMD_RUN_FREE_ON   (CSL_I2C_ICMDR_FREE_MASK)
 
#define I2C_CFG_CMD_RUN_FREE_OFF   (0U)
 
#define I2C_CFG_CMD_REPEAT_MODE_ON   (CSL_I2C_ICMDR_RM_MASK)
 
#define I2C_CFG_CMD_REPEAT_MODE_OFF   (0U)
 
#define I2C_CFG_CMD_LOOP_BACK_ON   (CSL_I2C_ICMDR_DLB_MASK)
 
#define I2C_CFG_CMD_LOOP_BACK_OFF   (0U)
 
#define I2C_CFG_CMD_10BIT_ADDRESS   (I2C_CFG_MASK_XA)
 
#define I2C_CFG_CMD_7BIT_ADDRESS   (0U)
 

MACROS that can be passed to I2CControllerIntStatusEx and I2CControllerIntClearEx

APIs as int status flag to check and clear interrupt status

#define I2C_INT_ARBITRATION_LOST   (CSL_I2C_ICSTR_AL_MASK)
 
#define I2C_INT_NO_ACK   (CSL_I2C_ICSTR_NACK_MASK)
 
#define I2C_INT_ADRR_READY_ACESS   (CSL_I2C_ICSTR_ARDY_MASK)
 
#define I2C_INT_RECV_READY   (CSL_I2C_ICSTR_ICRRDY_MASK)
 
#define I2C_INT_TRANSMIT_READY   (CSL_I2C_ICSTR_ICXRDY_MASK)
 
#define I2C_INT_STOP_CONDITION   (CSL_I2C_ICSTR_SCD_MASK)
 
#define I2C_INT_ADRR_ZERO   (CSL_I2C_ICSTR_AD0_MASK)
 
#define I2C_INT_ADRR_TARGET   (CSL_I2C_ICSTR_AAS_MASK)
 
#define I2C_INT_TRANSMIT_UNDER_FLOW   (CSL_I2C_ICSTR_XSMT_MASK)
 
#define I2C_INT_RECV_OVER_RUN   (CSL_I2C_ICSTR_RSFULL_MASK)
 
#define I2C_INT_BUS_BUSY   (CSL_I2C_ICSTR_BB_MASK)
 
#define I2C_INT_NO_ACK_SENT   (CSL_I2C_ICSTR_NACKSNT_MASK)
 
#define I2C_INT_TARGET_DIRECTION   (CSL_I2C_ICSTR_SDIR_MASK)
 
#define I2C_ALL_INTS
 
#define I2C_INT_MASK_ARBITRATION_LOST   (CSL_I2C_ICIMR_AL_MASK)
 
#define I2C_INT_MASK_NO_ACK   (CSL_I2C_ICIMR_NACK_MASK)
 
#define I2C_INT_MASK_ADRR_READY_ACESS   (CSL_I2C_ICIMR_ARDY_MASK)
 
#define I2C_INT_MASK_RECV_READY   (CSL_I2C_ICIMR_ICRRDY_MASK)
 
#define I2C_INT_MASK_TRANSMIT_READY   (CSL_I2C_ICIMR_ICXRDY_MASK)
 
#define I2C_INT_MASK_STOP_CONDITION   (CSL_I2C_ICIMR_SCD_MASK)
 
#define I2C_INT_MASK_ADRR_TARGET   (CSL_I2C_ICIMR_AAS_MASK)
 
#define I2C_ALL_INTS_MASK
 

Macro Definition Documentation

◆ I2C_STS_SUCCESS

#define I2C_STS_SUCCESS   ((int32_t) 0)

Return status when the API execution was successful.

◆ I2C_STS_ERR

#define I2C_STS_ERR   ((int32_t)-1)

Return status when the API execution was not successful due to a generic Error.

◆ I2C_STS_ERR_TIMEOUT

#define I2C_STS_ERR_TIMEOUT   ((int32_t)-2)

Return status when the API execution was not successful due to a time out.

◆ I2C_STS_ERR_INVALID_PARAM

#define I2C_STS_ERR_INVALID_PARAM   ((int32_t)-3)

Return status when the API execution failed due invalid parameters.

◆ I2C_STS_ERR_BUS_BUSY

#define I2C_STS_ERR_BUS_BUSY   ((int32_t)-4)

Return status when the API execution failed due to driver busy.

◆ I2C_STS_ERR_NO_ACK

#define I2C_STS_ERR_NO_ACK   ((int32_t)-5)

Return status when the API execution failed due to no Acknowledgement from target.

◆ I2C_STS_ERR_ARBITRATION_LOST

#define I2C_STS_ERR_ARBITRATION_LOST   ((int32_t)-6)

Return status when the API execution failed due to loss in arbitration during transmission.

◆ I2C_NO_WAIT

#define I2C_NO_WAIT   ((uint32_t)0)

Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available.

◆ I2C_WAIT_FOREVER

#define I2C_WAIT_FOREVER   ((uint32_t)-1)

Value to use when needing a timeout of infinity or wait forver until resource is available.

◆ I2C_STATE_RESET

#define I2C_STATE_RESET   ((uint8_t) 0U)

I2C driver is in Reset State prior to driver init and post driver deinit.

◆ I2C_STATE_IDLE

#define I2C_STATE_IDLE   ((uint8_t) 1U)

I2C driver accepts runtime APIs only Ready State, otherwise return error.

◆ I2C_STATE_BUSY

#define I2C_STATE_BUSY   ((uint8_t) 2U)

I2C driver is busy performing operation with peripherals, return error when APIs are invoked.

◆ I2C_STATE_ERROR

#define I2C_STATE_ERROR   ((uint8_t) 3U)

I2C driver ran into error, returns error for all APIs other than deinit in this state.

◆ I2C_100KHZ

#define I2C_100KHZ   ((uint8_t) 0U)

I2C bus frequency : 100KHz.

◆ I2C_400KHZ

#define I2C_400KHZ   ((uint8_t) 1U)

I2C bus frequency : 400KHz.

◆ I2C_MEM_ADDR_SIZE_8_BITS

#define I2C_MEM_ADDR_SIZE_8_BITS   ((uint8_t) 1U)

I2C Target Internal Memory address 8 bits.

◆ I2C_MEM_ADDR_SIZE_16_BITS

#define I2C_MEM_ADDR_SIZE_16_BITS   ((uint8_t) 2U)

I2C Target Internal Memory address 16 bits.

◆ I2C_WRITE_STATE

#define I2C_WRITE_STATE   ((uint8_t) 10U)

I2C is in Write state.

◆ I2C_READ_STATE

#define I2C_READ_STATE   ((uint8_t) 11U)

I2C is in Write state.

◆ I2C_TARGET_XFER_STATE

#define I2C_TARGET_XFER_STATE   ((uint8_t) 12U)

I2C is trasferring in target mode.

◆ I2C_TARGET_RESTART_STATE

#define I2C_TARGET_RESTART_STATE   ((uint8_t) 13U)

I2C is restarting trasfer in target mode.

◆ I2C_CFG_MASK_TX

#define I2C_CFG_MASK_TX   (CSL_I2C_ICMDR_TRX_MASK)

◆ I2C_CFG_MASK_RX

#define I2C_CFG_MASK_RX   (CSL_I2C_ICMDR_TRX_MASK)

◆ I2C_CFG_MASK_STOP

#define I2C_CFG_MASK_STOP   (CSL_I2C_ICMDR_STP_MASK)

◆ I2C_CFG_MASK_START

#define I2C_CFG_MASK_START   (CSL_I2C_ICMDR_STT_MASK)

◆ I2C_CFG_MASK_RUN_FREE

#define I2C_CFG_MASK_RUN_FREE   (CSL_I2C_ICMDR_FREE_MASK)

◆ I2C_CFG_MASK_REPEAT_MODE

#define I2C_CFG_MASK_REPEAT_MODE   (CSL_I2C_ICMDR_RM_MASK)

◆ I2C_CFG_MASK_LOOP_BACK

#define I2C_CFG_MASK_LOOP_BACK   (CSL_I2C_ICMDR_DLB_MASK)

◆ I2C_CFG_MASK_XA

#define I2C_CFG_MASK_XA   (CSL_I2C_ICMDR_XA_MASK)

◆ I2C_CFG_CMD_TX

#define I2C_CFG_CMD_TX   (CSL_I2C_ICMDR_TRX_MASK)

◆ I2C_CFG_CMD_RX

#define I2C_CFG_CMD_RX   (0U)

◆ I2C_CFG_CMD_STOP

#define I2C_CFG_CMD_STOP   (CSL_I2C_ICMDR_STP_MASK)

◆ I2C_CFG_CMD_START

#define I2C_CFG_CMD_START   (CSL_I2C_ICMDR_STT_MASK)

◆ I2C_CFG_CMD_RUN_FREE_ON

#define I2C_CFG_CMD_RUN_FREE_ON   (CSL_I2C_ICMDR_FREE_MASK)

◆ I2C_CFG_CMD_RUN_FREE_OFF

#define I2C_CFG_CMD_RUN_FREE_OFF   (0U)

◆ I2C_CFG_CMD_REPEAT_MODE_ON

#define I2C_CFG_CMD_REPEAT_MODE_ON   (CSL_I2C_ICMDR_RM_MASK)

◆ I2C_CFG_CMD_REPEAT_MODE_OFF

#define I2C_CFG_CMD_REPEAT_MODE_OFF   (0U)

◆ I2C_CFG_CMD_LOOP_BACK_ON

#define I2C_CFG_CMD_LOOP_BACK_ON   (CSL_I2C_ICMDR_DLB_MASK)

◆ I2C_CFG_CMD_LOOP_BACK_OFF

#define I2C_CFG_CMD_LOOP_BACK_OFF   (0U)

◆ I2C_CFG_CMD_10BIT_ADDRESS

#define I2C_CFG_CMD_10BIT_ADDRESS   (I2C_CFG_MASK_XA)

◆ I2C_CFG_CMD_7BIT_ADDRESS

#define I2C_CFG_CMD_7BIT_ADDRESS   (0U)

◆ I2C_INT_ARBITRATION_LOST

#define I2C_INT_ARBITRATION_LOST   (CSL_I2C_ICSTR_AL_MASK)

◆ I2C_INT_NO_ACK

#define I2C_INT_NO_ACK   (CSL_I2C_ICSTR_NACK_MASK)

◆ I2C_INT_ADRR_READY_ACESS

#define I2C_INT_ADRR_READY_ACESS   (CSL_I2C_ICSTR_ARDY_MASK)

◆ I2C_INT_RECV_READY

#define I2C_INT_RECV_READY   (CSL_I2C_ICSTR_ICRRDY_MASK)

◆ I2C_INT_TRANSMIT_READY

#define I2C_INT_TRANSMIT_READY   (CSL_I2C_ICSTR_ICXRDY_MASK)

◆ I2C_INT_STOP_CONDITION

#define I2C_INT_STOP_CONDITION   (CSL_I2C_ICSTR_SCD_MASK)

◆ I2C_INT_ADRR_ZERO

#define I2C_INT_ADRR_ZERO   (CSL_I2C_ICSTR_AD0_MASK)

◆ I2C_INT_ADRR_TARGET

#define I2C_INT_ADRR_TARGET   (CSL_I2C_ICSTR_AAS_MASK)

◆ I2C_INT_TRANSMIT_UNDER_FLOW

#define I2C_INT_TRANSMIT_UNDER_FLOW   (CSL_I2C_ICSTR_XSMT_MASK)

◆ I2C_INT_RECV_OVER_RUN

#define I2C_INT_RECV_OVER_RUN   (CSL_I2C_ICSTR_RSFULL_MASK)

◆ I2C_INT_BUS_BUSY

#define I2C_INT_BUS_BUSY   (CSL_I2C_ICSTR_BB_MASK)

◆ I2C_INT_NO_ACK_SENT

#define I2C_INT_NO_ACK_SENT   (CSL_I2C_ICSTR_NACKSNT_MASK)

◆ I2C_INT_TARGET_DIRECTION

#define I2C_INT_TARGET_DIRECTION   (CSL_I2C_ICSTR_SDIR_MASK)

◆ I2C_ALL_INTS

#define I2C_ALL_INTS
Value:
I2C_INT_NO_ACK | \
I2C_INT_ADRR_READY_ACESS | \
I2C_INT_RECV_READY | \
I2C_INT_TRANSMIT_READY | \
I2C_INT_STOP_CONDITION | \
I2C_INT_ADRR_ZERO | \
I2C_INT_ADRR_TARGET | \
I2C_INT_TRANSMIT_UNDER_FLOW | \
I2C_INT_RECV_OVER_RUN | \
I2C_INT_BUS_BUSY | \
I2C_INT_NO_ACK_SENT | \
I2C_INT_TARGET_DIRECTION \
)

◆ I2C_INT_MASK_ARBITRATION_LOST

#define I2C_INT_MASK_ARBITRATION_LOST   (CSL_I2C_ICIMR_AL_MASK)

◆ I2C_INT_MASK_NO_ACK

#define I2C_INT_MASK_NO_ACK   (CSL_I2C_ICIMR_NACK_MASK)

◆ I2C_INT_MASK_ADRR_READY_ACESS

#define I2C_INT_MASK_ADRR_READY_ACESS   (CSL_I2C_ICIMR_ARDY_MASK)

◆ I2C_INT_MASK_RECV_READY

#define I2C_INT_MASK_RECV_READY   (CSL_I2C_ICIMR_ICRRDY_MASK)

◆ I2C_INT_MASK_TRANSMIT_READY

#define I2C_INT_MASK_TRANSMIT_READY   (CSL_I2C_ICIMR_ICXRDY_MASK)

◆ I2C_INT_MASK_STOP_CONDITION

#define I2C_INT_MASK_STOP_CONDITION   (CSL_I2C_ICIMR_SCD_MASK)

◆ I2C_INT_MASK_ADRR_TARGET

#define I2C_INT_MASK_ADRR_TARGET   (CSL_I2C_ICIMR_AAS_MASK)

◆ I2C_ALL_INTS_MASK

#define I2C_ALL_INTS_MASK
Value:
I2C_INT_MASK_NO_ACK | \
I2C_INT_MASK_ADRR_READY_ACESS | \
I2C_INT_MASK_RECV_READY | \
I2C_INT_MASK_TRANSMIT_READY | \
I2C_INT_MASK_STOP_CONDITION | \
I2C_INT_MASK_ADRR_TARGET \
)

Typedef Documentation

◆ I2C_Clock_getTicks

typedef uint32_t(* I2C_Clock_getTicks) (void)

The definition of a get System Tick function used by the I2C driver to keep track of time.

Returns
Returns system ticks in 32-bit unsigned int format

◆ I2C_Clock_usecToTicks

typedef uint32_t(* I2C_Clock_usecToTicks) (uint64_t usecs)

The definition of a micro seconds to ticks function used by the I2C driver to get ticks from microseconds.

Parameters
usecsMicro Seconds
Returns
Returns system ticks in 32-bit unsigned int format

◆ I2C_Clock_uSleep

typedef void(* I2C_Clock_uSleep) (uint32_t usec)

The definition of a sleep function used by the I2C driver for delay.

Parameters
usecMicro Seconds

◆ I2C_lld_transferCompleteCallback

typedef void(* I2C_lld_transferCompleteCallback) (void *args, const I2CLLD_Message *msg, int32_t transferStatus)

The definition of a transfer completion callback function used by the I2C driver when used in Controller Callback Mode.

Parameters
argsVoid Pointer
msgPointer to I2CLLD_Message Object
transferStatusTransfer Status

◆ I2C_lld_targetTransferCompleteCallback

typedef void(* I2C_lld_targetTransferCompleteCallback) (void *args, const I2CLLD_targetTransaction *targetTxn, int32_t transferStatus)

The definition of a transfer completion callback function used by the I2C driver when used in Target Mode.

Parameters
argsVoid Pointer
targetTxnPointer to I2CLLD_targetTransaction Object
transferStatusTransfer Status

◆ I2CLLD_Handle

typedef struct I2CLLD_Object * I2CLLD_Handle

Function Documentation

◆ I2C_lld_init()

int32_t I2C_lld_init ( I2CLLD_Handle  handle)

API to Initializes the I2C instance.

Parameters
handle[IN] Handle to the I2C instance used
Returns
I2C_StatusCode

◆ I2C_lld_deInit()

int32_t I2C_lld_deInit ( I2CLLD_Handle  handle)

API to De-Initializes the I2C instance.

Parameters
handle[IN] Handle to the I2C instance used
Returns
I2C_StatusCode

◆ I2C_lld_Transaction_init()

int32_t I2C_lld_Transaction_init ( I2CLLD_Transaction transaction)

API to set default values of I2CLLD_Transaction in transaction.

Parameters
transaction[IN] Pointer to the structure to be initialized
Returns
I2C_StatusCode

◆ I2C_lld_Message_init()

int32_t I2C_lld_Message_init ( I2CLLD_Message msg)

API to set default values of I2CLLD_Message in msg.

Parameters
msg[IN] Pointer to the structure to be initialized
Returns
I2C_StatusCode

◆ I2C_lld_write()

int32_t I2C_lld_write ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams,
uint32_t  timeout 
)

API to initiate an I2C write operation in polled mode as I2C Controller.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_target_write()

int32_t I2C_lld_target_write ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams,
uint32_t  timeout 
)

API to initiate an I2C write operation in polled mode as I2C Target.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_writeIntr()

int32_t I2C_lld_writeIntr ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams 
)

API to initiate an I2C write operation in interrupt mode as I2C Controller.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_target_writeIntr()

int32_t I2C_lld_target_writeIntr ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams 
)

API to Initiate an I2C write operation in interrupt mode as I2C Target.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_read()

int32_t I2C_lld_read ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams,
uint32_t  timeout 
)

API to initiate an I2C read operation in polled mode as I2C Controller.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_target_read()

int32_t I2C_lld_target_read ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams,
uint32_t  timeout 
)

API to initiate an I2C read Operation in polled mode as I2C Target.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_readIntr()

int32_t I2C_lld_readIntr ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams 
)

API to initiate an I2C read operation in interrupt mode as I2C Controller.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_target_readIntr()

int32_t I2C_lld_target_readIntr ( I2CLLD_Handle  handle,
I2C_ExtendedParams extendedParams 
)

API to initiate an I2C read operation in interrupt mode as I2C Target.

Parameters
handle[IN] Handle to the I2C instance used
extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_mem_write()

int32_t I2C_lld_mem_write ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams,
uint32_t  timeout 
)

API to initiate a Memory write Operation in polling Mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_mem_writeIntr()

int32_t I2C_lld_mem_writeIntr ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams 
)

API to initiate a Memory write operation in interrupt Mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_mem_read()

int32_t I2C_lld_mem_read ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams,
uint32_t  timeout 
)

API to initiate a Memory read operation in Polled mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
timeout[IN] Timeout for read operation in Micro Seconds I2cTimeoutValues
Returns
I2C_StatusCode

◆ I2C_lld_mem_readIntr()

int32_t I2C_lld_mem_readIntr ( I2CLLD_Handle  handle,
I2C_Memory_ExtendedParams mem_extendedParams 
)

API to initiate a Memory read operation in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
mem_extendedParams[IN] Pointer to structure containing transfer parameters
Returns
I2C_StatusCode

◆ I2C_lld_transferPoll()

int32_t I2C_lld_transferPoll ( I2CLLD_Handle  handle,
I2CLLD_Message msg 
)

API to initiate a transfer from I2C in polled mode.

Parameters
handle[IN] Handle to the I2C instance used
msg[IN] Pointer to the I2CLLD_Message structure that contains values for this specific transfer
Returns
I2C_StatusCode

◆ I2C_lld_transferIntr()

int32_t I2C_lld_transferIntr ( I2CLLD_Handle  handle,
I2CLLD_Message msg 
)

API to initiate a transfer from I2C in interrupt mode.

Parameters
handle[IN] Handle to the I2C instance used
msg[IN] Pointer to the I2CLLD_Message structure that contains values for this specific transfer
Returns
I2C_StatusCode

◆ I2C_lld_targetTransferIntr()

int32_t I2C_lld_targetTransferIntr ( I2CLLD_Handle  handle,
I2CLLD_targetTransaction txn 
)

API to initiate a transfer from I2C in interrupt mode as target.

Parameters
handle[IN] Handle to the I2C instance used
txn[IN] Pointer to the I2CLLD_targetTransaction structure that contains values for this specific transfer
Returns
I2C_StatusCode

◆ I2C_lld_probe()

int32_t I2C_lld_probe ( I2CLLD_Handle  handle,
uint32_t  targetAddr 
)

API to probe I2C.

Parameters
handle[IN] handle to the I2C instance used
targetAddr[IN] address of the target to probe
Returns
I2C_StatusCode

◆ I2C_lld_setBusFrequency()

int32_t I2C_lld_setBusFrequency ( I2CLLD_Handle  handle,
uint32_t  busFrequency 
)

API to set the bus frequency.

Parameters
handle[IN] handle to the I2C instance used
busFrequency[IN] frequency value to be set I2cBitRates
Returns
I2C_StatusCode

◆ I2C_lld_controllerIsr()

void I2C_lld_controllerIsr ( void *  args)

I2C Controller ISR, can be used as IRQ handler in Controller mode.

Parameters
args[IN] Argument to the ISR

◆ I2C_lld_targetIsr()

void I2C_lld_targetIsr ( void *  args)

I2C Target ISR, can be used as IRQ handler in Target mode.

Parameters
args[IN] Argument to the ISR

◆ I2CControllerControl()

void I2CControllerControl ( uint32_t  baseAddr,
uint32_t  ctrlMask,
uint32_t  ctrlCmds 
)

◆ I2CSetDataCount()

void I2CSetDataCount ( uint32_t  baseAddr,
uint32_t  count 
)

◆ I2CControllerStart()

void I2CControllerStart ( uint32_t  baseAddr)

◆ I2CControllerIntEnableEx()

void I2CControllerIntEnableEx ( uint32_t  baseAddr,
uint32_t  intFlag 
)

◆ I2CControllerTargetAddrSet()

void I2CControllerTargetAddrSet ( uint32_t  baseAddr,
uint32_t  targetAddr 
)

◆ I2CControllerIntClearEx()

void I2CControllerIntClearEx ( uint32_t  baseAddr,
uint32_t  intFlag 
)

◆ I2CModeControl()

void I2CModeControl ( uint32_t  baseAddr,
uint32_t  ctrlMask,
uint32_t  ctrlCmds 
)

◆ I2CTargetEnable()

void I2CTargetEnable ( uint32_t  baseAddr)
I2C_INT_MASK_ARBITRATION_LOST
#define I2C_INT_MASK_ARBITRATION_LOST
Definition: i2c_lld.h:250
i2c_lld.h
I2C LLD Driver API/interface file.
I2C_INT_ARBITRATION_LOST
#define I2C_INT_ARBITRATION_LOST
Definition: i2c_lld.h:221