AM263Px MCU+ SDK  26.00.00

Introduction

Contains API to configure Bootseg and ECCM IP.

Data Structures

struct  FSS_ECCRegionConfig
 
struct  FSS_Config
 

Functions

int32_t FSS_addressBitMask (FSS_Handle handle, uint32_t bitMask, uint8_t segment)
 Mask the address bits. More...
 
int32_t FSS_disableAddressRemap (FSS_Handle handle)
 Disable remap. More...
 
int32_t FSS_selectRegionA (FSS_Handle handle)
 Map region A of flash to initial position. More...
 
int32_t FSS_selectRegionB (FSS_Handle handle)
 Map region N of flash to initial position. More...
 
uint32_t FSS_getBootRegion (FSS_Handle handle)
 Which boot region is been selected. More...
 
void FSS_enableECC (void)
 Enable ECC for Flash. More...
 
void FSS_disableECC (void)
 Disable ECC. More...
 
void FSS_setECCRegionSize (uint32_t regionIndex, uint32_t size_in_bytes)
 Set size of an ECCM region. More...
 
void FSS_setECCRegionStart (uint32_t regionIndex, uint32_t ecc_reg_start)
 Set start address of an ECCM region. More...
 
int32_t FSS_configECCMRegion (FSS_ECCRegionConfig *parameter)
 Configure en ECCM Region. More...
 
int32_t FSS_ConfigEccm (uint32_t numRegion, FSS_ECCRegionConfig *parameter)
 Configure ECCM hardware. More...
 

Typedefs

typedef void * FSS_Handle
 

Macros

#define Region_Index_0   ((uint32_t)(0))
 Index for ECCM region 0. More...
 
#define Region_Index_1   ((uint32_t)(1))
 Index for ECCM region 1. More...
 
#define Region_Index_2   ((uint32_t)(2))
 Index for ECCM region 2. More...
 
#define Region_Index_3   ((uint32_t)(3))
 Index for ECCM region 3. More...
 

Macro Definition Documentation

◆ Region_Index_0

#define Region_Index_0   ((uint32_t)(0))

Index for ECCM region 0.

◆ Region_Index_1

#define Region_Index_1   ((uint32_t)(1))

Index for ECCM region 1.

◆ Region_Index_2

#define Region_Index_2   ((uint32_t)(2))

Index for ECCM region 2.

◆ Region_Index_3

#define Region_Index_3   ((uint32_t)(3))

Index for ECCM region 3.

Typedef Documentation

◆ FSS_Handle

typedef void* FSS_Handle

Function Documentation

◆ FSS_addressBitMask()

int32_t FSS_addressBitMask ( FSS_Handle  handle,
uint32_t  bitMask,
uint8_t  segment 
)

Mask the address bits.

Use this function to remap external flash. Lower 12 bits cannot be masked.

The address that will be sent to external flash will be (address & bitMask) | ((bitMask + 1) * segment)

Suppose external flash is 32MB and it is required to map upper 16MB to address 0 so that read from address 0 would automatically translar to 16MB read. In this case the bitMask would be 0xffffff and segment would be 1. address that would be sent to flash is (0xffffff * address) | 0x1000000

Parameters
handlehandle to FSS instance
bitMaskbit mask
segmentsegment
Returns
SystemP_SUCCESS on successfull execution

◆ FSS_disableAddressRemap()

int32_t FSS_disableAddressRemap ( FSS_Handle  handle)

Disable remap.

Parameters
handlehandle to FSS instance
Returns
SystemP_SUCCESS on successfull execution

◆ FSS_selectRegionA()

int32_t FSS_selectRegionA ( FSS_Handle  handle)

Map region A of flash to initial position.

Parameters
handlehandle to FSS instance
Returns
SystemP_SUCCESS on successfull execution

◆ FSS_selectRegionB()

int32_t FSS_selectRegionB ( FSS_Handle  handle)

Map region N of flash to initial position.

Parameters
handlehandle to FSS instance
Returns
SystemP_SUCCESS on successfull execution

◆ FSS_getBootRegion()

uint32_t FSS_getBootRegion ( FSS_Handle  handle)

Which boot region is been selected.

Parameters
handlehandle to FSS instance.
Returns
selected boot region.

◆ FSS_enableECC()

void FSS_enableECC ( void  )

Enable ECC for Flash.

This function enabled ECC for the data that is stored in flash. For every 32 Bytes of data, 4 bytes of ECC is assumed. Make sure the data is in flash is prepared at compile time.

◆ FSS_disableECC()

void FSS_disableECC ( void  )

Disable ECC.

◆ FSS_setECCRegionSize()

void FSS_setECCRegionSize ( uint32_t  regionIndex,
uint32_t  size_in_bytes 
)

Set size of an ECCM region.

Parameters
regionIndexregion ID
size_in_bytessize of region in bytes

◆ FSS_setECCRegionStart()

void FSS_setECCRegionStart ( uint32_t  regionIndex,
uint32_t  ecc_reg_start 
)

Set start address of an ECCM region.

Parameters
regionIndexregion ID
ecc_reg_startstart address

◆ FSS_configECCMRegion()

int32_t FSS_configECCMRegion ( FSS_ECCRegionConfig parameter)

Configure en ECCM Region.

Parameters
parameterparameters for the region
Returns
int32_t

◆ FSS_ConfigEccm()

int32_t FSS_ConfigEccm ( uint32_t  numRegion,
FSS_ECCRegionConfig parameter 
)

Configure ECCM hardware.

Parameters
numRegionregion ID
parameterregion config data