AM263Px MCU+ SDK  26.00.00
Ethernet interface (RGMII / MII) selection

The diagram below depicts the signals for RGMII and MII respectively.

Figure: Ethernet RGMII and MII Signalling
  • RGMII is the default interface configured in SDK examples.
  • To configure MII interface follow steps captured below:
    • Modify the following changes in CPSW example Syscfg-GUI

  1. SOC Pinmux selection in 'Syscfg‑Gui → TI NETWORKING → Enet (CPSW) → CPSW Pinmux Config'

  1.1. If 'Mac Port 1' is used, select MII from drop down against RMII(1)/RGMII(1)/MII(1).
  1.2. If 'Mac Port 2' is used, select MII from drop down against RMII(2)/RGMII(2)/MII(2).

MII_PINMUX_PORT1 instance MII_PINMUX_PORT2 instance

  2. MII1 Pinmux selection in 'Syscfg‑Gui → TI NETWORKING → Enet (CPSW) → IO Set'

  2.1. If 'Mac Port 1' is used, select MII1 from drop down against MII1.
  2.2. If 'Mac Port 2' is used, select MII2 from drop down against MII2.

MII_PINMUX_PORT1 instance MII_PINMUX_PORT2 instance

  3. PHY Pinmux selection for "RX_ER" pin in 'Syscfg‑Gui → TI BOARD DRIVERS → ENETPHY (Enet CPSW/ICSS) → Extended Configuration'

Figure: Ethernet PHY RX_ER Pin config

Back To Top