AM263Px MCU+ SDK  26.00.00
dp83tg721.h File Reference

Introduction

This file contains the type definitions and helper macros for the DP83TG721 Ethernet PHY.

Go to the source code of this file.

Data Structures

struct  Dp83tg721_Cfg
 DP83TG721 PHY configuration parameters. More...
 

Macros

#define DP83TG721_LED_NUM   (2U)
 Number of LEDs available in the PHY. More...
 

Functions

void Dp83tg721_initCfg (Dp83tg721_Cfg *cfg)
 Initialize DP83TC811 PHY specific config params. More...