AM263Px MCU+ SDK  26.00.00
dp83tg720.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2020
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
49 #ifndef DP83TG720_H_
50 #define DP83TG720_H_
51 
52 /* ========================================================================== */
53 /* Include Files */
54 /* ========================================================================== */
55 
56 #include <stdint.h>
57 
58 #include "phy_common.h"
59 #include "port.h"
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
65 /* ========================================================================== */
66 /* Macros */
67 /* ========================================================================== */
68 
69 /* None */
70 
71 /* ========================================================================== */
72 /* Structures and Enums */
73 /* ========================================================================== */
74 
78 typedef enum Dp83tg720_MasterSlaveMode_e
79 {
82 
85 
89 
93 typedef struct Dp83tg720_Cfg_s
94 {
97 
100 
103 
106 
109 } Dp83tg720_Cfg;
110 
111 /* ========================================================================== */
112 /* Global Variables Declarations */
113 /* ========================================================================== */
114 
115 /* None */
116 
117 /* ========================================================================== */
118 /* Function Declarations */
119 /* ========================================================================== */
120 
129 
131  uint8_t phyAddr,
132  Phy_RegAccessCb_t* pRegAccessCb);
133 
135  const void *pversion);
136 
138  Phy_Mii mii);
139 
141  const void *pExtCfg,
142  const uint32_t extCfgSize,
143  Phy_Mii mii,
144  bool loopbackEn);
145 
147 
149 
151 /* ========================================================================== */
152 /* Deprecated Function Declarations */
153 /* ========================================================================== */
154 
155 /* None */
156 
157 /* ========================================================================== */
158 /* Static Function Definitions */
159 /* ========================================================================== */
160 
161 /* None */
162 
163 #ifdef __cplusplus
164 }
165 #endif
166 
167 #endif /* DP83TG720_H_ */
168 
Dp83tg720_Cfg::interruptEn
bool interruptEn
Definition: dp83tg720.h:102
Dp83tg720_config
int32_t Dp83tg720_config(EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn)
Dp83tg720_Cfg::sgmiiAutoNegEn
bool sgmiiAutoNegEn
Definition: dp83tg720.h:105
Dp83tg720_Cfg::rxClkShiftEn
bool rxClkShiftEn
Definition: dp83tg720.h:99
Dp83tg720_bind
void Dp83tg720_bind(EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb)
Phy_RegAccessCb_t
Definition: phy_common.h:283
Dp83tg720_Cfg::MasterSlaveMode
Dp83tg720_MasterSlaveMode MasterSlaveMode
Definition: dp83tg720.h:108
EthPhyDrv_Handle
uint8_t EthPhyDrv_Handle[ETHPHYDRV_MAX_OBJ_SIZE]
Definition: phy_common.h:302
Dp83tg720_isResetComplete
bool Dp83tg720_isResetComplete(EthPhyDrv_Handle hPhy)
Phy_Mii
Phy_Mii
Definition: phy_common.h:220
Dp83tg720_isMacModeSupported
bool Dp83tg720_isMacModeSupported(EthPhyDrv_Handle hPhy, Phy_Mii mii)
Dp83tg720_reset
void Dp83tg720_reset(EthPhyDrv_Handle hPhy)
Dp83tg720_printRegs
void Dp83tg720_printRegs(EthPhyDrv_Handle hPhy)
Dp83tg720_isPhyDevSupported
bool Dp83tg720_isPhyDevSupported(EthPhyDrv_Handle hPhy, const void *pversion)
Dp83tg720_Cfg
DP83TG720 PHY configuration parameters.
Definition: dp83tg720.h:94
phy_common.h
DP83TG720_MASTER_MODE
@ DP83TG720_MASTER_MODE
Definition: dp83tg720.h:84
Dp83tg720_Cfg::txClkShiftEn
bool txClkShiftEn
Definition: dp83tg720.h:96
Dp83tg720_MasterSlaveMode
Dp83tg720_MasterSlaveMode
DP83TG720 Master/Slave modes.
Definition: dp83tg720.h:79
DP83TG720_SLAVE_MODE
@ DP83TG720_SLAVE_MODE
Definition: dp83tg720.h:87
DP83TG720_MASTER_SLAVE_STRAP
@ DP83TG720_MASTER_SLAVE_STRAP
Definition: dp83tg720.h:81
Dp83tg720_initCfg
void Dp83tg720_initCfg(Dp83tg720_Cfg *cfg)
Initialize DP83TG720 PHY specific config params.