AM263Px MCU+ SDK  26.00.00
dp83869.h File Reference

Introduction

This file contains the type definitions and helper macros for the DP83869 Ethernet PHY.

Go to the source code of this file.

Data Structures

struct  Dp83869_Cfg
 DP83869 PHY configuration parameters. More...
 

Macros

#define DP83869_LED_NUM   (4U)
 Number of LEDs available in the PHY. More...
 

Enumerations

enum  Dp83869_Gpio0Mode {
  DP83869_GPIO0_CLK_OUT = 0x0U, DP83869_GPIO0_INT = 0x2U, DP83869_GPIO0_LINK_STATUS = 0x3U, DP83869_GPIO0_TX_SFD = 0x5U,
  DP83869_GPIO0_RX_SFD = 0x6U, DP83869_GPIO0_WOL = 0x7U, DP83869_GPIO0_ED = 0x8U, DP83869_GPIO0_PRBS_ERR = 0x9U,
  DP83869_GPIO0_LED_2 = 0xAU, DP83869_GPIO0_LED_GPIO_3 = 0xBU, DP83869_GPIO0_CRS = 0xCU, DP83869_GPIO0_COL = 0xDU,
  DP83869_GPIO0_CONSTANT0 = 0xEU, DP83869_GPIO0_CONSTANT1 = 0xFU
}
 GPIO_0 mux modes. More...
 
enum  Dp83869_Gpio1Mode {
  DP83869_GPIO1_CLK_OUT = 0x0U, DP83869_GPIO1_INT = 0x2U, DP83869_GPIO1_LINK_STATUS = 0x3U, DP83869_GPIO1_TX_SFD = 0x5U,
  DP83869_GPIO1_RX_SFD = 0x6U, DP83869_GPIO1_WOL = 0x7U, DP83869_GPIO1_ED = 0x8U, DP83869_GPIO1_PRBS_ERR = 0x9U,
  DP83869_GPIO1_LED_2 = 0xAU, DP83869_GPIO1_LED_GPIO_3 = 0xBU, DP83869_GPIO1_CRS = 0xCU, DP83869_GPIO1_COL = 0xDU,
  DP83869_GPIO1_CONSTANT0 = 0xEU, DP83869_GPIO1_CONSTANT1 = 0xFU
}
 GPIO_1 mux modes. More...
 
enum  Dp83869_LedMode {
  DP83869_LED_LINKED = 0x0U, DP83869_LED_RXTXACT = 0x1U, DP83869_LED_TXACT = 0x2U, DP83869_LED_RXACT = 0x3U,
  DP83869_LED_COLLDET = 0x4U, DP83869_LED_LINKED_1000BT = 0x5U, DP83869_LED_LINKED_100BTX = 0x6U, DP83869_LED_LINKED_10BT = 0x7U,
  DP83869_LED_LINKED_10100BT = 0x8U, DP83869_LED_LINKED_1001000BT = 0x9U, DP83869_LED_FULLDUPLEX = 0xAU, DP83869_LED_LINKED_BLINKACT = 0xBU,
  DP83869_LED_RXTXERR = 0xDU, DP83869_LED_RXERR = 0xEU
}
 LED modes (sources). More...
 

Functions

void Dp83869_initCfg (Dp83869_Cfg *cfg)
 Initialize DP83869 PHY specific config params. More...
 
void Dp83869_bind (EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb)
 
bool Dp83869_isPhyDevSupported (EthPhyDrv_Handle hPhy, const void *pVersion)
 
bool Dp83869_isMacModeSupported (EthPhyDrv_Handle hPhy, Phy_Mii mii)
 
int32_t Dp83869_config (EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn)
 
void Dp83869_reset (EthPhyDrv_Handle hPhy)
 
bool Dp83869_isResetComplete (EthPhyDrv_Handle hPhy)
 
void Dp83869_printRegs (EthPhyDrv_Handle hPhy)