AM263Px MCU+ SDK  26.00.00
Achieving Fast Secure Boot and Boot time calculator

Achieving Fast Secure Boot

Introduction

This document is intended for the users who want to achieve the least secure boot time for a signed (optionally encrypted) application through Flash interface

Steps to build, flash, load and run secure applications

  • Make sure pyelftools, construct and cryptography is installed from pip. This package is required for encrypting MCELF application images.
pip install pyelftools construct cryptography
  • Set MCELF_MERGE_SEGMENTS_FLAG = false and MCELF_MAX_SEGMENT_SIZE = 65536(64KB) in devconfig.mak file present in MCU+ SDK.
  • Build the libraries for the specific SOC in MCU+ SDK .
make libs DEVICE=am263px


  • Build the HSM runtime firmware for the HSSE device with the command below in TIFSMCU.
make -s -C hsm_firmware/am263px/hsse/hsm0-0_nortos/ti-arm-clang/ all DEVICE=am263px DEVICE_TYPE=HS
  • Build the fastboot SBL project which has various optimizations.   
    make -sj -c examples/drivers/boot/sbl_ospi_fastboot/am263px-cc/r5fss0-0_nortos/ti-arm-clang/ all DEVICE=am263px DEVICE_TYPE=HS
Note
The HSM runtime flash address can be configured via sysconfig tool. Open the sysconfig gui for the fastboot SBL and change the HSM Runtime Image Offset option to the new value. The flash address must be the same in the flash writer config and the SBL sysconfig for correct SBL operation.
HSM Runtime Flash Offset
  • Build the application with DEVICE and DEVICE_TYPE=HS options to make a secure MCELF signed application . The extension of this application is *.mcelf.hs .
make -sj -c examples/hello_world/am263px-cc/r5fss0-0_nortos/ti-arm-clang/ all DEVICE=am263px DEVICE_TYPE=HS


Note
Make sure that application and SBL OCRAM usage is mutually exclusive except the vector table. This can be done by looking at the MAP files of both the SBL and Application. In case of overlap between the two, move the application to a greater address using sysconfig memory configurator tool.

  

  • Please use fast_sbl_ospi.cfg present in ${MCU_PLUS_SDK_PATH}/tools/boot/sbl_prebuilt/am263px-cc/fast_sbl_ospi.cfg . 
Note
HSM runtime firmware path must be provided in this fast sbl config in addition to sbl_qspi_fastboot, application and sbl_uart_uniflash binary paths .
  • Set the board to OSPI bootmode and reset the device.

No logs are expected in sbl_ospi_fastboot since UART logging is disabled.

Component wise secure boot time measurement

Secure Boot time can be measured by using GPIOs at various points of execution.

The points of interest for Secure Boot are:

  1. HSMRT load request and acknowledgement
    • This can be measured with the Hsmclient_loadHSMRtFirmwareNonBlocking function and Hsmclient_mboxRxISRNonBlocking ISR present in hsmclient_loadhsmrt.c in the source/security/security_common folder.
  2. Flash read call in board flash drivers.
    • This can be measured with the functions present in flash_xxxx_xspi.c in the source/board/flash/xspi/ folder.
  3. HSM Authentication/Encryption request:
    • This can be measured by toggling GPIOs in the TIFS streaming service ISRs.

Boot time calculator

The boot time calculator can be used get an idea of the secure boot time values which can be achieved with fast boot sbls and tifs mcu. The numbers are as per SDK 10.00 version.

Checkout the secure boot time calculator tool here .