AM263Px MCU+ SDK  26.00.00
SDL R5FCPU_UTILS Example

Introduction

This example demonstrates-

  • How to read all the static registers of ARM Cortex R5F CPU, which all can be found in System control section in R5F TRM.

Use Cases

  • Read All the R5F CPU Static Registers.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss1-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/sdl/r5f_cpu_utils/

Steps to Run the Example

See Also

R5F_CPU_UTILS

Sample Output

Shown below is a sample output when the application is run for R5F,

For detail description of these register values, one can refer ARM CORTEX R5F TRM in System control section.

R5F CPU STATIC REGISTER READ Start...
The MPU Register read started for MPU REGION -> 0x0
The SCTLR register value is 0x1e5187d
The MPUIR register value is 0x1000
The RGNR register value is 0x0
The MPURbaseAddr register value is 0x0
The MPURsize register value is 0x3d
The MPURaccessControl register value is 0x1204
The MPU Register read started for MPU REGION -> 0x1
The SCTLR register value is 0x1e5187d
The MPUIR register value is 0x1000
The RGNR register value is 0x1
The MPURbaseAddr register value is 0x0
The MPURsize register value is 0x1d
The MPURaccessControl register value is 0x20b
The MPU Register read started for MPU REGION -> 0x2
The SCTLR register value is 0x1e5187d
The MPUIR register value is 0x1000
The RGNR register value is 0x2
The MPURbaseAddr register value is 0x80000
The MPURsize register value is 0x1d
The MPURaccessControl register value is 0x20b
The MPU Register read started for MPU REGION -> 0x3
The SCTLR register value is 0x1e5187d
The MPUIR register value is 0x1000
The RGNR register value is 0x3
The MPURbaseAddr register value is 0x70000000
The MPURsize register value is 0x29
The MPURaccessControl register value is 0x20b
All the R5F MPU Static register read are complete.
The SCTLR register value is 0x1e5187d
The ACTLR register value is 0x2f
The SecondaryACTLR register value is 0x400000
The CPACR register value is 0xc0f00000
The BTCMRegionR register value is 0x80019
The ATCMRegionR register value is 0x25
The SlavePortControlR register value is 0x0
The CONTEXTIDR register value is 0x0
The nVALIRQSET register value is 0x0
The nVALFIQSET register value is 0x0
The nVALRESETSET register value is 0x0
The nVALDEBUGSET register value is 0x0
The nVALIRQCLEAR register value is 0x0
The nVALFIQCLEAR register value is 0x0
The nVALRESETCLEAR register value is 0x0
The nVALDEBUGCLEAR register value is 0x0
The BuildOption1R register value is 0x80000
The BuildOption2R register value is 0x8abfc5c7
The PinOptionR register value is 0xc
The LLPPnormalAXIRR register value is 0x0
The LLPPvirtualAXIRR register value is 0x0
The AHBRR register value is 0x5000004d
The PMCNTENSET register value is 0x80000000
The PMCR register value is 0x41151801
The PMUSERENR register value is 0x0
The PMINTENSET register value is 0x0
The PMINTENCLR register value is 0x0
R5F CPU STATIC REGISTER READ Complete!
All test have passed.