AM263Px MCU+ SDK  26.00.00
SDL PBIST

Introduction

This example demonstrates the usage of the PBIST module. The example shows how to setup and use the PBIST controller. The example configures the algorithm and memory group. Example also prints the time taken for test execution.

Use Cases

Use Case Description
UC-1 Configure wrong combination of algorithm and memory group.
UC-2 Configure correct combination of algorithm and memory group.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss1-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/sdl/pbist/pbist_mcu/

Steps to Run the Example

See Also

PBIST

Sample Output

Shown below is a sample output when the application is run,

[Cortex_R5_0]
PBIST Application
Starting PBIST failure insertion test on TOP PBIST
PBIST failure Insertion test complete for TOP BIST
PBIST Failure Insertion Test completed in 47 micro secs
Starting PBIST test on TOP PBIST
PBIST complete for R5 STC
PBIST complete for R51 STC
PBIST complete for R50 TMU1
PBIST complete for R50 TMU2
PBIST complete for R50 TMU3
PBIST complete for R50 TMU4
PBIST complete for R50 TMU5
PBIST complete for R50 TMU6
PBIST complete for R51 TMU1
PBIST complete for R51 TMU2
PBIST complete for R51 TMU3
PBIST complete for R51 TMU4
PBIST complete for R51 TMU5
PBIST complete for R51 TMU6
PBIST complete for PBISTROM
PBIST complete for ROM0
PBIST complete for ROM1
PBIST complete for CPSW
PBIST complete for ECU_PERIPH
PBIST complete for FOTA
PBIST complete for ICSSM
PBIST complete for MBOX
PBIST complete for MSS_L2_1
PBIST complete for MSS_L2_2
PBIST complete for MSS_L2_3
PBIST complete for MSS_L2_4
PBIST complete for MSS_L2_5
PBIST complete for TPCC
PBIST complete for OSPI
PBIST complete for R5SS0 CPU0 RL2
PBIST complete for R5SS0 CPU1 RL2
PBIST complete for R5SS1 CPU0 RL2
PBIST complete for R5SS1 CPU1 RL2
PBIST complete for MSS R5SS0 C0
PBIST complete for MSS R5SS0 C1
PBIST complete for MSS R5SS1 C0
PBIST complete for MSS R5SS1 C1
PBIST complete for MSS MMCH0
PBIST complete for MSS MMCH1
PBIST complete for MSS CR5B R5FSS0 ATCM0
PBIST complete for MSS CR5B R5FSS1 ATCM0
PBIST complete for MSS CR5B R5FSS0 BTCM0
PBIST complete for MSS CR5B R5FSS1 BTCM0
PBIST complete for MSS R5FSS1 VIM0
PBIST complete for MSS R5FSS1 VIM1
All tests have passed.
PBIST test complete for TOP BIST
PBIST test completed in 8715 micro secs
[Cortex_R5_2]
PBIST Application
Starting PBIST failure insertion test on TOP PBIST
PBIST failure Insertion test complete for TOP BIST
PBIST Failure Insertion Test completed in 20 micro secs
Starting PBIST test on TOP PBIST
PBIST complete for R5 STC
PBIST complete for R51 STC
PBIST complete for R50 TMU1
PBIST complete for R50 TMU2
PBIST complete for R50 TMU3
PBIST complete for R50 TMU4
PBIST complete for R50 TMU5
PBIST complete for R50 TMU6
PBIST complete for R51 TMU1
PBIST complete for R51 TMU2
PBIST complete for R51 TMU3
PBIST complete for R51 TMU4
PBIST complete for R51 TMU5
PBIST complete for R51 TMU6
PBIST complete for PBISTROM
PBIST complete for ROM0
PBIST complete for ROM1
PBIST complete for CPSW
PBIST complete for ECU_PERIPH
PBIST complete for FOTA
PBIST complete for ICSSM
PBIST complete for MBOX
PBIST complete for MSS_L2_1
PBIST complete for MSS_L2_2
PBIST complete for MSS_L2_3
PBIST complete for MSS_L2_4
PBIST complete for MSS_L2_5
PBIST complete for TPCC
PBIST complete for OSPI
PBIST complete for R5SS0 CPU0 RL2
PBIST complete for R5SS0 CPU1 RL2
PBIST complete for R5SS1 CPU0 RL2
PBIST complete for R5SS1 CPU1 RL2
PBIST complete for MSS R5SS0 C0
PBIST complete for MSS R5SS0 C1
PBIST complete for MSS R5SS1 C0
PBIST complete for MSS R5SS1 C1
PBIST complete for MSS MMCH0
PBIST complete for MSS MMCH1
PBIST complete for MSS CR5B R5FSS0 ATCM0
PBIST complete for MSS CR5B R5FSS1 ATCM0
PBIST complete for MSS CR5B R5FSS0 BTCM0
PBIST complete for MSS CR5B R5FSS1 BTCM0
PBIST complete for MSS R5FSS1 VIM1
All tests have passed.
PBIST test complete for TOP BIST
PBIST test completed in 8846 micro secs