AM263Px MCU+ SDK  26.00.00
 RL2 Example

Introduction

Rl2 example provides how to use RL2 in applications and also shows how RL2 brings in benefits.

Supported Combinations

Parameter       Value
CPU + OS       r5fss0-0 nortos
Toolchain       ti-arm-clang
Boards         am263px-cc
Example folder examples/drivers/rl2

Steps to Run the Example

Sample Output

Starting OSPI Bootloader ...
[BOOTLOADER_PROFILE] Boot Media       : NOR SPI FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 133.333 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 0 KB
[BOOTLOADER_PROFILE] Cores present    :
r5f0-0
[BOOTLOADER PROFILE] System_init                      :        249us
[BOOTLOADER PROFILE] Drivers_open                     :         78us
[BOOTLOADER PROFILE] LoadHsmRtFw                      :        862us
[BOOTLOADER PROFILE] Board_driversOpen                :      30997us
[BOOTLOADER PROFILE] CPU load                         :         78us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      32267us
Image loading done, switching to application ...
L2 Cache:       i = 0   Miss = 129      Hits = 0
L2 Cache:       i = 1   Miss = 0        Hits = 129
L2 Cache:       i = 2   Miss = 0        Hits = 129
L2 Cache:       i = 3   Miss = 0        Hits = 129
L2 Cache:       i = 4   Miss = 0        Hits = 129
L2 Cache:       i = 5   Miss = 0        Hits = 129
L2 Cache:       i = 6   Miss = 0        Hits = 129
L2 Cache:       i = 7   Miss = 0        Hits = 129
L2 Cache:       i = 8   Miss = 0        Hits = 129
L2 Cache:       i = 9   Miss = 0        Hits = 129
Profile Point: With RL2
Cycle Count: 65854
No. Of CPU instructions executed Count: 21107
ICache Miss Count: 9
ICache Access Count: 65819
Profile Point: Without RL2
Cycle Count: 210590
No. Of CPU instructions executed Count: 20602
ICache Miss Count: 1
ICache Access Count: 210600
All tests have passed!!

Description

On how to configure RL2, please go through Configuring OptiFlash various IP.

This example shows how RL2 is used and how its different functions are used. With RL2 enabled, the function that was being executed is getting cached in the RL2 cache bank. First time, it caused 129 L2 cache misses, and because each L2 cache line (at a size of 128KB) is 32 bytes, it implies that a total of ~4KB of code is being cached. This is in alignment with the size of the function that is being executed from the flash. Later on, every time there were L2 cache hits,

Another point to highlight is performance improvement. This is clear from the cycle count with RL2 and without RL2.