This example shows usage of direct FreeRTOS APIs, i.e not via the DPL APIs. It shows usage of user mode task create API, task notification APIs, semaphore APIs. It also shows how to signal to FreeRTOS task from ISRs.
The example does below:-
Following tables summaries relevant memory map used by the example along with the static MPU regions configurations as well as the task specific MPU regions configurations,
| Memory Section | Origin | Size | Static MPU Region Mapping | Dynamic MPU Region Mapping |
|---|---|---|---|---|
| R5F_VECS | 0x00000000 | 64 B | [1]ATCM | - |
| R5F_TCMA | 0x00000040 | 31.9 KB | [1]ATCM | - |
| R5F_TCMB | 0x00080000 | 32 KB | [2]BTCM | - |
| FLASH | 0x60100000 | 512 KB | [6]FLASH | - |
| SBL | 0x70000000 | 256 KB | [3]OCRAM_BACKGROUND | - |
| OCRAM | 0x70040000 | 128 KB | [4]OCRAM_UNPRIVILEGED | - |
| PRIVILEGED_TEXT | 0x70060000 | 64 KB | [5]OCRAM_PRIVILEGED_TEXT | - |
| PRIVILEGED_DATA | 0x70070000 | 56 KB | [3]OCRAM_BACKGROUND | [8]Ping/Pong Task Stack Region |
| PING_TEXT | 0x7007E000 | 2 KB | [3]OCRAM_BACKGROUND | [9]Ping Task Region 0 |
| PING_DATA | 0x7007E800 | 2 KB | [3]OCRAM_BACKGROUND | [10]Ping Task Region 1 |
| PONG_TEXT | 0x7007F000 | 2 KB | [3]OCRAM_BACKGROUND | [9]Pong Task Region 0 |
| PONG_DATA | 0x7007F800 | 2 KB | [3]OCRAM_BACKGROUND | [10]Pong Task Region 1 |
| [idx]Static MPU Regions | Base Address | Size | Execute | Access Permissions |
|---|---|---|---|---|
| [0]BACKGROUND_REGION | 0x00000000 | 2 GB | No | Supervisor RW, User RW |
| [1]ATCM | 0x00000000 | 32 KB | Yes | Supervisor RW, User BLOCK |
| [2]BTCM | 0x00080000 | 32 KB | Yes | Supervisor RW, User BLOCK |
| [3]OCRAM_BACKGROUND | 0x70000000 | 2 MB | No | Supervisor RW, User BLOCK |
| [4]OCRAM_UNPRIVILEGED | 0x70040000 | 128 KB | Yes | Supervisor RW, User RW |
| [5]OCRAM_PRIVILEGED_TEXT | 0x70060000 | 64 KB | Yes | Supervisor RD, User BLOCK |
| [6]FLASH | 0x60100000 | 512 KB | Yes | Supervisor RD, User BLOCK |
| [idx]Ping/Pong Task MPU Regions | Base Address | Size | Execute | Access Permissions |
|---|---|---|---|---|
| [8]Stack Region | - | - | No | Supervisor RW, User RW |
| [9]PING_TEXT/PONG_TEXT | 0x7007E000/0x7007F000 | *2 KB | Yes | Supervisor RD, User RD |
| [10]PING_DATA/PONG_DATA | 0x7007E800/0x7007F800 | *2 KB | No | Supervisor RW, User RW |
Note:
The example source files are split to dedicated files to achieve following access restrictions,
task_switch_mpu.c is by default placed in privileged functions and privileged data sections respectively with following in linker script:- task_switch_mpu.c. Ping/Pong task stacks are defined in task_switch_mpu.c and will be placed in privileged data section. But as part of user task creation a dedicated MPU region will be configured for the task stack. task_switch_mpu_ping.c is by default placed in corresponding sections reserved for the ping task with the following in linker script:- __TEXT_PING_START, __TEXT_PING_END, __DATA_PING_START, __DATA_PING_END will be used to create the MPU regions for the ping task. Hence other user mode tasks won't have access to any of the text/data in task_switch_mpu_ping.c. task_switch_mpu_pong.c is by default placed in corresponding sections reserved for the pong task with the following in linker script:- __TEXT_PONG_START, __TEXT_PONG_END, __DATA_PONG_START, __DATA_PONG_END will be used to create the MPU regions for the pong task. Hence other user mode tasks won't have access to any of the text/data in task_switch_mpu_pong.c. task_switch_mpu_common.c is by default placed in generic text and data segments in OCRAM which falls under OCRAM_UNPRIVILEGED MPU region configuration. These will be accessible by user mode tasks unless explicitly specified by an attribute to place in a different dedicated section with reduced access permissions.task_switch_mpu.ctask_switch_mpu_ping.ctask_switch_mpu_pong.ctask_switch_mpu_common.c| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 freertos_mpu |
| Toolchain | ti-arm-clang |
| Boards | am263px-cc, am263px-lp |
| Example folder | examples/kernel/freertos/task_switch_mpu |
Shown below is a sample output when the application is run,