AM263Px MCU+ SDK  26.00.00
LIN SCI Internal Loopback Interrupt

Introduction

This example is a application which demonstrates the SCI message communication. Instance LIN1 is set to Transmit as well as Recieve.

The LIN1 instance initiates the transmission by sending SCI bytes. It receives the same message.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/lin/lin_sci_loopback

Steps to Run the Example

See Also

LIN

Sample Output

Shown below is a sample output when the application is run,

[LIN] SCI Loopback mode, application started ...
All tests have passed!!