AM263Px MCU+ SDK  26.00.00
SBL CAN UNIFLASH

Introduction

This is a flash-writer application which can boot the application as well. This works in conjunction with the can_uniflash.py python script. It uses bootloader APIs to do basic SOC initialization required to be able to flash binaries to the QSPI flash. Like other SBLs, this is also booted by the ROM bootloader.

Once the example starts running it attempts to receive files via CAN interface and process them in a loop. Once it receives a file (this is sent by the can_uniflash.py script), it finds out what to do with the received file from the file header. This can be primarily used for Flashing the received file at the given offset.

MCAN SBL CAN UNIFLASH Process

This bootloader runs in two steps:

  • Flashing the SBL CAN UNIFLASH at offset 0x0 (Setup the EVM in UART Boot Mode)
  • Running the can_uniflash.py python script for sending the application image file. (Setup the EVM in QSPI Boot Mode)

MCAN SBL CAN UNIFLASH Flow Overview

Refer Steps to Run the Example

SBL CAN Uniflash Multicore ELF

  • For AM26xx devices, use the Multicore ELF project of SBL CAN Uniflash
  • To flash an mcelf file via CAN uniflash, use the project examples/drivers/boot/sbl_can_uniflash_multicore_elf

Protocol

A simple custom made protocol is created for communication between the Host Machine and the Board. Messages between a CAN bootloader host and the target use a simple command and acknowledge (ACK) protocol. The host sends a command and within a timeout period the target responds with an ACK.

The CAN Uniflash provides a short list of commands that are used during the flashing operation.

Commands Description
PING This command is used to receive an PONG command from the bootloader indicating that communication has been established.
PONG Returned as response to the initial PING command from the Bootloader
DATA To send data packets
RUN To run the application
ACK Response from the Bootloader on recieveing the CAN Packets
LSTMSG To indicate the last data packet of the application
LSTMSGCF Response from the Bootloader on recieveing the last data packet of the application

Please refer the image below:

SBL CAN Communication Protocol between Host Machine and the Board

Settings Used in this Application

In this application, the CAN settings are:

  • Extended Identifier used
  • Make Sure to set correct timing parameters. Current parameters is as per SDK-CAN driver.
    • BitrateFD : f_clock_mhz=80, nom_brp=1, nom_tseg1=67, nom_tseg2=12, nom_sjw=12, data_brp=1, data_tseg1=13, data_tseg2=2, data_sjw=1
  • CAN-FD is supported
  • Refer to MCAN, for MCAN dependencies.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-lp
Example folder examples/drivers/boot/sbl_can_uniflash_multicore_elf

NOTE: Tested on Windows, using PCAN-USB Peripheral.

Steps to Run the Example

Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from a QSPI boot media unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.

  • Example is tested using PCAN-USB module
  • Hardware Conectivity, First make sure the connections to the PCAN-USB module to PC are proper. Connect the PCAN-USB module to PC from USB and Serial Port to be connected as mentioned in the image below.

MCAN Hardware Connectivity with PCAN USB.
  • Software Setup, To use SBL CAN using PCAN-USB Peripheral,First Download and Install the PCAN-Driver from https://www.peak-system.com/Drivers.523.0.html?&L=1
    • Peak Systems provides PCAN-Basic API for Connecting to CAN and CAN FD Buses. PCAN-Basic consists of the actual device driver and an interface DLL, which provides the API functions. It can be downloaded from here, https://www.peak-system.com/PCAN-Basic.239.0.html?&L=1
    • After downloading the PCAN-Basic, please extract it. PCAN-Basic directory contains PCANBasic.py python file, under
      .\pcan-basic\PCAN-Basic API\Include\PCANBasic.py
    • Create a folder named pcan at following location in SDK directory:
      ${SDK_INSTALL_PATH}/tools/boot/pcan
    • We've to place this PCANBasic.py python file under this folder in SDK:
      ${SDK_INSTALL_PATH}/tools/boot/pcan/PCANBasic.py
    • PCANBasic.dll library needs to be installed in order to run applications that use this API. PCAN Device Driver application also installs PCANBasic.dll library. Please refer https://www.peak-system.com/produktcd/Develop/PC%20interfaces/Windows/PCAN-Basic%20API/ReadMe.txt for more information on this.
    • Interface DLL file needs to be present in the following windows directory:
      For x64 Windows systems:
      \x86\PCANBasic.dll --> Windows\SysWOW64
      \x64\PCANBasic.dll --> Windows\System32
    • One can use the Microsoft sigcheck tool (can be dowloaded from https://learn.microsoft.com/en-us/sysinternals/downloads/sigcheck) to find out if your PCANBasic.dll file is 32 or 64 bit version.
      sigcheck.exe C:\Windows\SysWOW64\PCANBasic.dll
  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • After hardware and software setup follow below steps to run the example:
    • First the SBL CAN bootloader will be flashed.
    • Create a flash configuration file, using the default flash configuration file present, at below as reference
${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/{board}/default_sbl_can_uniflash.cfg
  • In this config file, modify the paths to the flashing application and CAN bootloader, in case you are not using the pre-built applications
--flash-writer={path to flash application .tiimage}
--file={path to CAN Uniflash .tiimage} --operation=flash --flash-offset=0x0
  • Run below python command on the Windows command prompt (cmd.exe) or Linux bash shell to flash the files.
cd ${SDK_INSTALL_PATH}/tools/boot
python uart_uniflash.py -p {name of your UART com port} --cfg={path to your edited config file}
  • Refer to the page Basic steps to flash files for more information
  • After flashing the bootloader, Setup the EVM in QSPI Boot Mode.
  • CAN Uniflash Python Script
  • For sending the application image mcelf_sbl_can_uniflash_app.cfg can be editted with the path of the image of the desired application.
  • cfg file contains only one command with arguments like –file, –operation and –flash-offset.
    For AM263Px, Default Flash Offset is at 0x81000.
    --file={SDK_PATH}/examples/drivers/ipc/ipc_rpmsg_echo/am263px-lp/system_freertos_nortos/ipc_rpmsg_echo_system.debug.mcelf --operation=flash-sector-write --flash-offset=0x81000
  • The application image file is sent using can_uniflash.py python script:
cd ${SDK_INSTALL_PATH}/tools/boot
python can_uniflash.py --cfg={path to your edited sbl_can_uniflash_app config file}

See Also

BOOTLOADER

Sample Output

After sending the application image over CAN, logs can be seen on the UART terminal