AM263Px MCU+ SDK  26.00.00
OSPI Graph Plotter

Introduction

This example is used to plot the ospi phy tuning sweep on a graph.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/ospi/ospi_graph_plotter

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Use the python script provided with the example to plot the graph -> python phy_tuning_graph_plotter.py path/to/generated/bin/file .

See Also

OSPI

Sample Output

Sweeping... !!!
Writing to file: graph.bin
All tests have passed!!