AM263Px MCU+ SDK  26.00.00
GPIO MULTI LED Blink

Introduction

This example configures multiple GPIO pins connected to LEDs on the EVM in output mode. The application toggles the each LED on/off for 10 seconds and exits.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-cc
Example folder examples/drivers/gpio/gpio_multi_led_blink/

Steps to Run the Example

AM263PX-CC

  • Watch out for LEDs LD6 and LD7 on the CC to blink.

See Also

GPIO

Sample Output

Shown below is a sample output when the application is run,

GPIO Multi LED Blink Test Started ...
Each LED will Blink for 10 seconds ...
GPIO Multi LED Blink Test Passed!!
All tests have passed!!