AM263Px MCU+ SDK  26.00.00
Using FOTA Agent (FSS Switch To B)

Introduction

This example provides a simple use case on how to implement a FOTAAgent in a FOTA use case. FOTAAgent is used to write files received on the interface to the flash.

Hello world application is being embedded into this example as a C array which is then programmed using FOTAAgent (FOTA Agent) APIs. However, in a real-world use case, a new application will be received on some interface (eg. CAN, Ethernet, etc.) in some packets.

This application, flash the program using the following loop:

for (uint32_t cnt = 0; cnt < hello_world_release_xip_size; cnt++)
{
/*
as and when a byte is being recv, it is being sent to agent which will handle
all the intricacies.
*/
uint8_t byte = hello_world_release_xip[cnt];
status = FOTAAgent_writeUpdate(&gFotaAgentHandle, &byte, 1);
DebugP_assert(status == SystemP_SUCCESS);
}

In the actual application, for loop can be replaced with a while loop, which would terminate when all the packets have been received.

Typically, after application compilation, TI post-build step produces .mcelf and .mcelf_xip files. It is required to flash these 2 files in the flash. Therefore, it is required to call FOTAAgent API 2 times on these 2 files.

Once both the files are flashed in the external flash, it is required to update the boot sector of the flash.

offset = BOOINFO_ADDRESS;
CacheP_inv((void *)(SOC_getFlashDataBaseAddr() + offset), ERASE_SECTOR_SIZE, CacheP_TYPE_ALL);
memcpy((void *)&bootinfo.bin, (void *)(SOC_getFlashDataBaseAddr() + offset), ERASE_SECTOR_SIZE);
bootinfo.fields.bootRegion = BOOT_REGION_B;
status = FLSOPSKD_erase(&gFotaAgentHandle.flopsHandle, offset);
DebugP_assert(status == SystemP_SUCCESS);
status = FLSOPSKD_write(&gFotaAgentHandle.flopsHandle, offset, (uint8_t *)&bootinfo.bin, ERASE_SECTOR_SIZE);
DebugP_assert(status == SystemP_SUCCESS);
CacheP_inv((void *)(SOC_getFlashDataBaseAddr() + offset), ERASE_SECTOR_SIZE, CacheP_TYPE_ALL);

The above code does that.

If the SBL OSPI SWAP is being used, the on next board reset, hello world application will run instead of this application.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc
Example folder examples/drivers/fss/fss_switch_b

Steps to Run the Example

Sample Output

Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 133.333 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 66 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init : 599us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 136us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 9337us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 2757us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 4838us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 18us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 17687us
Image loading done, switching to application ...
Starting application
Receiving application...
Got MCELF file
Got MCELF_XIP file
Done writing new application to flash...
Updating Flash's Boot Sector...
Finish Updating Flash's Boot Sector... Please reset board to start new application
Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 133.333 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 7 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init : 599us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 136us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 9336us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 2766us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 3787us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 18us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 16644us
Image loading done, switching to application ...
Hello World!