AM263Px MCU+ SDK  26.00.00
CANFD Loopback Interrupt

Introduction

This example demonstrates the CAN message transmission and reception in digital loop back mode for standard and extended CAN with the following configuration.

  • Message ID for standard and extended CAN is 0x1C and 0x29E respectively.
  • MCAN is configured in Interrupt Mode.
  • Arbitration Bit Rate 1Mbps.
  • Data Bit Rate 5Mbps.
  • Buffer mode is used for Tx and RX to store message in message RAM.

Message is transmitted and received back internally using internal loopback mode. When the received message id and the data matches with the transmitted one, then the example is completed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263px-cc, am263px-lp
Example folder examples/drivers/mcan/canfd_loopback_interrupt_std_exd

Steps to Run the Example

See Also

CANFD (HLD)

Sample Output

Shown below is a sample output when the application is run,

[MCAN] Loopback Interrupt mode for Standard and Extended CAN test application started ...
MCAN Extended mode test started..
MCAN Extended mode test passed.
MCAN Standard mode test started..
MCAN Standard mode test passed.
All tests have passed!!