AM263Px MCU+ SDK  26.00.00
Torque Measurement

Introduction

Predicting rotor torque in motors presents a significant engineering challenge: direct measurement requires costly sensors that add weight, a critical concern for electric vehicles striving for efficiency. While traditional statistical methods for estimating rotor torque exist, they are limited by the need for domain expertise and motor-specific tuning.

This project leverages deep learning to efficiently predict rotor torque in Permanent Magnet Synchronous Motors (PMSM), enabling a substantial reduction in the hardware sensors required for motor instrumentation and control.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263px-lp
Example folder examples/ai/torque_measurement/

Dataset and Model Details

Dataset

The dataset contains sensor measurements collected from a PMSM running on a controlled test bench. The measurements were collected by the LEA department at Paderborn University at 2 Hz sampling rate.

Column Name Description
i_d Current d-component (active)
i_q Current q-component (reactive)
u_d Voltage d-component (active)
u_q Voltage q-component (reactive)
motor_speed Motor speed
ambient Ambient temperature
torque Torque induced by current (target)

The model uses a subset of easily measurable inputs: Ambient temperature, Coolant temperature, Voltage components (u_d, u_q), and Phase current magnitude to predict torque.

Model Architecture

This regression model REGR_10k contains approximately 10,000 parameters with three convolutional layers (each with BatchNorm and ReLU) followed by two linear layers.

Input Features

The model takes 4D input (N,C,H,W):

  • N (1): batch size which is restricted to 1
  • C (10): channels for multiple parameters
  • H (128): samples of timeseries data
  • W (1): width of samples is restricted to 1 for timeseries applications

Output

This model produces a 1D output representing the continuous value of torque.

Feature Extraction Configuration

For this torque measurement system, no FFT or frequency-domain feature extraction is applied. The model uses normalization to convert floating point input into fixed point for efficient inference.

Configuration in user_input_config.h:

  • SKIP_NORMALIZE: Converts floating point input into fixed point input for the AI model

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • The application will predict torque values and compare against expected outputs

See Also

AI Examples

Sample Output

Torque Measurement Example Started ...
Feature extraction mismatches 0
All tests have passed!!
Golden vectors matched: 3 not matched: 0