Traditional HVAC controllers are reactive - they respond to temperature deviations only after they occur, leading to delayed corrections, unnecessary compressor cycling, and wasted energy. A smarter approach is to anticipate what the indoor temperature will be in the near future and act preemptively.
This project demonstrates on-device machine learning for HVAC control. A compact LSTM model running directly on the AM26x MCU predicts upcoming temperature trends from recent sensor readings, enabling smoother, more energy-efficient control decisions without relying on cloud connectivity.
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-lp |
| Example folder | examples/ai/hvac_indoor_temp_forecast/ |
This example uses a synthetic HVAC dataset designed to emulate realistic indoor thermal dynamics. The dataset captures the interplay between compressor operation, outdoor conditions, and the resulting indoor temperature.
| Parameter | Value |
|---|---|
| Signals | compressorFrequency, outdoorTemperature, indoorTemperature |
| Input Variables | 3 |
| Prediction Target | indoorTemperature (next timestep) |
The model learns to predict the indoor temperature at the next timestep given the past 5 readings of all three signals.
The model is FCST_LSTM10, a single-layer LSTM network with a hidden size of 10 and approximately 611 trainable parameters. LSTM gating mechanisms capture the temporal dependencies between compressor activity, outdoor conditions, and the resulting indoor temperature trajectory.
The model takes 4D input (N,C,H,W):
The model produces an output tensor of shape (1, 1, 1, 1), representing the predicted indoor temperature at the next timestep (forecast_horizon = 1). This is a continuous forecasting output that can be fed directly into a downstream control algorithm.
A SimpleWindow transform segments the continuous stream into fixed-length windows of 5 consecutive timesteps across all 3 input channels. No FFT, binning, or log scaling is applied - the LSTM model learns directly from raw sensor values.