Introduction
This example demonstrates the Device Agent Protocol (DAP) communication layer used for integration with Edge AI Studio. DAP provides a standardized UART-based protocol for streaming sensor data, receiving commands, and transmitting inference results between the microcontroller and Edge AI Studio.
This example serves as a reference implementation for:
- Establishing DAP communication with Edge AI Studio
- Implementing sensor data streaming
- Handling pipeline configuration commands
- Transmitting inference results
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263px-lp |
| Example folder | examples/ai/dap_default/ |
DAP Protocol Overview
The Device Agent Protocol (DAP) provides:
- Frame-based communication: CRC-validated frames for reliable data transfer
- Multiple data channels: Support for sensor signals, inference signals, results, values, and logs
- Command handling: Pipeline configuration and control commands from Edge AI Studio
- Multi-sensor streaming: Support for streaming data from multiple sensors simultaneously
Key DAP Functions
| Function | Description |
Dap_Init() | Initialize DAP instance |
Dap_Process() | Main processing loop |
Dap_SendSensorData() | Stream sensor data |
Dap_StartSensorStream() | Start sensor streaming |
Dap_StopSensorStream() | Stop sensor streaming |
Dependencies
- Edge AI Studio for communication
- UART interface for DAP protocol
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Connect Edge AI Studio to the device via UART
See Also
AI Examples
Sample Output
[DAP] Example started...
[DAP] Initialized successfully. Waiting for commands...