AM263Px MCU+ SDK
26.00.00
Enet CPSW Operation Modes Demo
Table of Contents
Introduction
CPSW DUAL MAC Mode
See Also
Introduction
CPSW operates in two modes
Switch Mode - packet forwarding is enabled and packets are forwarded to Host + Other MAC ports. This is the default configuration for CPSW.
MAC mode - packets are only given to the Host port and are not forwarded to other MAC Ports.
CPSW DUAL MAC Mode
In this mode, both the MAC ports of AM263PX are configured to be in MAC mode.
This mode requires two Network interfaces to operate.
It is recommended to use two separate subnets for working with DUAL MAC.
A single implementation of network interface and shared pool is used for both the Netifs.
Dual MAC feature is illustrated by the below image:
DUAL MAC Operation
See Also
Ethernet And Networking
generated by
1.8.20