AM263Px MCU+ SDK  26.00.00
PMIC

The PMIC driver provides API to control SPI based PMIC present in the board. It supports configuration of various features/modules in the PMIC. MCSPI controller is used to read/write to the PMIC registers. Refer to the corresponding PMIC datasheet for more details.

Features Supported

  • Support enable/disable watchdog
  • Watchdog in Trigger and Q&A mode with interrupt/reset support upon failure
  • GPIO configuration
  • Thermal monitoring
  • Voltage monitoring
  • IRQ
  • ESM

SysConfig Features

NA

Features NOT Supported

  • NA

Important Usage Guidelines

  • Power cycle the board to restore the PMIC register configurations.

Example Usage

Include the below file to access the APIs

#include <board/pmic.h>

Instance Open Blackbird PMIC Example

PMIC_Params gPmicParams[CONFIG_PMIC_NUM_INSTANCES] =
{
{
.deviceType = PMIC_DEV_BB_TPS65386X,
.commMode = PMIC_INTF_SPI,
.instType = PMIC_MAIN_INST,
.instance = CONFIG_MCSPI0,
},
};
PMIC_Handle[CONFIG_PMIC0] = PMIC_open(CONFIG_PMIC0, &gPmicParams[CONFIG_PMIC0]);
/*gPmicHandle[CONFIG_PMIC0] return from PMIC_open*/
PMIC_configure(gPmicHandle[CONFIG_PMIC0]);

Instance Close Example

PMIC_close(gPmicHandle[CONFIG_PMIC0]);

API

APIs for I2C/MCSPI based PMIC driver

PMIC_close
void PMIC_close(PMIC_Handle handle)
Close PMIC driver.
pmic.h
PMIC_open
PMIC_Handle PMIC_open(uint32_t instanceId, const PMIC_Params *params)
Open PMIC driver.
PMIC_configure
int32_t PMIC_configure(PMIC_Handle handle)
Configure PMIC driver.
PMIC_Handle
void * PMIC_Handle
Handle to the PMIC driver returned by PMIC_open()
Definition: pmic.h:73