Structure representing the cb_socket_lldcfg_update instance.
Data Fields | |
| const char * | dev |
| uint16_t | proto |
| uint16_t | vlanid |
| uint32_t | nTxPkts |
| uint32_t | nRxPkts [MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
| uint32_t | pktSize |
| int | dmaTxChId |
| int | dmaRxChId [MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
| int | dmaTxShared |
| int | dmaRxShared |
| int | dmaRxOwner |
| void(* | rxDefaultDataCb )(void *data, int size, int port, void *cbArg) |
| void * | rxDefaultCbArg |
| int | numRxChannels |
| const char* cb_socket_lldcfg_update_t::dev |
Device name to match the expected socket.
| uint16_t cb_socket_lldcfg_update_t::proto |
Protocol or ethernet type in the ethernet frame header to match the expected socket.
| uint16_t cb_socket_lldcfg_update_t::vlanid |
VLAN ID to match the expected socket.
| uint32_t cb_socket_lldcfg_update_t::nTxPkts |
Number of buffers allocated for transmit packets Positive value will be updated to LLDEnetCfg_t.
| uint32_t cb_socket_lldcfg_update_t::nRxPkts[MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
Number of buffers allocated for receive packets Positive value will be updated to LLDEnetCfg_t.
| uint32_t cb_socket_lldcfg_update_t::pktSize |
Transmit and receive maximum packet size. Positive value will be updated to LLDEnetCfg_t.
| int cb_socket_lldcfg_update_t::dmaTxChId |
DMA transmit channel ID. 0 or positive value will be updated to LLDEnetCfg_t
| int cb_socket_lldcfg_update_t::dmaRxChId[MAX_NUM_RX_DMA_CH_PER_INSTANCE] |
DMA receive channel ID. 0 or positive value will be updated to LLDEnetCfg_t
| int cb_socket_lldcfg_update_t::dmaTxShared |
Only Sitara support this param. >0: the dmaTxChId is shared between apps; 0: not shared 0 or positive value will be updated to LLDEnetCfg_t
| int cb_socket_lldcfg_update_t::dmaRxShared |
Only Sitara AM273x support this param. >0: the dmaRxChId is shared between apps; 0: not shared 0 or positive value will be updated to LLDEnetCfg_t
| int cb_socket_lldcfg_update_t::dmaRxOwner |
Only Sitara AM273x support this param. >0: the socket owns this RX DMA channel; 0: not own 0 or positive value will be updated to LLDEnetCfg_t
| void(* cb_socket_lldcfg_update_t::rxDefaultDataCb) (void *data, int size, int port, void *cbArg) |
Only Sitara AM273x support this param. Default RX data callback when there is no matching RX filter.
| void* cb_socket_lldcfg_update_t::rxDefaultCbArg |
Only Sitara AM273x support this param. Default RX data callback arg
| int cb_socket_lldcfg_update_t::numRxChannels |
Number of Rx DMA channels, only ICSSG peripheral has more than 1 Rx DMA channels.