MPU Firewall Target.
This structure contains parameters associated with an MPU Firewall memory map target.
Data Fields | |
| uint32_t | startAddr |
| uint32_t | regionSize |
| uint32_t Firewall_Target::startAddr |
Start address of the target
| uint32_t Firewall_Target::regionSize |
Size of the region