AM263Px MCU+ SDK  11.00.00
Diag_Mon_ExcFreq_Degradataion_data Struct Reference

Detailed Description

Structure to hold the control/status data for Diagnostics mentioned under Monitor excitation frequency degradation or loss (DOS)

Values that can be passed to RDC_getDiagnosticsExcFreqDegradationData(), RDC_setDiagnosticsExcFreqDegradationData() as Diag_Mon_ExcFreq_Degradataion_data parameter

Data Fields

uint16_t excfreqdetected_sin
 
uint16_t excfreqdetected_cos
 
uint16_t excfreqdrift_threshold_hi
 
uint16_t excfreqdrift_threshold_lo
 
uint16_t excfreq_level
 
uint8_t excfreqdrift_glitchcount
 
bool excfreqdrift_hi
 
bool excfreqdrift_cos_lo
 
bool excfreqdrift_sin_lo
 
bool excfreqdrift_en
 

Field Documentation

◆ excfreqdetected_sin

uint16_t Diag_Mon_ExcFreq_Degradataion_data::excfreqdetected_sin

◆ excfreqdetected_cos

uint16_t Diag_Mon_ExcFreq_Degradataion_data::excfreqdetected_cos

◆ excfreqdrift_threshold_hi

uint16_t Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_threshold_hi

◆ excfreqdrift_threshold_lo

uint16_t Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_threshold_lo

◆ excfreq_level

uint16_t Diag_Mon_ExcFreq_Degradataion_data::excfreq_level

◆ excfreqdrift_glitchcount

uint8_t Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_glitchcount

◆ excfreqdrift_hi

bool Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_hi

◆ excfreqdrift_cos_lo

bool Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_cos_lo

◆ excfreqdrift_sin_lo

bool Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_sin_lo

◆ excfreqdrift_en

bool Diag_Mon_ExcFreq_Degradataion_data::excfreqdrift_en