AM263Px MCU+ SDK  11.00.00
Diag_Mon_Cos_Phase_drift_data Struct Reference

Detailed Description

Structure to hold the control/status data for Diagnostics mentioned under Monitor Cos Phase drift (DOS)

Values that can be passed to RDC_getDiagnosticsCosPhaseDriftData(), RDC_setDiagnosticsCosPhaseDriftData() as Diag_Mon_Cos_Phase_drift_data parameter

Data Fields

int16_t phase_drift_threshold_hi
 
int16_t phase_drift_threshold_lo
 
uint8_t phase_drift_glitch_count
 
bool phase_drift_cos_hi
 
bool phase_drift_cos_lo
 
bool phase_drift_en
 

Field Documentation

◆ phase_drift_threshold_hi

int16_t Diag_Mon_Cos_Phase_drift_data::phase_drift_threshold_hi

◆ phase_drift_threshold_lo

int16_t Diag_Mon_Cos_Phase_drift_data::phase_drift_threshold_lo

◆ phase_drift_glitch_count

uint8_t Diag_Mon_Cos_Phase_drift_data::phase_drift_glitch_count

◆ phase_drift_cos_hi

bool Diag_Mon_Cos_Phase_drift_data::phase_drift_cos_hi

◆ phase_drift_cos_lo

bool Diag_Mon_Cos_Phase_drift_data::phase_drift_cos_lo

◆ phase_drift_en

bool Diag_Mon_Cos_Phase_drift_data::phase_drift_en