Data structure containing information about the operating mode specific to the SOC.
This structure is used to store the data about Lock step or Stand alone mode as provided by the user in the syscfg.
Data Fields | |
| uint32_t | r5fss0_opMode |
| uint32_t | r5fss1_opMode |
| uint32_t Bootloader_socCoreOpModeConfig::r5fss0_opMode |
[IN] Operating mode for first R5 subsystem
| uint32_t Bootloader_socCoreOpModeConfig::r5fss1_opMode |
[IN] Operating mode for second R5 subsystem