This module contains APIs to program and use the DTHE AES.
Files | |
| file | dthe_aes.h |
| This file contains the prototype of DTHE AES driver APIs. | |
Data Structures | |
| struct | DTHE_AES_Params |
| AES Driver Parameters This structure has all the parameters which are need by the AES Driver to perform the specified operation. More... | |
Functions | |
| DTHE_AES_Return_t | DTHE_AES_open (DTHE_Handle handle) |
| Function to Open DTHE AES Driver. More... | |
| DTHE_AES_Return_t | DTHE_AES_execute (DTHE_Handle handle, const DTHE_AES_Params *ptrParams) |
| The function is used to execute the AES Driver with the specified parameters. More... | |
| DTHE_AES_Return_t | DTHE_AES_close (DTHE_Handle handle) |
| Function to close DTHE AES Driver. More... | |
Enumerations | |
| enum | DTHE_AES_Return_t { DTHE_AES_RETURN_SUCCESS = 0x62E699D9U, DTHE_AES_RETURN_FAILURE = 0x904D041AU } |
| DTHE AES Driver Error code. More... | |
Macros | |
| #define | DTHE_AES_ECB_MODE (0x00000000U) |
| Flag for AES ECB Mode. More... | |
| #define | DTHE_AES_CBC_MODE (0x00000001U) |
| Flag for AES CBC Mode. More... | |
| #define | DTHE_AES_CTR_MODE (0x00000002U) |
| Flag for AES CTR Mode. More... | |
| #define | DTHE_AES_ICM_MODE (0x00000004U) |
| Flag for AES ICM Mode. More... | |
| #define | DTHE_AES_CFB_MODE (0x00000008U) |
| Flag for AES CFB Mode. More... | |
| #define | DTHE_AES_F8_MODE (0x00000010U) |
| Flag for AES F8 Mode. More... | |
| #define | DTHE_AES_F9_MODE (0x00000020U) |
| Flag for AES F9 Mode. More... | |
| #define | DTHE_AES_XTS_MODE (0x00000040U) |
| Flag for AES XTS Mode. More... | |
| #define | DTHE_AES_CBC_MAC_MODE (0x00000080U) |
| Flag for AES CBC-MAC Mode. More... | |
| #define | DTHE_AES_CMAC_MODE (0x00000100U) |
| Flag for AES CMAC Mode. More... | |
| #define | DTHE_AES_GCM_MODE (0x00000200U) |
| Flag for AES GCM Mode. More... | |
| #define | DTHE_AES_GHASH_ONLY_MODE (0x00000400U) |
| Flag for AES GCM Mode. More... | |
| #define | DTHE_AES_CCM_MODE (0x00000800U) |
| Flag for AES CCM Mode. More... | |
| #define | DTHE_AES_KEY_128_SIZE (0x00000001U) |
| Size of AES key is of 128-bit. More... | |
| #define | DTHE_AES_KEY_192_SIZE (0x00000002U) |
| Size of AES key is of 192-bit. More... | |
| #define | DTHE_AES_KEY_256_SIZE (0x00000003U) |
| Size of AES key is of 256-bit. More... | |
| #define | DTHE_AES_ENCRYPT (0x016FE45DU) |
| AES Encrypt Flag. More... | |
| #define | DTHE_AES_DECRYPT (0xDCBA4213U) |
| AES Decrypt Flag. More... | |
| #define | DTHE_AES_CTR_WIDTH_16 (0x00000001U) |
| AES CTR Counter Width is 16 (ICM) More... | |
| #define | DTHE_AES_CTR_WIDTH_32 (0x00000002U) |
| AES CTR Counter Width is 32. More... | |
| #define | DTHE_AES_CTR_WIDTH_64 (0x00000004U) |
| AES CTR Counter Width is 64. More... | |
| #define | DTHE_AES_CTR_WIDTH_96 (0x00000008U) |
| AES CTR Counter Width is 96. More... | |
| #define | DTHE_AES_CTR_WIDTH_128 (0x00000010U) |
| AES CTR Counter Width is 128. More... | |
| #define | DTHE_AES_ONE_SHOT_SUPPORT (0x00000000U) |
| AES STREAM SUPPORT. More... | |
| #define | DTHE_AES_STREAM_INIT (0xAA11BB22U) |
| AES STREAM SUPPORT : INIT. More... | |
| #define | DTHE_AES_STREAM_UPDATE (0x33CC44DDU) |
| AES STREAM SUPPORT : UPDATE. More... | |
| #define | DTHE_AES_STREAM_FINISH (0xEE55FF66U) |
| AES STREAM SUPPORT : FINISH. More... | |
| #define | DTHE_AES_NO_MODE (0x0U) |
| AES No Mode Suppored. More... | |
| #define | DTHE_AES_GCM_MODE_1 (0x1U) |
| AES GCM Operation Select Mode 1. More... | |
| #define | DTHE_AES_GCM_MODE_2 (0x2U) |
| AES GCM Operation Select Mode 2. More... | |
| #define | DTHE_AES_GCM_MODE_3 (0x3U) |
| AES GCM Operation Select Mode 3. More... | |
| #define | DTHE_AES_XTS_MODE_1 (0x1U) |
| AES XTS Operation Select Mode 1. More... | |
| #define | DTHE_AES_XTS_MODE_2 (0x2U) |
| AES XTS Operation Select Mode 2. More... | |
| #define | DTHE_AES_XTS_MODE_3 (0x3U) |
| AES XTS Operation Select Mode 3. More... | |
| #define DTHE_AES_ECB_MODE (0x00000000U) |
Flag for AES ECB Mode.
| #define DTHE_AES_CBC_MODE (0x00000001U) |
Flag for AES CBC Mode.
| #define DTHE_AES_CTR_MODE (0x00000002U) |
Flag for AES CTR Mode.
| #define DTHE_AES_ICM_MODE (0x00000004U) |
Flag for AES ICM Mode.
| #define DTHE_AES_CFB_MODE (0x00000008U) |
Flag for AES CFB Mode.
| #define DTHE_AES_F8_MODE (0x00000010U) |
Flag for AES F8 Mode.
| #define DTHE_AES_F9_MODE (0x00000020U) |
Flag for AES F9 Mode.
| #define DTHE_AES_XTS_MODE (0x00000040U) |
Flag for AES XTS Mode.
| #define DTHE_AES_CBC_MAC_MODE (0x00000080U) |
Flag for AES CBC-MAC Mode.
| #define DTHE_AES_CMAC_MODE (0x00000100U) |
Flag for AES CMAC Mode.
| #define DTHE_AES_GCM_MODE (0x00000200U) |
Flag for AES GCM Mode.
| #define DTHE_AES_GHASH_ONLY_MODE (0x00000400U) |
Flag for AES GCM Mode.
| #define DTHE_AES_CCM_MODE (0x00000800U) |
Flag for AES CCM Mode.
| #define DTHE_AES_KEY_128_SIZE (0x00000001U) |
Size of AES key is of 128-bit.
| #define DTHE_AES_KEY_192_SIZE (0x00000002U) |
Size of AES key is of 192-bit.
| #define DTHE_AES_KEY_256_SIZE (0x00000003U) |
Size of AES key is of 256-bit.
| #define DTHE_AES_ENCRYPT (0x016FE45DU) |
AES Encrypt Flag.
| #define DTHE_AES_DECRYPT (0xDCBA4213U) |
AES Decrypt Flag.
| #define DTHE_AES_CTR_WIDTH_16 (0x00000001U) |
AES CTR Counter Width is 16 (ICM)
| #define DTHE_AES_CTR_WIDTH_32 (0x00000002U) |
AES CTR Counter Width is 32.
| #define DTHE_AES_CTR_WIDTH_64 (0x00000004U) |
AES CTR Counter Width is 64.
| #define DTHE_AES_CTR_WIDTH_96 (0x00000008U) |
AES CTR Counter Width is 96.
| #define DTHE_AES_CTR_WIDTH_128 (0x00000010U) |
AES CTR Counter Width is 128.
| #define DTHE_AES_ONE_SHOT_SUPPORT (0x00000000U) |
AES STREAM SUPPORT.
| #define DTHE_AES_STREAM_INIT (0xAA11BB22U) |
AES STREAM SUPPORT : INIT.
| #define DTHE_AES_STREAM_UPDATE (0x33CC44DDU) |
AES STREAM SUPPORT : UPDATE.
| #define DTHE_AES_STREAM_FINISH (0xEE55FF66U) |
AES STREAM SUPPORT : FINISH.
| #define DTHE_AES_NO_MODE (0x0U) |
AES No Mode Suppored.
| #define DTHE_AES_GCM_MODE_1 (0x1U) |
AES GCM Operation Select Mode 1.
| #define DTHE_AES_GCM_MODE_2 (0x2U) |
AES GCM Operation Select Mode 2.
| #define DTHE_AES_GCM_MODE_3 (0x3U) |
AES GCM Operation Select Mode 3.
| #define DTHE_AES_XTS_MODE_1 (0x1U) |
AES XTS Operation Select Mode 1.
| #define DTHE_AES_XTS_MODE_2 (0x2U) |
AES XTS Operation Select Mode 2.
| #define DTHE_AES_XTS_MODE_3 (0x3U) |
AES XTS Operation Select Mode 3.
| enum DTHE_AES_Return_t |
| DTHE_AES_Return_t DTHE_AES_open | ( | DTHE_Handle | handle | ) |
Function to Open DTHE AES Driver.
| handle | DTHE_Handle returned from DTHE_open(). |
| DTHE_AES_Return_t DTHE_AES_execute | ( | DTHE_Handle | handle, |
| const DTHE_AES_Params * | ptrParams | ||
| ) |
The function is used to execute the AES Driver with the specified parameters.
| handle | DTHE_Handle returned from DTHE_open(). |
| ptrParams | Pointer to the parameters to be used to execute the driver. |
| DTHE_AES_Return_t DTHE_AES_close | ( | DTHE_Handle | handle | ) |
Function to close DTHE AES Driver.
| handle | DTHE_Handle returned from DTHE_open(). |