AM263Px MCU+ SDK  11.00.00

Introduction

Functions

int32_t SDL_TOG_getIntrCountInternal (uint32_t baseAddr, SDL_TOG_IntrSrc intrSrc, uint32_t *pIntrCnt)
 Read internal interrupt count. More...
 
int32_t SDL_TOG_setTimeoutVal (uint32_t baseAddr, uint32_t timeoutVal)
 Set the timeout value. More...
 
int32_t SDL_TOG_setIntrPending (uint32_t baseAddr, SDL_TOG_IntrSrc intrSrc)
 Set interrupt source(s) More...
 

Timeout interrupt sources

This is the SDL-FL API documentation for the VBUSM Slave Timeout Gasket module.

The following procedure describes how to properly use this SDL-FL API:

  1. Call SDL_TOG_setTimeoutVal to configure the desired timeout counter value if you wish a shorter timeout than the default maximum timeout.
  2. Enable/disable interrupt sources as needed by calling SDL_TOG_setIntrEnable. Note that all interrupt sources are enabled by default.
  3. Call SDL_TOG_start to start the timer counting
  4. If an interrupt is signaled from the gasket, then... a) Call SDL_TOG_getIntrPending to determine the pending interrupt sources b) Clear interrupt source(s) by calling SDL_TOG_clrIntrPending c) Service the cause of the interrupt as needed. If the system determines that it needs to flush all outstanding transactions (for instance, because the main SoC is in an error condition and is going to be reset), software may do this by calling SDL_TOG_setFlushMode with true. Once all transactions are flushed, software should exit Flush mode by calling SDL_TOG_setFlushMode with false. If the destination side is in reset, this should trigger hardware flush, keeping the gasket returning any transactions that arrive. d) The SDL_TOG_getErrInfo function can be called to get detailed information about the error if needed. e) Ack the interrupt by calling SDL_TOG_getIntrCount and SDL_TOG_ackIntr
typedef uint32_t SDL_TOG_IntrSrc
 This enumerator defines the possible timeout interrupt sources. More...
 
#define SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT   ((uint32_t) 1U<<0)
 
#define SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE   ((uint32_t) 1U<<1)
 
#define SDL_TOG_INTRSRC_COMMAND_TIMEOUT   ((uint32_t) 1U<<2)
 
#define SDL_TOG_INTRSRC_ALL   (SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT | SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE | SDL_TOG_INTRSRC_COMMAND_TIMEOUT)
 

Macro Definition Documentation

◆ SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT

#define SDL_TOG_INTRSRC_TRANSACTION_TIMEOUT   ((uint32_t) 1U<<0)

Transaction timeout

◆ SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE

#define SDL_TOG_INTRSRC_UNEXPECTED_RESPONSE   ((uint32_t) 1U<<1)

Unexpected response

◆ SDL_TOG_INTRSRC_COMMAND_TIMEOUT

#define SDL_TOG_INTRSRC_COMMAND_TIMEOUT   ((uint32_t) 1U<<2)

Command timeout

◆ SDL_TOG_INTRSRC_ALL

Typedef Documentation

◆ SDL_TOG_IntrSrc

typedef uint32_t SDL_TOG_IntrSrc

This enumerator defines the possible timeout interrupt sources.

Function Documentation

◆ SDL_TOG_getIntrCountInternal()

int32_t SDL_TOG_getIntrCountInternal ( uint32_t  baseAddr,
SDL_TOG_IntrSrc  intrSrc,
uint32_t *  pIntrCnt 
)

Read internal interrupt count.

This function reads the internal interrupt count.

Parameters
baseAddr[IN] Base address of the Timeout gasket registers
intrSrc[IN] Interrupt source(s) to set
pIntrCnt[OUT] Pointer to interrupt source count
Returns
SDL_PASS The function completed successfully SDL_EBADARGS baseAddr and timeoutVal are invalid

◆ SDL_TOG_setTimeoutVal()

int32_t SDL_TOG_setTimeoutVal ( uint32_t  baseAddr,
uint32_t  timeoutVal 
)

Set the timeout value.

This function sets the desired timeout value. Note the Timer runs on the VBUS clock and that determines the actual time.

Parameters
baseAddr[IN] Base address of the Timeout gasket registers
timeoutVal[IN] Timeout count value
Returns
SDL_PASS The function completed successfully SDL_EBADARGS baseAddr and timeoutVal are invalid

◆ SDL_TOG_setIntrPending()

int32_t SDL_TOG_setIntrPending ( uint32_t  baseAddr,
SDL_TOG_IntrSrc  intrSrc 
)

Set interrupt source(s)

This function allows software to set the specified interrupt source(s).

The intrSrcs value is composed of a logical OR of the desired interrupt sources defined in SDL_TOG_IntrSrc.

Parameters
baseAddr[IN] Base address of the Timeout gasket registers
intrSrc[IN] Interrupt source(s) to set
Returns
SDL_PASS The function completed successfully SDL_EBADARGS baseAddr and intrSrcs is invalid